This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ev-cog-ad3029wz [17 Sep 2018 09:11] Gowtham shanmugaraj . |
resources:eval:user-guides:ev-cog-ad3029wz [03 Jan 2021 21:46] Robin Getz fix links |
||
---|---|---|---|
Line 1: | Line 1: | ||
====== EV-COG-AD3029WZ Development Kit ====== | ====== EV-COG-AD3029WZ Development Kit ====== | ||
- | The **[[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD3029.html|EV-COG-AD3029WZ]]** (referred also as MCU Cog) is a development platform based on the industry leading ultra low power **[[adi>ADuCM3029]]** 32-bit ARM Cortex™-M4F microcontroller. The platform is designed to be a development and prototyping vehicle to get customer ideas from concept to production with a minimal risk and faster time to market.\\ | + | The **[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD3029.html|EV-COG-AD3029WZ]]** (referred also as MCU Cog) is a development platform based on the industry leading ultra low power **[[adi>ADuCM3029]]** 32-bit ARM Cortex™-M4F microcontroller. The platform is designed to be a development and prototyping vehicle to get customer ideas from concept to production with a minimal risk and faster time to market.\\ |
{{ :resources:eval:user-guides:front_image_new.png?nolink&550|}} | {{ :resources:eval:user-guides:front_image_new.png?nolink&550|}} | ||
Applications using EV-COG-AD3029WZ board can be developed using one of the following toolchains. | Applications using EV-COG-AD3029WZ board can be developed using one of the following toolchains. |