Wiki

This version is outdated by a newer approved version.DiffThis version (17 Sep 2018 09:11) was approved by Gowtham shanmugaraj.The Previously approved version (17 Sep 2018 07:52) is available.Diff

This is an old revision of the document!


EV-COG-AD3029WZ Development Kit

The EV-COG-AD3029WZ (referred also as MCU Cog) is a development platform based on the industry leading ultra low power ADuCM3029 32-bit ARM Cortex™-M4F microcontroller. The platform is designed to be a development and prototyping vehicle to get customer ideas from concept to production with a minimal risk and faster time to market.
Applications using EV-COG-AD3029WZ board can be developed using one of the following toolchains.

  1. Crosscore Embedded Studio 2.7.0 and above - an Eclipse based Analog Devices Interactive Development Environment.
  2. IAR Embedded Workbench for ARM 8.20 and above
  3. Keil uVision 4 and above
  4. ARM mbed Compiler

Make sure a valid license for the selected toolchain is installed before using EV-COG-AD3029WZ board. The software and power measurement is same for both EV-COG-AD3029WZ and EV-COG-AD3029LZ

  1. Software Packs & Board Support Package: EV-COG-AD3029WZ software architecture is categorized into 4 groups as below.
resources/eval/user-guides/ev-cog-ad3029wz.1537168313.txt.gz · Last modified: 17 Sep 2018 09:11 by Gowtham shanmugaraj