Analog Devices EV-COG-AD3029LZ Off-Chip Drivers and Examples
There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029LZ works with EV-COG-AD3029WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
General Description/Overview
The EV-COG-AD3029LZ software pack provides access to all the necessary on-board peripheral drivers for the EV-COG-AD3029LZ development platform. This software layer is the secondary layer needed when writing applications using this development platform. The EV-COG-AD3029LZ software pack builds on top of what the ADuCm302x software pack provides. The EV-COG-AD3029LZ software pack makes it easier to use the on-board peripherals so creating your application layer is will be easier. Combined with the ADuCM302x and Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD3029LZ development platform.
The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio 2.6.0 ® and the ADuCM302x Device Family Pack 2.0.0.
EV-COG-AD3029LZ software pack contains the following components:
Bluetooth Companion Module
On-Chip Driver Examples (
GPIO,
RTC,
SPI, Systick, TMR,
UART, WDT)
Bluetooth Profile Examples
Android IoTNode application software
Documentation
For detailed information regarding the EV-COG-AD3029LZ software pack, please see our complete EV-COG-AD3029LZ software user guide.
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD3029LZ platform.
Downloading the EV-COG-AD3029LZ Software Pack
The software pack can be downloaded in several ways.
Downloaded via the tools program
It is
recommended to download the EV-COG-AD3029LZ software pack through from the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the EV-COG-AD3029LZ software pack through CrossCore Embedded Studio please see our
CrossCore Embedded Studio Quickstart Userguide.
Downloaded to local directory
However if you do decide to download the EV-COG-AD3029LZ software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.
End of Document
Back