Example Projects
Following application are available with EV-COG-AD3029LZ.
Wifi Example: This WiFi Example project provides software support to enable WiFi functionality using ESP8266 WiFi module along with EV-Cog-AD3029LZ over
UART Interface.
SD Card Example: This document explains about the hardware and software setup, which is required to interface the SDHC memory card to the EV-COG-AD3029LZ through
SPI Interface.
SmartMesh Slave Mode Temperature Sensor Example:This document explains how temperature data can be sent via EV-COG-SMARTMESH1Z configured in the slave mode to the E-manager connected to the users PC. It also explains the software flow and how to view the expected output.
Back
End of Document