This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:cn0507-network-analyzer:hw_setup:start [06 Sep 2019 04:05] – Jhake Zebedee Aquino | resources:eval:user-guides:cn0507-network-analyzer:hw_setup:start [06 Sep 2019 07:36] (current) – Jhake Zebedee Aquino | ||
---|---|---|---|
Line 2: | Line 2: | ||
- Mount the CN-0507 board over the EVAL-ADICUP3029. | - Mount the CN-0507 board over the EVAL-ADICUP3029. | ||
- Connect the EVAL-ADICUP3029 to the Laptop thru a micro USB cable. | - Connect the EVAL-ADICUP3029 to the Laptop thru a micro USB cable. | ||
- | - Connect a 6V DC power supply to the CN-0507 | + | - Connect a 6V DC power supply |