This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:eval-adpd410x:fluorescence [27 Jun 2022 23:08] – [Firmware Setup] fixing the to do box and changing it into a download box Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:eval-adpd410x:fluorescence [22 Jul 2022 09:16] (current) – Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== EVAL-ADPD410X-ARDZ Fluorescence Measurement Demo ====== | ====== EVAL-ADPD410X-ARDZ Fluorescence Measurement Demo ====== | ||
- | The **[[ADI> | + | The **[[ADI> |
<note important> | <note important> | ||
- | This demo uses a lot of the optical, mechanical, and photodiode and LED components from the [[ADI> | + | This demo uses a lot of the optical, mechanical, and photodiode and LED components from the [[ADI> |
</ | </ | ||
Line 14: | Line 14: | ||
===== Demo Requirements ===== | ===== Demo Requirements ===== | ||
The following is a list of items needed to replicate this demo. | The following is a list of items needed to replicate this demo. | ||
- | * [[ADI> | + | * [[ADI> |
* [[ADI> | * [[ADI> | ||
* Host computer with PyADI-IIO and relevant dependencies installed (See [[resources: | * Host computer with PyADI-IIO and relevant dependencies installed (See [[resources: | ||
Line 43: | Line 43: | ||
| POWER (S5) | WALL/ | | POWER (S5) | WALL/ | ||
- | Connect the EVAL-ADPD4100-ARDZ or EVAL-ADPD4101-ARDZ to the EVAL-ADICUP3029 using the headers shown below.\\ {{: | + | Connect the [[ADI>EVAL-ADPD410x-ARDZ]] to the [[ADI>EVAL-ADICUP3029]] using the headers, as shown below.\\ {{: |
===== Firmware Setup ===== | ===== Firmware Setup ===== | ||
- | Connect the EVAL-ADICUP3029 to the PC using the micro-USB to USB cable. | + | Connect the [[ADI>EVAL-ADICUP3029]] to the PC using the micro USB to USB cable. |
Drag and drop the appropriate .hex file from the list below to the Daplink Drive. (See [[: | Drag and drop the appropriate .hex file from the list below to the Daplink Drive. (See [[: | ||
Line 72: | Line 72: | ||
===== Hardware Connection ===== | ===== Hardware Connection ===== | ||
- | Connect the 365 nm LED Board, Transmit Photodiode Board, and Fluorescence Photodiode Board to the prototyping connectors of the [[ADI> | + | Connect the 365 nm LED Board, Transmit Photodiode Board, and Fluorescence Photodiode Board to the prototyping connectors of the [[ADI> |
===== Software Setup ===== | ===== Software Setup ===== | ||
This demo uses a PyADI-IIO example script. See [[: | This demo uses a PyADI-IIO example script. See [[: | ||
- | - Connect the [[ADI> | + | - Connect the [[ADI> |
- | - Connect the EVAL-ADICUP3029 to the PC using the micro-USB cable and note the serial port from the Device Manager as in [[resources: | + | - Connect the [[ADI>EVAL-ADICUP3029]] to the PC using the micro-USB cable and note the serial port from the Device Manager as in [[resources: |
- Open command prompt or terminal and navigate through the examples folder inside the downloaded or cloned // | - Open command prompt or terminal and navigate through the examples folder inside the downloaded or cloned // | ||
- Run the example script using the command. < | - Run the example script using the command. < | ||
- | - The script will ask for a serial port. Input the noted serial port and press Enter. In cases when the board is not found, press the reset button (S1) on the EVAL-ADPD4100-ARDZ or EVAL-ADPD4101-ARDZ and input the noted serial port again.\\ {{: | + | - The script will ask for a serial port. Input the noted serial port and press Enter. In cases when the board is not found, press the reset button (S1) on the [[ADI>EVAL-ADPD410x-ARDZ]] and input the noted serial port again.\\ {{: |
- When the board is detected, you will be asked to specify the demo application to use. Since this setup is only applicable for fluorescence measurements, | - When the board is detected, you will be asked to specify the demo application to use. Since this setup is only applicable for fluorescence measurements, | ||
- A plot will appear showing the measured and computed quinine concentration. You have the option to save a copy of the displayed waveform at any point in time using the matplotlib controls at the top. Remove the cuvette and replace the quinine sample with a different concentration to observe the measurement change.\\ {{: | - A plot will appear showing the measured and computed quinine concentration. You have the option to save a copy of the displayed waveform at any point in time using the matplotlib controls at the top. Remove the cuvette and replace the quinine sample with a different concentration to observe the measurement change.\\ {{: |