This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:eval-ad5770r-pmdz [06 Oct 2021 10:32] – removed unintended changes Ian Vincent Andal | resources:eval:user-guides:circuits-from-the-lab:eval-ad5770r-pmdz [03 Mar 2023 00:54] (current) – Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== EVAL-AD5770R-PMDZ | + | ====== EVAL-AD5770R-PMDZ |
\\ | \\ | ||
The EVAL-AD5770R-PMDZ is a minimalist SPI Pmod board for the AD5770R. This module is designed as a low cost alternative to the fully featured AD5770R evaluation board and has no extra signal conditioning for the DAC. | The EVAL-AD5770R-PMDZ is a minimalist SPI Pmod board for the AD5770R. This module is designed as a low cost alternative to the fully featured AD5770R evaluation board and has no extra signal conditioning for the DAC. | ||
Line 12: | Line 12: | ||
===== About the AD5770R ===== | ===== About the AD5770R ===== | ||
\\ | \\ | ||
- | The AD5770R is a 6-channel, 14-bit, multi-range, | + | The [[adi>AD5770R]] is a 6-channel, 14-bit, multi-range, |
\\ | \\ | ||
\\ | \\ | ||
Line 119: | Line 119: | ||
====== Schematic, PCB Layout, Bill of Materials ====== | ====== Schematic, PCB Layout, Bill of Materials ====== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | * {{ : | + | [[adi> |
- | * {{ : | + | * Schematic |
- | * {{ : | + | * PCB Layout |
+ | * Bill of Materials | ||
+ | * Allegro Project | ||
</ | </ | ||