This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0585 [18 May 2023 12:53] – [Reference Demos & Software] Paul Pop | resources:eval:user-guides:circuits-from-the-lab:cn0585 [29 May 2023 10:36] – tables updates Paul Pop | ||
---|---|---|---|
Line 363: | Line 363: | ||
Remote data streaming to and from hardware is made available through system object interfaces, which are unique for each component or platform. | Remote data streaming to and from hardware is made available through system object interfaces, which are unique for each component or platform. | ||
- | The hardware interfacing system objects provide a since class to both configure a given platform and move data back and forth from the device. | + | The hardware interfacing system objects provide a class to both configure a given platform and move data back and forth from the device. |
After running the [[https:// | After running the [[https:// | ||
Line 382: | Line 382: | ||
|< 100% 15% 5% 80% >| | |< 100% 15% 5% 80% >| | ||
^ Interface signal name ^ Width ^ Description ^ | ^ Interface signal name ^ Width ^ Description ^ | ||
- | | CN0585 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | | + | | IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | |
- | | CN0585 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | | + | | IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | |
- | | CN0585 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | + | | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | |
- | | CN0585 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | + | | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | |
| IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | ||
| CN0585 DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | | | CN0585 DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | | ||
Line 391: | Line 391: | ||
| CN0585 DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | | | CN0585 DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | | ||
| CN0585 DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. | | | CN0585 DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. | | ||
- | | IP Data Valid OUT | 1 | Output signal that has to be logic ' | + | | IP Load Tx Data OUT | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid. | |
- | | IP Load Tx Data OUT | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. | | + | |
Line 399: | Line 398: | ||
{{ : | {{ : | ||
- | == Recieve | + | == Receive |
|< 100% 15% 5% 80% >| | |< 100% 15% 5% 80% >| | ||
^ Interface signal name ^ Width ^ Description ^ | ^ Interface signal name ^ Width ^ Description ^ | ||
- | | IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | |
- | | IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | |
- | | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | |
- | | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | |
- | | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | + | | IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. |
| IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. | | | IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. | | ||
| IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. | | | IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. | | ||
Line 419: | Line 418: | ||
- | == Transmit and Recieve | + | == Transmit and Receive |
|< 100% 15% 5% 80% >| | |< 100% 15% 5% 80% >| | ||
^ Interface signal name ^ Width ^ Description ^ | ^ Interface signal name ^ Width ^ Description ^ |