This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0584 [29 May 2023 10:44] – [Additional Information and Useful Links] Paul Pop | resources:eval:user-guides:circuits-from-the-lab:cn0584 [31 May 2023 10:39] – [MATLAB and Simulink] Paul Pop | ||
---|---|---|---|
Line 315: | Line 315: | ||
==== MATLAB and Simulink ==== | ==== MATLAB and Simulink ==== | ||
- | |||
<WRAP round download> | <WRAP round download> | ||
Required MATLAB Add-Ons: | Required MATLAB Add-Ons: | ||
Line 353: | Line 352: | ||
|< 100% 15% 5% 80% >| | |< 100% 15% 5% 80% >| | ||
^ Interface signal name ^ Width ^ Description ^ | ^ Interface signal name ^ Width ^ Description ^ | ||
- | | CN0584 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | | + | | IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | |
- | | CN0584 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | | + | | IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | |
- | | CN0584 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | + | | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | |
- | | CN0584 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | + | | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | |
| IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | ||
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | IP Data Valid OUT | 1 | Output signal that has to be logic ' | + | | IP Load Tx Data OUT | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid. | |
- | | IP Load Tx Data OUT | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. | | + | |
Line 373: | Line 371: | ||
|< 100% 15% 5% 80% >| | |< 100% 15% 5% 80% >| | ||
^ Interface signal name ^ Width ^ Description ^ | ^ Interface signal name ^ Width ^ Description ^ | ||
- | | IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | |
- | | IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | |
- | | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | |
- | | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | + | | CN0585 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | |
- | | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | + | | IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. |
| IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. | | | IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. | | ||
| IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. | | | IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. | | ||
Line 397: | Line 395: | ||
| IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | ||
| IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | ||
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
| IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | | IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | ||
| IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | ||
Line 407: | Line 405: | ||
| IP Data 2 OUT | 16 | ADAQ23876 ADC 2 channel data. To be used as input for the ADC CPAK IP. | | | IP Data 2 OUT | 16 | ADAQ23876 ADC 2 channel data. To be used as input for the ADC CPAK IP. | | ||
| IP Data 3 OUT | 16 | ADAQ23876 ADC 3 channel data. To be used as input for the ADC CPAK IP. | | | IP Data 3 OUT | 16 | ADAQ23876 ADC 3 channel data. To be used as input for the ADC CPAK IP. | | ||
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
- | | CN0584 | + | | CN0585 |
| IP Data Valid OUT | 1 | Output signal that has to be logic ' | | IP Data Valid OUT | 1 | Output signal that has to be logic ' | ||
| IP Load Tx Data OUT | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. | | | IP Load Tx Data OUT | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. | | ||
Line 417: | Line 415: | ||
{{ : | {{ : | ||
- | |||