Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (29 May 2023 10:44) was approved by Paul Pop.The Previously approved version (29 May 2023 08:17) is available.Diff

This is an old revision of the document!


EVAL-CN0584-EBZ User Guide

The EVAL-CN0584-EBZ Low Latency Development Kit (LLDK) board is a development platform consisting of 4 x 16-bit ADC channels and 4 x 16-bit DAC channels that are interfaced with an FPGA through the FMC Low Pin Count (LPC) Connector.

The LLDK board provides a complete data acquisition and signal generation platform with on-board power rails, voltage monitoring, logic level translation, general purpose I/O, I2C, SPI, and a personality interface connector.

The key performance benefit of the LLDK system is the ability to perform a complete capture and conversion of precision analog input data in <70ns with the ADC module and generate a settled full-scale analog output in <250ns from initial data written to the DAC.

Connections and Configurations

ADC Inputs

Channel Positive Input Signal Negative Input Signal
Channel 0 J1 J2
Channel 1 J3 J4
Channel 2 J5 J6
Channel 3 J7 J8

ADC Input Range Configuration

The CN0584 has configurable input voltage ranges of ±10 V(Default), ±5 V, ±4.096 V, ±2.5 V, and ±1.5 V. The input range can be changed by modifying resistor placements on the AFE Board.

Channel Input Voltage Range AFE Board Modification
Channel 0 ±10 V (default) Include R19A, R21A, R22A, R24A; DNI R18A, R20A, R23A, R25A
±5 V Include R18A, R20A, R23A, R25A; DNI R19A, R21A, R22A, R24A
±4.096 V Include R19A, R21A; DNI R18A, R20A, R22A, R23A, R24A, R25A
±2.5 V Include R18A, R20A; DNI R19A, R21A, R22A, R23A, R24A, R25A
±1.5 V Include R18A, R19A, R20A, R21A; DNI R22A, R23A, R24A, R25A
Channel 1 ±10 V (default) Include R19B, R21B, R22B, R24B; DNI R18B, R20B, R23B, R25B
±5 V Include R18B, R20B, R23B, R25B; DNI R19B, R21B, R22B, R24B
±4.096 V Include R19B, R21B; DNI R18B, R20B, R22B, R23B, R24B, R25B
±2.5 V Include R18B, R20B; DNI R19B, R21B, R22B, R23B, R24B, R25B
±1.5 V Include R18B, R19B, R20B, R21B; DNI R22B, R23B, R24B, R25B
Channel 2 ±10 V (default) Include R19C, R21C, R22C, R24C; DNI R18C, R20C, R23C, R25C
±5 V Include R18C, R20C, R23C, R25C; DNI R19C, R21C, R22C, R24C
±4.096 V Include R19C, R21C; DNI R18C, R20C, R22C, R23C, R24C, R25C
±2.5 V Include R18C, R20C; DNI R19C, R21C, R22C, R23C, R24C, R25C
±1.5 V Include R18C, R19C, R20C, R21C; DNI R22C, R23C, R24C, R25C
Channel 3 ±10 V (default) Include R19D, R21D, R22D, R24D; DNI R18D, R20D, R23D, R25D
±5 V Include R18D, R20D, R23D, R25D; DNI R19D, R21D, R22D, R24D
±4.096 V Include R19D, R21D; DNI R18D, R20D, R22D, R23D, R24D, R25D
±2.5 V Include R18D, R20D; DNI R19D, R21D, R22D, R23D, R24D, R25D
±1.5 V Include R18D, R19D, R20D, R21D; DNI R22D, R23D, R24D, R25D

DAC Outputs

The CN0584 can support multiple output voltage ranges which can be configured, such as 0 V to 5 V, −5 V to +5 V, and −10 V to +10 V, and custom intermediate ranges with full 16-bit resolution. In order to change the output range, resistor placements on the AFE board must be modified and register settings must be applied.

Channel Output Span VZS (V) VFS (V) AFE Board Modification Register Setting
CH0+/- 10V (Default) -10.382 10.380 Include R9; DNI R10, R11 CH0_CH1_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R10; DNI R9, R11 CH0_CH1_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R10; DNI R9, R11 CH0_CH1_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R11; DNI R9, R10 CH0_CH1_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R11; DNI R9, R10 CH0_CH1_OUTPUT_RANGE = 0x000
CH1+/- 10V (Default) -10.382 10.380 Include R12; DNI R13, R14 CH0_CH1_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R13; DNI R12, R14 CH0_CH1_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R13; DNI R12, R14 CH0_CH1_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R14; DNI R12, R13 CH0_CH1_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R14; DNI R12, R13 CH0_CH1_OUTPUT_RANGE = 0x000
CH2+/- 10V (Default) -10.382 10.380 Include R15; DNI R16, R17 CH2_CH3_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R16; DNI R15, R17 CH2_CH3_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R16; DNI R15, R17 CH2_CH3_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R17; DNI R15, R16 CH2_CH3_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R17; DNI R15, R16 CH2_CH3_OUTPUT_RANGE = 0x000
CH3+/- 10V (Default) -10.382 10.380 Include R18; DNI R19, R20 CH2_CH3_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R19; DNI R18, R20 CH2_CH3_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R19; DNI R18, R20 CH2_CH3_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R20; DNI R18, R19 CH2_CH3_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R20; DNI R18, R19 CH2_CH3_OUTPUT_RANGE = 0x000

Voltage Reference

The default ADC configuration uses an internal 2.048V 5ppm/°C voltage reference with an optional external LTC6655 2.048V 5ppm/°C reference that is jumper selectable.

The default DAC configuration uses an internal 2.5V 3ppm/°C voltage reference with an optional external ADR4525 2.5V 2ppm/°C reference that is jumper selectable.

VREF Jumper Settings
ADC_VREF Short P5
DAC_VREF Short P4

Power Supply Considerations and Configuration

All power for the CN0584 is provided by the CN0585 through the AFE connector. The CN0584 uses the +15 V and -15 V rails to provide the positive and negative supply voltages for the ADG5421F input protection switches. The +12 V and -12 V rails provide the positive and negative supply voltages for the ADA4898-1 ADC buffer amplifiers. The +3.3 V rail powers the EEPROM circuit. The power rails used in the hardware in the loop low latency development kit include:

Power Rail Description
+12 V LT3045-1 provides the 12V rail supplying up 280mA
-12 V LT3094 provides the -12V rail supplying up to -280mA
+15 V LTM8049 provides the +15V rail at 80% efficiency
-15 V LTM8049 provides the -15V rail at 80% efficiency
+3.3 V Fed through from the FPGA FMC connector to the AFE connector

System Setup Using a Zed Board

The EVAL-CN0584-EBZ is fully supported using a Zedboard.

Demo Requirements

The following is a list of items needed in order to replicate this demo.

  • Hardware
    • ZedBoard Rev D or later board
    • 12Vdc, 3A power supply
    • 16GB (or larger) Class 10 (or faster) micro-SD card
    • Micro-USB cable
    • User interface setup (choose one):
      • HDMI monitor, keyboard, mouse plugged directly into the Zedboard
      • Host Windows/Linux/Mac computer on the same network as the Zedboard

Loading Image on SD Card

In order to boot the Zedboard and control the EVAL-CN0584-EBZ, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided on the Kuiper Linux page.

Configuring the SD Card

Follow the configuration procedure under Configuring the SD Card for FPGA Projects on the Kuiper Linux page. Copy the following files onto the boot directory to configure the SD card:

  • uImage file for Zynq
  • BOOT.BIN specific to your EVAL-CN0585-FMCZ + ZedBoard
  • devicetree.dtb for Zynq specific to your EVAL-CN0585-FMCZ + ZedBoard

Setting up the Hardware

You will need to:

  • Get the ZedBoard.
  • Insert the SD-CARD into the SD Card Interface Connector (J12).
  • Connect the EVAL-CN0585-FMCZ board into the ZedBoard FMC connector.
  • Connect the EVAL-CN0584-EBZ board into the EVAL-CN0585-FMCZ.
  • Connect USB UART J14 (Micro USB) to your host PC.
  • Plug your ethernet cable into the RJ45 ethernet connector(J11).
  • Plug the Power Supply into the 12V Power input connector (J20) (DO NOT turn the device on).
  • Set the jumpers as seen in the below picture: zed_jumpers.jpg
  • Loopback the DAC's output channels to the ADC's inputs as seen in the below picture: loopback_connection.jpg
  • Turn it on.
  • Wait ~30 seconds for the “DONE” LED to turn blue. This is near the DISP1.

All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

Application Software (both locally and remotely on the FPGA)

Hardware Connection

The Libiio is a library used for interfacing with IIO devices and is required to be installed on your computer.

Download and Install the latest Libiio package on your machine.

To be able to connect your device, the software must be able to create a context. The context creation in the software depends on the backend used to connect to the device as well as the platform where the EVAL-CN0584-EBZ is attached. The Zedboard running ADI Kuiper Linux is currently the only platform supported for the CN0584. The user needs to supply a URI which will be used in the context creation.

The iio_info command is a part of the libIIO package that reports all IIO attributes.

Upon installation, simply enter the command on the terminal command line to access it.

For FPGA Direct Local Access:

iio_info

For Windows machine connected to an FPGA:

iio_info -u ip:<ip address of your ip>

Example:

  • If your Zedboard has the IP address 192.168.1.7, you have to use iio_info -u ip::192.168.1.7 as your URI
Do note that the Windows machine and the FPGA board should be connected to the same network in order for the machine to detect the device.

IIO Oscilloscope

Make sure to download/update to the latest version of IIO-Oscilloscope found on this linkhttps://github.com/analogdevicesinc/iio-oscilloscope/releases
  • Once done with the installation or an update of the latest IIO-Oscilloscope, open the application. The user needs to supply a URI which will be used in the context creation of the IIO Oscilloscope and the instructions can be seen in the previous section.
  • Press refresh to display available IIO Devices and press connect.
  • After the board is connected set the raw value to 1 for the following output voltages of the one-bit-adc-dac device which is the controller for the MAX7301ATL+ I/O Expander. This step will configure the value for the following pins which are connected to the MAX7301ATL+ I/O Expander:
one-bit-adc-dac device channel Schematic PIN
Voltage0 GPIO0_VIO
Voltage1 GPIO1_VIO
Voltage2 GPIO2_VIO
Voltage3 GPIO3_VIO
Voltage4 GPIO6_VIO
Voltage5 GPIO7_VIO
Voltage6 PAD_ADC0
Voltage7 PAD_ADC1
Voltage8 PAD_ADC2
Voltage9 PAD_ADC3
  • Select the desired input source for both AD3552R devices.
Even if the input source is set to adc_input or ramp_input the steps regarding the DAC Data Management tab have to be followed.
  • Select the desired output range for both AD3552R devices.
Make sure you don't try to read/write the output_range attribute when the stream_status is in start_stream or start_stream_synced.
  • From the DAC Data Manager Window select the output channels of the DAC and enable the cyclic buffer.
  • Load an example file from the IIO Oscilloscope/lib/osc/waveforms folder.
If the source is set as dma_input and the data from all 4 channels needs to be synchronized make sure that you press the load button for the axi-ad3552r-1 device first then for axi-ad3552r-0.

dac_data_management_cn0585.jpg

  • Click on the load button.
If the source is set as dma_input and the data from all 4 channels needs to be synchronized make sure that you write the start_stream_synced for the axi-ad3552r-1 device first then for axi-ad3552r-0.
  • Select the stream_status IIO Attribute and start the stream (start_stream_synced means that all 4 channels are updated at the same time and the data streaming process waits for both DACs to be started).

stream_status_iio.jpg

If the source is set as dma_input and the data from all 4 channels needs to be synchronized make sure that you write the start_stream_synced for the axi-ad3552r-1 device first then for axi-ad3552r-0.
  • After the stream_status has been written you should see the data capture window: captured_loopback_signal_cn0585.jpg
Note that there is a phase delay between voltage0/voltage2 and voltage1/voltage3 because the DAC device channels are updated consecutively See the DAC UPDATE MODES section in AD3552R Data Sheet.
If you intend to stop the stream transmission and start it again synchronized set the stream_status IIO Attribute to stop_stream for axi-ad3552r-1 device first then for the axi-ad3552r-0 device.

PyADI-IIO

PyADI-IIO is a Python abstraction module for ADI hardware with IIO drivers to make them easier to use. This module provides device-specific APIs built on top of the current libIIO Python bindings. These interfaces try to match the driver naming as much as possible without the need to understand the complexities of libIIO and IIO.

Follow the step-by-step procedure on how to install, configure, and set up PYADI-IIO and install the necessary packages/modules needed by referring to this link.

Running the example

Github link for the Python sample script: CN0585 Python Example

After installing and configuring PYADI-IIO on your machine, you are now ready to run Python script examples. In our case, run the cn0585_fmcz_example.py found in the examples folder.

D:\pyadi-iio>export PYTHONPATH=D:/pyadi-iio/ 
D:\pyadi-iio>python examples/cn0585_fmcz_example.py ip:your_board_ip

Press enter and you will get these readings:

$ python examples/cn0585_fmcz_example.py
uri: ip:your_board_ip
############# EEPROM INFORMATION ############
read 256 bytes from /sys/devices/soc0/fpga-axi@0/41620000.i2c/i2c-1/1-0050/eeprom
Date of Man     : Fri Jan 20 08:11:00 2023
Manufacturer    : Analog Devices
Product Name    : LLDK-LTC2387-AD3552R
Serial Number   : 56864654
Part Number     : 1234
FRU File ID     : 12131321
PCB Rev         : VB
PCB ID          : HIL
BOM Rev         : VC
Uses LVDS       : Y

#############################################
GPIO4_VIO state is: 0
GPIO5_VIO state is: 0
Voltage monitor values:
Channel :  temp0 :  49.25 Deg. C
Channel :  voltage0 :  2.26745605283 V
Channel :  voltage1 :  0.6274414057359999 V
Channel :  voltage2 :  2.061157224874 V
Channel :  voltage3 :  0.7531738275079999 V
Channel :  voltage4 :  2.092285154536 V
Channel :  voltage5 :  2.084960935792 V
Channel :  voltage6 :  2.2534179669039998 V
Channel :  voltage7 :  1.80969238133 V
AXI4-Lite 0x108 register value: 0x2
AXI4-Lite 0x10c register value: 0xB
Sample data min: 0
Sample data max: 65535
input_source:dac0: adc_input
input_source:dac1: adc_input
Maximum measured voltage 0 : 10.115187500000001
Maximum measured voltage 1 : 0.00103125
Maximum measured voltage 2 : 0.00034375000000000003
Maximum measured voltage 3 : 0.00103125
Minimum measured voltage 0: 10.107625
Minimum measured voltage 1: -0.00034375000000000003  
Minimum measured voltage 2: -0.00103125
Minimum measured voltage 3: -0.00034375000000000003

The following window will pop up:

python_plot.jpg

If you plan to transmit multiple cycles of synchronous stream, make sure axi-ad3552r-1 is started/stopped first, then axi-ad3552r-0.


Github link for the Matlab sample script: CN0585StreamingTest.m

The steps described in the Analog Devices Transceiver Toolbox For MATLAB and Simulink page have to be followed to configure the Matlab/Simulink project using the MathWorks HDL Workflow Advisor.

Device Control and Data Streaming

Remote data streaming to and from hardware is made available through system object interfaces, which are unique for each component or platform. The hardware interfacing system objects provide a class to both configure a given platform and move data back and forth from the device. After running the CN0585StreamingTest.m example The following window will pop up:

matlab_plot.jpg

This is the terminal output that can be observed if the HDL Targeting with HDL-Coder flow was followed and there are 2 AXI4-Lite registers in the HDL DUT IP:

terminal_matlab_cn0585.jpg

If you plan to transmit multiple cycles of synchronous stream, make sure axi-ad3552r-1 is started/stopped first, then axi-ad3552r-0.

HDL Targeting with HDL-Coder

Precision Toolbox supports the IP Core generation flow from MathWorks which allows for automated integration of DSP into HDL reference designs from Analog Devices. This workflow will take Simulink subsystems, run HDL-Coder to generate source Verilog, and then integrate that into a larger reference design.

Transmit reference design (Tx)
Interface signal name Width Description
CN0584 ADC Data 0 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 1 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 2 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 3 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design.
IP Valid Tx Data IN 1 Input signal that has logic 1 value for a clock cycle period when the data starts to be valid.
CN0584 DAC Data 0 OUT 16 AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP.
CN0584 DAC Data 1 OUT 16 AD3552R_0 DAC 1 channel data. To be used as input into the AD3552R interface IP.
CN0584 DAC Data 2 OUT 16 AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP.
CN0584 DAC Data 3 OUT 16 AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP.
IP Data Valid OUT 1 Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid.
IP Load Tx Data OUT 1 Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle.
HDL Block diagram for Tx Reference design

Receive reference design (Rx)
Interface signal name Width Description
IP Data 0 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design.
IP Data 1 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design.
IP Data 2 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design.
IP Data 3 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design.
IP Valid Tx Data IN 1 Input signal that has logic 1 value for a clock cycle period when the data starts to be valid.
IP Data 0 OUT 16 ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP.
IP Data 1 OUT 16 ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP.
IP Data 2 OUT 16 ADAQ23876 ADC 2 channel data. To be used as input for the ADC CPAK IP.
IP Data 3 OUT 16 ADAQ23876 ADC 3 channel data. To be used as input for the ADC CPAK IP.
IP Data Valid OUT 1 Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid.
HDL Block diagram for Rx Reference design

Transmit and Receive reference design (Tx & Rx)
Interface signal name Width Description
IP Data 0 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design.
IP Data 1 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design.
IP Data 2 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design.
IP Data 3 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 0 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 1 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 2 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design.
CN0584 ADC Data 3 IN 16 Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design.
IP Valid Rx Data IN 1 Input signal that has logic 1 value for a clock cycle period when the data starts to be valid.
IP Valid Tx Data IN 1 Input signal that has logic 1 value for a clock cycle period when the data starts to be valid.
IP Data 0 OUT 16 ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP.
IP Data 1 OUT 16 ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP.
IP Data 2 OUT 16 ADAQ23876 ADC 2 channel data. To be used as input for the ADC CPAK IP.
IP Data 3 OUT 16 ADAQ23876 ADC 3 channel data. To be used as input for the ADC CPAK IP.
CN0584 DAC Data 0 OUT 16 AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP.
CN0584 DAC Data 1 OUT 16 AD3552R_0 DAC 1 channel data. To be used as input into the AD3552R interface IP.
CN0584 DAC Data 2 OUT 16 AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP.
CN0584 DAC Data 3 OUT 16 AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP.
IP Data Valid OUT 1 Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid.
IP Load Tx Data OUT 1 Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle.
HDL Block diagram for Tx and Rx Reference design

Schematic, PCB Layout, Bill of Materials

EVAL-CN0584-EBZ Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • Allegro Project

Reference Demos & Software

Hardware Registration

Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!

resources/eval/user-guides/circuits-from-the-lab/cn0584.1685349842.txt.gz · Last modified: 29 May 2023 10:44 by Paul Pop