This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0548 [11 Jan 2022 12:06] – [Simplified Block Diagram] Harvey John De Chavez | resources:eval:user-guides:circuits-from-the-lab:cn0548 [11 Jan 2022 12:08] – [PyADI-IIO] Harvey John De Chavez | ||
---|---|---|---|
Line 101: | Line 101: | ||
\\ \\ | \\ \\ | ||
The other important attribute is the gain. The gain attribute corresponds to the internal gain of the ADC. A user can apply an internal gain to the ADC allowing the differential ADC input to be amplified. This feature can come in handy when dealing with small signals but the user must take precaution as applying an internal gain effectively decreases the input rating of the board. It is highly recommended to read and consult the datasheet of the ADC before creating a customized hex file. | The other important attribute is the gain. The gain attribute corresponds to the internal gain of the ADC. A user can apply an internal gain to the ADC allowing the differential ADC input to be amplified. This feature can come in handy when dealing with small signals but the user must take precaution as applying an internal gain effectively decreases the input rating of the board. It is highly recommended to read and consult the datasheet of the ADC before creating a customized hex file. | ||
- | \\ | + | \\ \\ |
+ | \\ | ||
====PyADI-IIO ==== | ====PyADI-IIO ==== | ||