This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0540:coraz7s [25 Feb 2022 18:19] – updating procedure through UART Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0540:coraz7s [25 Feb 2022 18:22] (current) – Brandon Bushey | ||
---|---|---|---|
Line 76: | Line 76: | ||
- The serial terminal connection will default to auto login and will place you in the root directory of the SD card. | - The serial terminal connection will default to auto login and will place you in the root directory of the SD card. | ||
- From here its a good idea to check to see if your devices can be found using the command **// | - From here its a good idea to check to see if your devices can be found using the command **// | ||
- | | + | |
- Type **// | - Type **// | ||
- That should echo back some information where you can pull out the inet address of eth0.{{ : | - That should echo back some information where you can pull out the inet address of eth0.{{ : |