This is an old revision of the document!
Geiger counters are one of the most commonly used tools to measure radiation levels. This is a very popular sensor in other countries like Japan where power is mainly generated from nuclear plants. This type of sensor is generally deployed in numbers across different areas and are linked together to a cloud server for easy monitoring.
EVAL-CN0536-ARDZ is a low-power Geiger counter in an Arduino form factor that can run on a 3V to 5V system supply. It has a low cost, high voltage generation power supply that is robust and adjustable voltage output from 280V to 500V output. One of the key major part of the circuit in figure 1 is to generate high voltage output using Analog Devices precision programmable oscillator that is versatile, compact and easy to use LTC6906 that can be set to run oscillate from 10khz to 1Mhz using single user defined resistor value. This reference circuit design is compatible with most of the Geiger-Muller tube sensors available in the market today with a voltage rating between 280V to 500V.
To set and regulate the high voltage output supply and capture Geiger-Muller tube distinct pulses , the circuit shown in figure 1 has Analog devices LTC1540, a nano power comparator with built in voltage reference to precisely set the user required voltage output and LTC1441 ultralow power dual comparator to translate Geiger pulse to logic level 3V or 5V .
It has also LT6994 robust built in delay block timer chip that generateS the Geiger clicking sound to a regular buzzer. The LT6994 is a programmable delay block timer with a range of 1µs to 33.6 seconds. The LT6994 is part of the TimerBlox® family of versatile silicon timing devices. A single resistor, RSET, programs an internal master oscillator frequency, setting the LT6994’s time base. The input-to-output delay is determined by this master oscillator and internal clock divider.
The circuit also has LEDs indicating radiation levels , reports counts per minute ,microSieverts per minute via USB UART terminal display or via internet through MQTT.
This user guide will discuss how to use the EVAL-ADICUP3029 and evaluation software on how to configure and collect data from the EVAL-CN0536-ARDZ Evaluation Board (CN-0536 Board).
All connector pinouts for the EVAL-CN0536-ARDZ are described in the table below.
Connector | Pin No. | Pin Name | ADuCM3029 Pin Function | CN0536 Pin Function |
---|---|---|---|---|
Arduino DIO High | 1 | SCL | I2C0_SCL/GPIO04 | NC |
2 | SDA | I2C0_SDA/GPIO05 | NC | |
3 | AREF | VREF+ | NC | |
4 | AGND | AGND (Analog ground) | DGND | |
5 | SCLK | SPI0_CLK/SPT0_BCLK/GPIO00 | NC | |
6 | MISO | SPI0_MISO/SPT0_BD0/GPIO02 | NC | |
7 | MOSI | SPI0_MOSI/SPT0_BFS/GPIO01 | NC | |
8 | CS | SPI0_CS1/SYS_CLKIN/SPI1_CS3/GPIO26 | NC | |
9 | RDY | SPI0_RDY/GPIO30 | NC | |
10 | IO28 | GPIO28 | NC | |
Arduino DIO Low | 1 | IO08 | BPR0_TONE_N/GPIO08 | NC (FOR TESTING) |
2 | IO27 | TMR1_OUT/GPIO27 | HV POWER GOOD | |
3 | IO33 | XINT0_WAKE3/TMR2_OUT/GPIO33 | GEIGER DETECT SIGNAL | |
4 | IO09 | BPR0_TONE_P/SPI2_CS1/GPIO09 | ||
5 | IO13 | XINT0_WAKE2/GPIO13 | ||
6 | IO15 | XINT0_WAKE0/GPIO15 | NC | |
7 | TX | UART0_TX/GPIO10 | NC | |
8 | RX | UART0_RX/GPIO11 | NC | |
Arduino Analog | 1 | AIN0 | ADC0_VIN0/GPIO35 | LED1 |
2 | AIN1 | ADC0_VIN1/GPIO36 | LED2 | |
3 | AIN2 | ADC0_VIN2/GPIO37 | LED3 | |
4 | AIN3 | ADC0_VIN3/GPIO38 | LED4 | |
5 | AIN4 | ADC0_VIN4/SPI2_CS3/GPIO39 | NC | |
6 | AIN5 | ADC0_VIN5/SPI0_CS2/GPIO40 | NC(FOR TESTING ONLY) | |
Arduino Power | 1 | NC | - not connected - | NC |
2 | IOREF | +3.3V | IO_VREF (+3V3) | |
3 | RESET | SYS_HWRST_N | NC | |
4 | 3.3V | +3.3V | NC | |
5 | 5V | +5V | 5V | |
6 | GND | DGND (Digital Ground) | GND | |
7 | GND | DGND (Digital Ground) | GND | |
8 | Vin | DC Barrel Jack Power +7V to +12V | +7.5V |
EVAL-CN0536-ARDZ Design & Integration Files
End of Document