Wiki

This version is outdated by a newer approved version.DiffThis version (02 Jun 2021 10:54) was approved by Mihail Chindris.The Previously approved version (09 Mar 2021 17:31) is available.Diff

This is an old revision of the document!


EVAL-CN0536-ARDZ Shield Overview

Geiger counters are most commonly used by people to measure radiation levels in different specific places. This is a very popular sensor in other countries like Japan that has active nuclear power plants as their source to generate electricity. This type of sensor is sometimes deployed in different places that are linked to the cloud database to monitor dangerous radiation levels that may occur. EVAL-CN0536-ARDZ is a low-power Geiger counter radiation detector in an Arduino shield form factor that can run on 3V to 5V system supply. It has a low cost, high voltage generation power supply that is robust and adjustable voltage output from 280V to 500V output. One of the key major part of the circuit in figure 1 is  to generate high voltage output using Analog Devices precision programmable oscillator that is versatile, compact and easy to use LTC6906 that can be set to run oscillate from 10khz to 1Mhz using single user defined resistor value. This reference circuit design is compatible with most of the Geiger-Muller tube sensors available in the market today with a voltage rating between 280V to 500V.

To set and regulate the high voltage output supply and capture Geiger-Muller tube distinct pulses , the circuit shown in figure 1 has Analog devices LTC1540, a nano power comparator with built in voltage reference to precisely set the user required voltage output and LTC1441 ultralow power dual comparator to translate Geiger pulse to logic level 3V or 5V .

It has also LT6994 robust built in delay block timer chip that generateS the Geiger clicking sound to a regular buzzer. The LT6994 is a programmable delay block timer with a range of 1µs to 33.6 seconds. The LT6994 is part of the TimerBlox® family of versatile silicon timing devices. A single resistor, RSET, programs an internal master oscillator frequency, setting the LT6994’s time base. The input-to-output delay is determined by this master oscillator and internal clock divider.

The circuit also has LEDs indicating radiation levels , reports counts per minute ,microSieverts per minute via USB UART terminal display or via internet through MQTT.

This user guide will discuss how to use the EVAL-ADICUP3029 and evaluation software on how to configure and collect data from the EVAL-CN0536-ARDZ Evaluation Board (CN-0536 Board).

EVAL-CN0536-ARDZ attached to EVAL-ADICUP3029

Simplified functional block diagram


General Setup

Equipment

Peripheral Connectors

All connector pinouts for the EVAL-CN0536-ARDZ are described in the table below.

Connector Pin No. Pin Name ADuCM3029 Pin Function CN0536 Pin Function
Arduino DIO High 1 SCL I2C0_SCL/GPIO04 NC
2 SDA I2C0_SDA/GPIO05 NC
3 AREF VREF+ NC
4 AGND AGND (Analog ground) DGND
5 SCLK SPI0_CLK/SPT0_BCLK/GPIO00 NC
6 MISO SPI0_MISO/SPT0_BD0/GPIO02 NC
7 MOSI SPI0_MOSI/SPT0_BFS/GPIO01 NC
8 CS SPI0_CS1/SYS_CLKIN/SPI1_CS3/GPIO26 NC
9 RDY SPI0_RDY/GPIO30 NC
10 IO28 GPIO28 NC
Arduino DIO Low 1 IO08 BPR0_TONE_N/GPIO08 NC (FOR TESTING)
2 IO27 TMR1_OUT/GPIO27 HV POWER GOOD
3 IO33 XINT0_WAKE3/TMR2_OUT/GPIO33 GEIGER DETECT SIGNAL
4 IO09 BPR0_TONE_P/SPI2_CS1/GPIO09
5 IO13 XINT0_WAKE2/GPIO13
6 IO15 XINT0_WAKE0/GPIO15 NC
7 TX UART0_TX/GPIO10 NC
8 RX UART0_RX/GPIO11 NC
Arduino Analog 1 AIN0 ADC0_VIN0/GPIO35 LED1
2 AIN1 ADC0_VIN1/GPIO36 LED2
3 AIN2 ADC0_VIN2/GPIO37 LED3
4 AIN3 ADC0_VIN3/GPIO38 LED4
5 AIN4 ADC0_VIN4/SPI2_CS3/GPIO39 NC
6 AIN5 ADC0_VIN5/SPI0_CS2/GPIO40 NC(FOR TESTING ONLY)
Arduino Power 1 NC - not connected - NC
2 IOREF +3.3V IO_VREF (+3V3)
3 RESET SYS_HWRST_N NC
4 3.3V +3.3V NC
5 5V +5V 5V
6 GND DGND (Digital Ground) GND
7 GND DGND (Digital Ground) GND
8 Vin DC Barrel Jack Power +7V to +12V +7.5V

Schematic, PCB Layout, Bill of Materials

EVAL-CN0536-ARDZ Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • Allegro Project

Software

End of Document

resources/eval/user-guides/circuits-from-the-lab/cn0536.1622624059.txt.gz · Last modified: 02 Jun 2021 10:54 by Mihail Chindris