This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0534 [27 Oct 2021 08:39] – [General Setup] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0534 [30 Nov 2021 19:49] (current) – updated intro paragraph Brandon Bushey | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Overview ===== | ===== Overview ===== | ||
- | The International Telecommunication Union (ITU) allocates the unlicensed | + | The International Telecommunication Union (ITU) allocates the un-licensed |
- | The 5.8GHz band is preferred for short-range digital communication applications (such as WiFi) because of the number of channels and the bandwidth available. While the transmission range is shorter | + | The 5.8 GHz band is preferred for short range digital communication applications (such as WiFi) because of the number of channels and the bandwidth available. While the transmission range is short-er |
- | This design provides | + | This design provides high gain, robust overpower monitoring, and protection all in a small footprint, |
- | The circuit shown in the figure below is a high performance RF receiver system with 10dB of gain, optimized for operation at a center frequency of 5.8GHz. By keeping the input unfiltered and using a filter to attenuates out-of-band interferers at the amplifier output, the entire system noise figure performance is at 2dB. | + | |
- | The circuit includes a high speed overpower cutoff that protects sensitive downstream equipment connected to the receiver system. | + | |
- | The RF inputs and outputs are standard SMA connectors, and the entire design is powered from a single micro USB connector. | + | The circuit is a high performance RF receiver system with +23 dB of gain, optimized for operation at a center frequency of 5.8 GHz. The input is unfiltered, maintaining a noise figure of 2 dB, while a bandpass filter at the output attenuates out-of-band interferers. |
+ | |||
+ | The circuit includes a high speed overpower detector and switch that protects sensitive downstream equipment connected to the receiver system. The receiver system also automatically returns to normal operation when the RF power level drops within the acceptable range. | ||
{{ : | {{ : | ||
- | {{ : | + | {{ : |
===== General Setup ===== | ===== General Setup ===== | ||
Line 27: | Line 28: | ||
===== Connectors ===== | ===== Connectors ===== | ||
- | {{ : | + | {{ : |
==== SMA Connectors ==== | ==== SMA Connectors ==== | ||
Line 122: | Line 123: | ||
=== Auto Shutdown Operation === | === Auto Shutdown Operation === | ||
- | The plot is as shown below with transmit power set to -10 dBFS producing a 40.25 dB RSSI RF power input reading | + | The plot is as shown below with transmit power set to -10 dBFS producing a 40.25 dB RSSI RF power input reading |
{{ : | {{ : | ||