Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0534 [30 Mar 2021 14:31] – [ADALM-Pluto Preparation] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0534 [27 Oct 2021 08:33] – [IIO Oscilloscope] erbe reyta |
---|
The RF inputs and outputs are standard SMA connectors, and the entire design is powered from a single micro USB connector. | The RF inputs and outputs are standard SMA connectors, and the entire design is powered from a single micro USB connector. |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_system_block_diagram_simplified_v2_.png |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_system_block_diagram_simplified_v3_.png?900 |}} |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:eval-cn0534-ebz.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_top_view.png?600 |}} |
| |
===== General Setup ===== | ===== General Setup ===== |
| |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:led_power_indicatorv2.gif?400 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_led_power_indicator.png?600 |}} |
| |
<note>LED, DS1 from CN0534, will automatically turn on indicating that the CN0534 is powered and operational. If the LED is off, the CN0534 could still be powered properly, but the RF input power into the amplifier might be activating the automatic shutdown, so try to lower the RF input signal by 10dB and see if the LED turns on.</note> | <note>LED, DS1 from CN0534, will automatically turn on indicating that the CN0534 is powered and operational. If the LED is off, the CN0534 could still be powered properly, but the RF input power into the amplifier might be activating the automatic shutdown, so try to lower the RF input signal by 10dB and see if the LED turns on.</note> |
===== Connectors ===== | ===== Connectors ===== |
| |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_connector_labels.png?900 |}} |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:connector_label.gif |}} | |
==== SMA Connectors ==== | ==== SMA Connectors ==== |
| |
==== Test Setup ==== | ==== Test Setup ==== |
=== Normal Operation === | === Normal Operation === |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:hw_test_setup.jpg |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_and_adalm_pluto_test_setup.png?600 |}} |
- Connect the RF TX of Pluto SDR to J2 of the [[adi>CN0534|EVAL-CN0534-EBZ Board]] | - Connect the RF TX of Pluto SDR to J2 of the [[adi>CN0534|EVAL-CN0534-EBZ Board]] |
- Connect J1 of the [[adi>CN0534|EVAL-CN0534-EBZ Board]] to an RF attenuator to protect the RX of Pluto from exceeding its limits. | - Connect J1 of the [[adi>CN0534|EVAL-CN0534-EBZ Board]] to the RF RX of Pluto SDR |
- Connect P1 (micro USB) connector of the [[adi>CN0534|EVAL-CN0534-EBZ Board]] into a PC USB port or 5V USB charger. | - Connect P1 (micro USB) connector of the [[adi>CN0534|EVAL-CN0534-EBZ Board]] into a PC USB port or 5V USB charger. |
- The DS1 LED of CN0534 will automatically turn on indicating the board is powered on and is in operation. | - The DS1 LED of CN0534 will automatically turn on indicating the board is powered on and is in operation. |
| |
<note important>The ADALM-Pluto can be configured using an IIO Oscilloscope, visit the website on | <note important>The ADALM-Pluto can be configured using an IIO Oscilloscope, visit the website on |
[[:resources:tools-software:linux-software:iio_oscilloscope|IIO Oscilloscope]] to know more about the tool. | * [[:resources:tools-software:linux-software:iio_oscilloscope|IIO Oscilloscope]] to know more about the tool. |
| * Optional: an RF attenuator can be connected in between the [[adi>CN0534|EVAL-CN0534-EBZ Board]] RF Output and the RF RX of Pluto SDR to protect the RX of Pluto from exceeding its limits. |
</note> | </note> |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:connecting_of_iio_osc.jpg?400 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:connecting_of_iio_osc.jpg?400 |}} |
| |
=== ADALM Pluto Output === | === ADALM Pluto Loop-Back Operation === |
The plot shown below is the ADALM Pluto output with the RF TX and RX connected directly producing a -16dBFS RF power reading: | |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_loop_back_config_only_without_attenuator.jpg?400 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:adalm_pluto_loop_back_test_measurement_setup.png?200 |}} |
| The plot shown below is the ADALM Pluto output with the RF TX and RX connected directly with transmit power set to -30 dBFS producing a 63.5 dB RSSI RF power input reading: |
| |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:at_n30_rfoutput_scale_loop_back.png?600 |}} |
| And with transmit power set to -10 dBFS producing a 43.5 dB RSSI RF power input reading: |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:at_n10_rfoutput_scale_loop_back.png?600 |}} |
| |
The plot shown below is the ADALM Pluto output with the RF attenuator connected only producing a -26dBFS RF power reading: | |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_loop_back_config_only.jpg?400 |}} | |
| |
=== Normal Operation === | === Normal Operation === |
| |
To configure the the EVAL-CN0534-EBZ with the RF switch CLOSED, replicate configuration on the IIO Oscilloscope Tab as shown below: | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_adalm_pluto_test_measurement_setup.png?400 |}} |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_closed_ad9364_settings_2.png?250|}} | The plot is as shown below with transmit power set to -30 dBFS producing a 41.5 dB RSSI RF power input reading providing a gain of 22dB in reference with the loop back test operation: |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_closed_ad9364_settings_3.png?250|}} | |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_closed_ad9364_settings_1.png?250 |}} | |
| |
The plot is as shown below with -14dBFS RF power reading: | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:at_n30_rfoutput_scale.png?600 |}} |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_closed.png?400 |}} | |
| |
=== Auto Shutdown Operation === | === Auto Shutdown Operation === |
To configure the the EVAL-CN0534-EBZ with the RF switch OPENED, replicate configuration on the IIO Oscilloscope Tab as shown below: | |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_open_ad9364_settings_2.png?250|}} | |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_open_ad9364_settings_3.png?250|}} | |
{{:resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_open_ad9364_settings_1.png?250 |}} | |
| |
The plot is as shown below with -23dBFS RF power reading: | The plot is as shown below with transmit power set to -10 dBFS producing a 40.25 dB RSSI RF power input reading providing a 20 dB attenuation in reference with the loop back test operation: |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:rf_switch_open.png?400 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:at_n10_rfoutput_scale.png?600 |}} |
| |
----------------- | ----------------- |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_sample_application.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_sample_application.png?600 |}} |
| |
Never do this in normal operation. | Never do this in normal operation. |
</WRAP> | </WRAP> |
* [[ADI>CN0534|CN0534 Circuit Note Page]] | * [[ADI>CN0534|CN0534 Circuit Note Page]] |
* [[ADI>HMC717A|HMC717A Product Page]] | * [[ADI>HMC717A|HMC717A Product Page]] |
* [[ADI>HMC550|HMC550 Product Page]] | * [[ADI>ADL5904|ADL5405 Product Page]] |
* [[ADI>ADL5904|ADL5904 Product Page]] | * [[ADI>HMC802A|HMC802A Product Page]] |
| * [[ADI>LTC6991|LTC6991 Product Page]] |
| * [[ADI>LT8335|LT8335 Product Page]] |
* [[ADI>ADM7150|ADM7150 Product Page]] | * [[ADI>ADM7150|ADM7150 Product Page]] |
* [[ADI>LT3042|LT3042 Product Page]] | * [[ADI>ADP150|ADP150 Product Page]] |
* [[ADI>LTM8045|LTM8045 Product Page]] | |
* [[/university/tools/pluto/users/amp|RF Amplifier Considerations]] | * [[/university/tools/pluto/users/amp|RF Amplifier Considerations]] |
</WRAP> | </WRAP> |
| |
<WRAP round 80% download> | <WRAP round 80% download> |
[[adi>media/en/reference-design-documentation/design-integration-files/CN0534-DesignSupport.zip|EVAL-CN0534-SDPZ Design & Integration Files]] | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:cn0534_design_support_package.zip |EVAL-CN0534-SDPZ Design & Integration Files}} |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0534:eval-cn0534-ebz_design_files.zip |}} | |
| |
* Schematics | * Schematics |
* PCB Layout | * PCB Layout |
* Bill of Materials | * Bill of Materials |
* PADS project | * Gerber Files |
| * Allegro Board File |
</WRAP> | </WRAP> |
| |
//End of Document// | //End of Document// |