This version is outdated by a newer approved version.This version (05 Oct 2020 04:02) is a draft.
Approvals: 0/1
This is an old revision of the document!
EVAL-CN0509-EBZ Overview
CN0509 1 is a very wide input range USB charger capable of providing up to 2A at 5V from a wide range of DC sources including solar panels, fully charged or half-discharged car batteries, -48V telecom backup supplies, random stacks of alkaline cells, treadmill motors hacked to run as generators, wind turbines, etc. using the combination of wide input LTC7103 buck converter and an isolated flyback converter LT8302. The circuit will accept any DC voltage from 5V to 100V and produce an isolated 5V supply via a standard USB connector. The outer case of many cell phones and other portable electronics are often electrically connected to USB ground. As such, isolation is necessary in situations in which the power source’s relationship to Earth ground is unknown.
The circuit will survive up to 100V reverse connection to a power source with a green LED indicating correct input polarity and red led otherwise.
Features
Allows wide input range of 5V to 100V
Provides isolated and regulated 5V output
Provides up to 2A output current
Two
USB output ports for convenience
Documents Needed
Equipment Required
Block Assignments
USB Output Connectors
Test setup
Running the System
Ensure safe connection as it may deal with input voltages up to 100
V
Upon turning on DC input, CN0509 will turn on. The circuit will determine if input connection is in correct polarity through lighting DS1 or DS2.
If DS1 (green LED) turns on, this means correct polarity on the input and circuit delivers up to 10W on P2
USB output ports. Else, turn off input supply and re-connect supply outputs to P1 to correct connection.
Connect the device/load at P2 output
USB receptacle of CN0509. The lower port (closest to the PC board surface) includes the
USB DCP controller while the upper port just delivers power.
Charge your device! Take note that each device has its own “charge controller circuitry” that might limit the charging current if the voltage on the load goes below a certain level. Shown below is the maximum charging current on P2 lower port that CN0509 can provide given that the output voltage to the load is greater than 5V.
Schematic, PCB Layout, Bill of Materials