EVAL-CN0509-EBZ Overview
CN0509 is a wide input range (5V to 100V) USB charger capable of providing up to 2A at 5V from a wide range of DC sources including solar panels, fully charged or half-discharged car batteries, -48V telecom backup supplies, random stacks of alkaline cells, treadmill motors hacked to run as generators, wind turbines, etc. using the combination of wide input LTC7103 buck converter and an isolated flyback converter LT8302. The circuit accepts DC voltage from 5V to 100V and produce an isolated 5V supply via a standard USB connector. The outer case of many cell phones and other portable electronics are often electrically connected to USB ground. As such, isolation is necessary in situations in which the power source’s relationship to Earth ground is unknown.
The circuit will survive up to 100V reverse connection to a power source with a green LED indicating correct input polarity and red led otherwise.
Features
Allows wide input range of 5V to 100V
Provides isolated and regulated 5V output
Provides up to 2A output current
Two
USB output ports for convenience
Documents Needed
Equipment Required
Block Assignments
Connector P1 is the screw terminal block for input supply
Connector
P2 is the
USB output connectors for the load
Test point
TP1 is the LTC7103 output voltage programming pin VPRG2. This pin is left floating to program the chip to have 12
V fixed output voltage.
Test point PGOOD is the LTC7103 Open-Drain Power Good Output pin
Test point CLKOUT is the LTC7103 Output clock signal pin
Test point IMON is the LTC7103 Average Output Current Monitor pin. This pin generates a voltage between 0.4V and 1.3V that corresponds to an average output current between 0A and 2.5A.
Test point ICTRL is the LTC7103 ICTRL pin that programs the average output current in constant current mode. This is left floating to set the average output current to 2.5A and the peak current limit to 3.7A
Test point TP6 is the voltage input to the LTC7103
Test point 12V is the 12V output voltage of the LTC7103
Test point GND1 is the ground relative to input supply
Test point
VBUS is the
USB VBUS voltage which typically carries 5V
Test point
D- is the
USB data+ signal
Test point
D+ is the
USB data- signal
Test point GND is the isolated ground relative to output
USB Output Connectors
Test setup
Connect the input DC supply to P1 on
EVAL-CN0509-EBZ. Ensure safe connection because it may deal with input voltages up to 100
V.
Running the System
Turn on DC supply.
The circuit will determine if input connection is in correct polarity through lighting DS1 or DS2.
If DS1 (green LED) turns on, this means correct polarity on the input and circuit delivers up to 10W on P2
USB output ports.
If DS2 (red LED) illuminates, turn off the input supply, disconnect the power inputs, swap the power leads, and reconnect the supply outputs to P1.
Connect the
USB multimeter tester to the lower
USB port on the EVAL-CN0509-EBZ.
Connect a fast charge capable device to the
USB multimeter tester using the charging cable of the device.
You can check the
USB multimeter tester and see if the device is pulling more than 500
mA but less than 2 A.
Connect the
USB multimeter tester to the upper
USB port on the EVAL-CN0509-EBZ.
You can check the
USB multimeter tester and see if the device is pulling approximately 500
mA.
Take note that each device has its own “charge controller circuitry” that might limit the charging current if the voltage on the load goes below a certain level. Shown below is the maximum charging current on P2 lower port that CN0509 can provide given that the output voltage to the load is greater than 5V.
Schematic, PCB Layout, Bill of Materials