This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0508 [27 Jan 2023 09:03] – Replaced the obsolete Kuiper Linux page link Joyce Velasco | resources:eval:user-guides:circuits-from-the-lab:cn0508 [04 Apr 2023 13:54] – update Trisha Cabildo | ||
---|---|---|---|
Line 35: | Line 35: | ||
* 75W to 120W offline power supply or b | * 75W to 120W offline power supply or b | ||
* Bench power supply (Globtek TR9CR3000T00-IM(R6B)) | * Bench power supply (Globtek TR9CR3000T00-IM(R6B)) | ||
- | * Various power resistors, dummy load, or test circuit | + | * Various power resistors, dummy load, or test circuits |
* 40-pin ribbon cable (optional) | * 40-pin ribbon cable (optional) | ||
* Monitor with HDMI display | * Monitor with HDMI display | ||
Line 59: | Line 59: | ||
</ | </ | ||
\\ | \\ | ||
- | * Connector **P1** is the screw terminal block for input supply | + | * Connector **P1** is the screw terminal block for the input supply |
* Connector **P2** is the 5.5mm x 2.5mm barrel jack connector for input supply | * Connector **P2** is the 5.5mm x 2.5mm barrel jack connector for input supply | ||
* Connector **P3** is the 40-pin connector for Raspberry Pi | * Connector **P3** is the 40-pin connector for Raspberry Pi | ||
Line 65: | Line 65: | ||
* Connector **P8** is the ground output jack of the bench supply | * Connector **P8** is the ground output jack of the bench supply | ||
* Potentiometer **R43** is the manual control of output voltage | * Potentiometer **R43** is the manual control of output voltage | ||
- | * Potentiometer **R14** is the manual control of output current limit | + | * Potentiometer **R14** is the manual control of the output current limit |
* Header **P12** contains the output signal for the fan control | * Header **P12** contains the output signal for the fan control | ||
\\ | \\ | ||
Line 75: | Line 75: | ||
</ | </ | ||
- Set solder jumpers for the desired settings. | - Set solder jumpers for the desired settings. | ||
- | - Proceed with the [[/ | + | - Proceed with the [[/ |
- | - Burn the SD card with the latest ADI Kuiper Linux image. Insert the flashed SD card on designated slot on Raspberry Pi. | + | - Burn the SD card with the latest ADI Kuiper Linux image. Insert the flashed SD card into designated slot on Raspberry Pi. |
- Turn on the input supply. Wait for the Raspberry Pi to boot up. | - Turn on the input supply. Wait for the Raspberry Pi to boot up. | ||
- | - Open terminal and configure the device tree overlay file. See [[/ | + | - Open the terminal and configure the device tree overlay file. See [[/ |
- Wait for the Raspberry Pi to boot up again. Open the IIO Oscilloscope and select the CN0508 tab. | - Wait for the Raspberry Pi to boot up again. Open the IIO Oscilloscope and select the CN0508 tab. | ||
- | - You may change output voltage and view the measurements on other parameters such as current, temperature and potentiometer knob readings. | + | - You may change output voltage and view the measurements on other parameters such as current, temperature, and potentiometer knob readings. |
- For manual control, rotate the knob of R43. The output voltage of the system follows the lower voltage between the output voltages of the potentiometer and the DAC. | - For manual control, rotate the knob of R43. The output voltage of the system follows the lower voltage between the output voltages of the potentiometer and the DAC. | ||
- | - You may also change the current limit of the system by turning knob of R14. | + | - You may also change the current limit of the system by turning |
- The Raspberry Pi must be powered down properly in order to prevent eventual corruption of the SD card. This can be done by pressing S1 and waiting for the green heartbeat LED to stop blinking. At that point, power is safe to be removed. | - The Raspberry Pi must be powered down properly in order to prevent eventual corruption of the SD card. This can be done by pressing S1 and waiting for the green heartbeat LED to stop blinking. At that point, power is safe to be removed. | ||
- | - Alternatively, | + | - Alternatively, |
\\ | \\ | ||
Line 140: | Line 140: | ||
\\ | \\ | ||
===EEPROM_ID: | ===EEPROM_ID: | ||
- | EEPROM_ID sets the EEPROM I2C address. It consists of P4, P5 and P6 solder jumpers connected respectively to A2, A1 and A0 address selection pins of U7. The default address configuration is “111”. This EEPROM I2C address is configurable from 001 to 111. It cannot be set to " | + | EEPROM_ID sets the EEPROM I2C address. It consists of P4, P5, and P6 solder jumpers connected respectively to A2, A1, and A0 address selection pins of U7. The default address configuration is “111”. This EEPROM I2C address is configurable from 001 to 111. It cannot be set to " |
^ | ^ | ||
| | | | ||
Line 158: | Line 158: | ||
//<fc # | //<fc # | ||
</ | </ | ||
- | Connect | + | Connect |
{{ : | {{ : | ||
<wrap center 50%> | <wrap center 50%> | ||
Line 170: | Line 170: | ||
\\ | \\ | ||
==== Input Supply ==== | ==== Input Supply ==== | ||
- | Power to the EVAL-CN0508-RPIZ can be connected through P1 or P2. P1 is a two terminal screw terminal while P2 is a 5.5mm x 2.5mm center positive barrel jack. Please choose only one input between the two. Maximum | + | Power to the EVAL-CN0508-RPIZ can be connected through P1 or P2. P1 is a two-terminal screw terminal while P2 is a 5.5mm x 2.5mm center positive barrel jack. Please choose only one input between the two. The maximum |
{{ : | {{ : | ||
<wrap center 60%> | <wrap center 60%> | ||
Line 177: | Line 177: | ||
\\ | \\ | ||
==== Output connections ==== | ==== Output connections ==== | ||
- | You can connect a resistive load/test circuit, an electronic load or multimeter at the output banana jacks P7 and P8. P7 is the positive polarity and P8 is the ground. Also, make sure you are aware of your load's power consumption to avoid overheating. | + | You can connect a resistive load/test circuit, an electronic load, or multimeter at the output banana jacks P7 and P8. P7 is the positive polarity and P8 is the ground. Also, make sure you are aware of your load's power consumption to avoid overheating. |
{{ : | {{ : | ||
<wrap center 50%> | <wrap center 50%> | ||
Line 198: | Line 198: | ||
===== Software Setup ===== | ===== Software Setup ===== | ||
==== Loading CN0508 Image on SD Card ==== | ==== Loading CN0508 Image on SD Card ==== | ||
- | In order to control the CN0508 from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, | + | In order to control the CN0508 from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, |
\\ | \\ | ||
Write the image and follow the system configuration procedure. | Write the image and follow the system configuration procedure. | ||
==== Configuring the SD Card ==== | ==== Configuring the SD Card ==== | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [: |
< | < | ||
Line 218: | Line 218: | ||
\\ \\ <WRAP center round tip 50%>Make sure to have the latest version of IIO Oscilloscope. Complete instructions and update scripts are found at **[[resources: | \\ \\ <WRAP center round tip 50%>Make sure to have the latest version of IIO Oscilloscope. Complete instructions and update scripts are found at **[[resources: | ||
==== Electronic Control and Diagnostics via IIO Oscilloscope Plugin ==== | ==== Electronic Control and Diagnostics via IIO Oscilloscope Plugin ==== | ||
- | EVAL-CN0508-RPIZ allows electronic control of the output voltage and measurement display of other system diagnostics such as voltage, current and temperature through the [[ADI> | + | EVAL-CN0508-RPIZ allows electronic control of the output voltage and measurement display of other system diagnostics such as voltage, current, and temperature through the [[ADI> |
{{ : | {{ : | ||
<wrap center 50%> | <wrap center 50%> | ||
Line 227: | Line 227: | ||
Setting this value from 0 to 65535 will vary the output voltage of the DAC. | Setting this value from 0 to 65535 will vary the output voltage of the DAC. | ||
=== Temperature Monitor === | === Temperature Monitor === | ||
- | This shows the temperature readings of the two [[ADI> | + | This shows the temperature readings of the two [[ADI> |
=== DC Supply === | === DC Supply === | ||
- | This presents the output voltage and output current of the EVAL-CN0508-RPIZ. | + | This presents the output voltage and output current of the EVAL-CN0508-RPIZ. |
=== Potentiometers === | === Potentiometers === | ||
This shows the position of the voltage and current limit potentiometers. An indicator flag is raised if the output current reaches 95% of the current limit setpoint or if the measured output voltage falls more than 0.5V below the lower of (DAC setpoint, potentiometer setpoint). | This shows the position of the voltage and current limit potentiometers. An indicator flag is raised if the output current reaches 95% of the current limit setpoint or if the measured output voltage falls more than 0.5V below the lower of (DAC setpoint, potentiometer setpoint). |