This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0357 [07 Aug 2014 17:59] – [Installing the Software] James Fitzgerald | resources:eval:user-guides:circuits-from-the-lab:cn0357 [15 Aug 2022 03:59] (current) – Allan Uy | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== CN0357 Software User Guide====== | ||
+ | ===== Overview ===== | ||
+ | [[adi> | ||
+ | Electrochemical sensors offer several advantages for instruments that detect or measure the concentration of many toxic gases. Most sensors are gas specific and have usable resolutions under one part per million (ppm) of gas concentration. | ||
+ | The circuit shown in below uses the [[adi> | ||
+ | The [[adi> | ||
+ | For applications where measuring fractions of ppm gas concentration is important, using the [[adi> | ||
+ | |||
+ | This user guide will discuss how to use the evaluation software to collect data from the [[adi> | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Required Equipment ===== | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[https:// | ||
+ | * PC with the following //Minimum Requirements// | ||
+ | * Windows XP Service Pack 2 (32-bit) | ||
+ | * USB type A Port | ||
+ | * Processor rated at 1GHz or faster | ||
+ | * 512 MB RAM and 500 MB available hard disk space | ||
+ | * USB type A to USB type mini-B cable | ||
+ | ===== General Setup ===== | ||
+ | * The [[adi> | ||
+ | * The [[adi> | ||
+ | * The [[adi> | ||
+ | * The [[adi> | ||
+ | {{ : | ||
+ | ---- | ||
+ | ===== Installing the Software ===== | ||
+ | - Extract the file **CN0357_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Click **Next** to view the installation review page\\ \\ {{: | ||
+ | - Click **Next** to start the installation\\ \\ {{: | ||
+ | - Upon completion of the installation of the **CN-0357 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | ||
+ | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | ||
+ | |||
+ | ---- | ||
+ | ===== Connecting the Hardware ===== | ||
+ | - Connect the [[adi> | ||
+ | - Connect the [[adi> | ||
+ | - Connect the USB cable to **J1** of the [[adi> | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Using the Evaluation Software ===== | ||
+ | ==== Software Control and Indicator Descriptions ==== | ||
+ | {{: | ||
+ | ---- | ||
+ | {{: | ||
+ | -**Run Button** | ||
+ | * When this button is pressed, the SDP-B Board will collect concentration data and present the acquisitions in the chart. | ||
+ | -**Stop Button** | ||
+ | * When this button is pressed, the software stop collecting data from the CN0357 Board | ||
+ | -**Save Data Button** | ||
+ | * When this button is pressed, the software will save the data collected to a tab delimited ASCII spreadsheet file. | ||
+ | -**Clear Data Button** | ||
+ | * When this button is pressed, the software will clear all data collected from the chart history. | ||
+ | -**Control Tabs** | ||
+ | * __Measure Concentration__ - Clicking this tab brings the data collection chart to the front. | ||
+ | * __Configure System__ - Clicking this tab brings the system configuration settings to the front. | ||
+ | * __SDP Board Information__ - Clicking this tab brings the SDP Board Information to the front. | ||
+ | -**Concentration Numerical Indicator** | ||
+ | * This indicator displays the current concentration measured by the system. | ||
+ | -**Sensor Type Drop-down Menu** | ||
+ | * __Oxidation (sink)__ - Select this option if the sensor sinks current | ||
+ | * __Reduction (source)__ - Select this option if the sensor sources current. | ||
+ | -**Max Sensor Sensitivity Numerical Control** | ||
+ | * The maximum amount of current in nanoamps (nA) the sensor will sink/source per part per million (ppm). | ||
+ | * This control influences the feedback resistance set by the Rheostat ([[adi> | ||
+ | -**Typical Sensor Sensitivity Drop-down Menu** | ||
+ | * The typical amount of current in nanoamps (nA) the sensor will sink/source per part per million (ppm). | ||
+ | * This control influences the size of the LSB in terms of ppm/mV and mV/ppm. | ||
+ | -**Sensor Range Numerical Control** | ||
+ | * The maximum concentration the sensor can measure in parts per million. | ||
+ | -**Feedback Resistance Numerical Indicator** | ||
+ | * The feedback resistance of the transimpedance amplifier on the **CN0357 Board** ([[adi> | ||
+ | * This can be set by the Rheostat ([[adi> | ||
+ | -**ppm/mV Numerical Indicator** | ||
+ | * Parts per million concentration per millavolt | ||
+ | -**mV/ppm Numerical Indicator** | ||
+ | * millavolts per parts per million concentration | ||
+ | -**ADC Conversion Numerical Indicator** | ||
+ | * The converted voltage seen by the ADC ([[adi> | ||
+ | -**Chart Controls** | ||
+ | * These controls allow the user to zoom-in, zoom-out, and pan through the data collected. | ||
+ | -**System Status String Indicator** | ||
+ | * This indicator displays a message to the user detailing the current state of the software. | ||
+ | -**System Status LED Indicator** | ||
+ | * This indicator displays the current state of the software in the form of an LED. There are three status LED colors.\\ {{: | ||
+ | -**Buffer Mode Radio Buttons** | ||
+ | * __Buffered Mode__ - This allows the user to place source impedance on the front end without contributing to gain errors to the system. | ||
+ | * __Unbuffered Mode__ - This disables the buffers, lowering the power consumption of the device.\\ \\ <WRAP center round info 60%> \\ Enabling the buffers also reduces the **Analog Input Range** of the ADC</ | ||
+ | -**Mode Register Numerical Indicator** | ||
+ | * This register is used to configure the ADC for range, enable or disable the buffer, or place the device into power-down mode. | ||
+ | * The **Register Bit Designations** can be found on Page 11 of the [[adi> | ||
+ | -**Filter Register Numerical Indicator** | ||
+ | * This register is used to set the output word rate. | ||
+ | * Table 12 in the [[adi> | ||
+ | -**Reset ADC Button** | ||
+ | * The serial interface can be reset by writing a series of 1s on the DIN input. | ||
+ | * Reset returns the interface to the state in which it is expecting a write to the communications register. | ||
+ | * This operation resets the contents of all registers to their power-on values. | ||
+ | -**Feedback Selector Radio Buttons** | ||
+ | * __Rheostat__ - Selecting this option uses the Rheostat for the feedback resistance of the transimpedance amplifier and disables the **Fixed Resistor Numerical Control**. | ||
+ | * __Fixed Resistor__ - Selecting this option uses a fixed-resistor for the feedback resistance of the transimpedance amplifier and disables the **RDAC Value Numerical Indicator**, | ||
+ | -**Fixed Resistor Numerical Control** | ||
+ | * Input the value of the resistor populated at **R7** if not using the Rheostat | ||
+ | -**RDAC Value Numerical Indicator** | ||
+ | * The value transmitted to the RDAC register of the Rheostat in hexadecimal format. | ||
+ | -**Rheostat Resistance Numerical Indicator** | ||
+ | * The equivalent resistance of the Rheostat. | ||
+ | -**Program Rheostat Button** | ||
+ | * Load the current RDAC value to the 50-TP Memory Block of the Digital Rheostat.\\ \\ <WRAP center round important 60%>\\ Programming the current RDAC value to 50-TP can only occur 50 times.</ | ||
+ | |||
+ | |||
+ | ---- | ||
+ | ==== Running the System ==== | ||
+ | - Open the **CN0357.exe** application from the default installation location. | ||
+ | - The software will connect to the board automatically. | ||
+ | - Click the **Run Button** | ||
+ | - Click the **Stop Button** when acquisition is complete. | ||
+ | ==== Saving Data to a Spreadsheet File ==== | ||
+ | - Click the **Save Data Button**. | ||
+ | - Browse to the directory location where the spreadsheet file is to be saved. | ||
+ | - Name the file. | ||
+ | - Click the **OK Button**. | ||
+ | <WRAP center round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs</ | ||
+ | ===== Downloads ===== | ||
+ | {{: | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |