This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0355 [03 Jan 2021 22:03] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0355 [29 Jul 2021 07:47] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 143: | Line 143: | ||
**Step 8** - Set the temperature chamber at temp 2.\\ | **Step 8** - Set the temperature chamber at temp 2.\\ | ||
**Step 9** - Do Step 3 to Step 7 under column Temperature 2.\\ | **Step 9** - Do Step 3 to Step 7 under column Temperature 2.\\ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |