This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0355 [05 May 2015 20:13] – formatting Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:cn0355 [29 Jul 2021 07:47] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]] Evaluation Board |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board |
- | * [[http:// | + | * [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] Evaluation Board |
* [[ftp:// | * [[ftp:// | ||
* +6V DC power supply | * +6V DC power supply | ||
* USB Type-A plug to USB Mini-B plug cable | * USB Type-A plug to USB Mini-B plug cable | ||
* Honeywell (Mfg #: | * Honeywell (Mfg #: | ||
- | * 2/3/4-Wire RTD sensor\\ \\ <WRAP left tip round box 60%> | + | * 2/3/4-Wire RTD sensor\\ \\ <WRAP left tip round box 60%> |
===== Minimum PC/System Requirements ===== | ===== Minimum PC/System Requirements ===== | ||
Line 42: | Line 42: | ||
\\ \\ {{: | \\ \\ {{: | ||
- | - Plug the mini end of the USB cable into connector J1 of the [[http:// | + | - Plug the mini end of the USB cable into connector J1 of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and connect the other end of the USB cable into the Laptop or PC. |
- | - Connect the 120-pin connector of the [[http:// | + | - Connect the 120-pin connector of the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] circuit board to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board. |
- | - Populate a jumper across JP1 to give +3.3V voltage out in PMOD terminal as seen in the label found in [[http:// | + | - Populate a jumper across JP1 to give +3.3V voltage out in PMOD terminal as seen in the label found in [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. |
- | - Connect the 12-pin right angle male pin header of [[http:// | + | - Connect the 12-pin right angle male pin header of [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]] to the 12-pin right angle female pin header of [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]]. |
- | - Connect the +6V DC power supply or an equivalent power supply to JP1, the barrel jack wallwart terminal of the [[http:// | + | - Connect the +6V DC power supply or an equivalent power supply to JP1, the barrel jack wallwart terminal of the [[adi>SDP-PMD-IB1Z|SDP-PMD-IB1Z]] interposer board. |
- | - Connect the RTD sensor in P2 of [[http:// | + | - Connect the RTD sensor in P2 of [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]]. |
- | - Set P3 and P4 jumper configuration according to the type of RTD sensor that will be used to evaluate the sensor\\ \\ <WRAP left tip round box 60%> | + | - Set P3 and P4 jumper configuration according to the type of RTD sensor that will be used to evaluate the sensor\\ \\ <WRAP left tip round box 60%> |
- | - Connect the Pressure transducer in P1 of [[http:// | + | - Connect the Pressure transducer in P1 of [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]]. |
- | - Set P5, P6 and P7 jumper configuration to the desired Bridge type transducer voltage drive\\ \\ <WRAP left tip round box 60%> | + | - Set P5, P6 and P7 jumper configuration to the desired Bridge type transducer voltage drive\\ \\ <WRAP left tip round box 60%> |
- | - Plug in the wall wart and connect it to connector P8 of the [[http:// | + | - Plug in the wall wart and connect it to connector P8 of the [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]]. |
---- | ---- | ||
Line 59: | Line 59: | ||
\\ \\ | \\ \\ | ||
{{: | {{: | ||
- | * Interface the RTD and Bridge type transducer to the [[http:// | + | * Interface the RTD and Bridge type transducer to the [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]] as shown in the diagram above. |
---- | ---- | ||
Line 115: | Line 115: | ||
===== CALIBRATION PROCEDURE ===== | ===== CALIBRATION PROCEDURE ===== | ||
- | This section explains the steps required to properly calibrate the [[http:// | + | This section explains the steps required to properly calibrate the [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]]. |
\\ \\ <WRAP left tip round box 100%> | \\ \\ <WRAP left tip round box 100%> | ||
**Pre-Calibration Note**: | **Pre-Calibration Note**: | ||
Line 122: | Line 122: | ||
* 4 – point calibration requires an oven with calibrated temperature sensor and calibrated pressure source. | * 4 – point calibration requires an oven with calibrated temperature sensor and calibrated pressure source. | ||
* Dwell time of the temperature depends on the equipment that is being used to calibrate the system. | * Dwell time of the temperature depends on the equipment that is being used to calibrate the system. | ||
- | * The voltage drive set in the evaluation software should correspond to the configured jumper set up found in [[http:// | + | * The voltage drive set in the evaluation software should correspond to the configured jumper set up found in [[adi>EVAL-CN0355-PMDZ|EVAL-CN0355-PMDZ]]. |
* All units is in PSI | * All units is in PSI | ||
* Sensitivity is usually found in the datasheet of the transducer to be used. | * Sensitivity is usually found in the datasheet of the transducer to be used. | ||
Line 143: | Line 143: | ||
**Step 8** - Set the temperature chamber at temp 2.\\ | **Step 8** - Set the temperature chamber at temp 2.\\ | ||
**Step 9** - Do Step 3 to Step 7 under column Temperature 2.\\ | **Step 9** - Do Step 3 to Step 7 under column Temperature 2.\\ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |