This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0354 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0354 [29 Jul 2021 07:44] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 16: | Line 16: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[adi>en/ | + | * [[adi> |
- | * [[adi>EVAL-CN0354-PMDZ|EVAL-CN0354-PMDZ]] Evaluation Board (**CN-0354 Board**) | + | * [[adi> |
* [[adi> | * [[adi> | ||
* [[ftp:// | * [[ftp:// | ||
Line 30: | Line 30: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[adi>EVAL-CN0354-PMDZ|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** connects to the [[adi>en/ | + | * The [[adi> |
- | * The [[adi> | + | * The [[adi> |
* The [[adi> | * The [[adi> | ||
- | * The reference thermocouple connects to the [[adi>EVAL-CN0354-PMDZ|EVAL-CN0354-PMDZ]] **(CN-0354 Board)** via the thermocouple connector at **+TREF-** and the tip of the thermocouple must be placed as close to **U4** as possible. | + | * The reference thermocouple connects to the [[adi> |
* The thermocouples may be placed at any of the four channels of **P2**. \\ \\ <WRAP left tip round box 60%> | * The thermocouples may be placed at any of the four channels of **P2**. \\ \\ <WRAP left tip round box 60%> | ||
**NOTE:** If not all four thermocouple channels will be used, it is recommended to short out the positive and negative terminal of any unused channel at the isothermal block **P2** in order to avoid the **AD8495** from railing. | **NOTE:** If not all four thermocouple channels will be used, it is recommended to short out the positive and negative terminal of any unused channel at the isothermal block **P2** in order to avoid the **AD8495** from railing. | ||
Line 108: | Line 108: | ||
<WRAP left round info 60%>\\ The data is exported to an Excel spreadsheet file with columns labeled accordingly. </ | <WRAP left round info 60%>\\ The data is exported to an Excel spreadsheet file with columns labeled accordingly. </ | ||
+ | \\ \\ \\ \\ \\ \\ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||