Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0272 [29 Nov 2012 20:28] – [Establishing a USB Connection Link] James Fitzgeraldresources:eval:user-guides:circuits-from-the-lab:cn0272 [29 Jul 2021 06:04] (current) – Hardware Registration Harvey John De Chavez
Line 1: Line 1:
-====== CN0272 Software User Guide======+====== CN-0272 Software User Guide======
 ===== Overview ===== ===== Overview =====
-[[http://www.analog.com/CN0272|CN0272]] is a high-speed photodiode signal conditioning circuit with dark current compensation. The system converts current from a high-speed silicon PIN photodiode and drives the inputs of a 20 MSPS ADC. This combination of parts offers spectral sensitivity from 400 nm to 1050 nm with 49 nA of photocurrent sensitivity, a dynamic range of 91 dB and 2 MHz of bandwidth. The signal conditioning circuitry of the system consumes only 40 mA of current from the ±5 V supplies making this configuration suitable for portable high-speed high-resolution light intensity applications such as pulse oximetry.+[[adi>CN0272|CN-0272]] is a high-speed photodiode signal conditioning circuit with dark current compensation. The system converts current from a high-speed silicon PIN photodiode and drives the inputs of a 20 MSPS ADC. This combination of parts offers spectral sensitivity from 400 nm to 1050 nm with 49 nA of photocurrent sensitivity, a dynamic range of 91 dB and 2 MHz of bandwidth. The signal conditioning circuitry of the system consumes only 40 mA of current from the ±5 V supplies making this configuration suitable for portable high-speed high-resolution light intensity applications such as pulse oximetry.
  
 Other suitable applications for this circuit would be as an analog opto-isolator. It can also be adapted to applications that require larger bandwidth and less resolution such as adaptive speed control systems.  Other suitable applications for this circuit would be as an analog opto-isolator. It can also be adapted to applications that require larger bandwidth and less resolution such as adaptive speed control systems. 
  
-This user guide will discuss how to use the evaluation software to collect data from the [[http://www.analog.com/EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Daughter Board+This user guide will discuss how to use the evaluation software to collect data from the [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Daughter Board
  
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-simplified_schematic.png?nolink&|}} {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-simplified_schematic.png?nolink&|}}
 ===== Required Equipment ===== ===== Required Equipment =====
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) +  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) 
-  * [[http://www.analog.com/EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Daughter Board (**CN0272 Board**) +  * [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Daughter Board (**CN0272 Board**) 
-  * [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] Power Supply or equivalent +6V power supply+  * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] Power Supply or equivalent +6V power supply
   * [[ftp://ftp.analog.com/pub/cftl/CN0272/|CN0272 SDP Evaluation Software]]   * [[ftp://ftp.analog.com/pub/cftl/CN0272/|CN0272 SDP Evaluation Software]]
     * (supplied with provided CD in kit)     * (supplied with provided CD in kit)
Line 25: Line 25:
  
 ===== General Setup ===== ===== General Setup =====
-  * The [[http://www.analog.com/EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Board connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] SDP-B Board via the 120-Pin connector +  * The [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Board connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] SDP-B Board via the 120-Pin connector 
-  * The [[http://www.analog.com/EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] DC power supply powers the [[http://www.analog.com/EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Board via the DC barrel jack +  * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] DC power supply powers the [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Board via the DC barrel jack 
-  * The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] SDP-B Board connects to the PC via the USB cable. +  * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] SDP-B Board connects to the PC via the USB cable.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-test_setup.png?nolink&|}} 
 + 
 +----
  
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-test_setup.png?nolink&|}} 
 ===== Installing the Software ===== ===== Installing the Software =====
-  - Extract the file **CN0272 SDP Eval Software.zip** and open the file **setup.exe**.<html><br><br></html><WRAP left round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0272/|CN0272 SDP Evaluation Software]] to the default directory path **C:\Program Files\Analog Devices\CN0272\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP><html><br><br><br><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install1.png?nolink&|}} +  - Extract the file **CN0272 SDP Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0272/|CN0272 SDP Evaluation Software]] to the default directory path **C:\Program Files\Analog Devices\CN0272\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP>\\ \\ \\ \\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install1.png?nolink&|}} 
-  - Click **Next** to view the installation review page<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install2.png?nolink&|}}<html><br><br></html> +  - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install2.png?nolink&|}}\\ \\  
-  - Click **Next** to start the installation<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install3.png?nolink&|}}<html><br><br></html> +  - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install3.png?nolink&|}}\\ \\  
-  - Upon completion of the installation of the **CN0272 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute.<html><br><br></html><WRAP left round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP><html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install4.png?nolink&|}}<html><br><br></html> +  - Upon completion of the installation of the **CN0272 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you close all other applications before clicking **“Next”**.  This will make it possible to update relevant system files without having to reboot your computer.</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install4.png?nolink&|}}\\ \\  
-  - Press **“Next”** to set the installation location for the **SDP Drivers**.<html><br><br></html><WRAP left round important 50%>It is recommended that you install the drivers to the default directory path <html><br></html>**C:\Program Files\Analog Devices\SDP\Drivers**</WRAP><html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install5.png?nolink&|}} +  - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C:\Program Files\Analog Devices\SDP\Drivers**</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install5.png?nolink&|}} 
-  - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software.  Click **"Finish"** when done.<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install6.png?nolink&|}}+  - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software.  Click **"Finish"** when done.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-install6.png?nolink&|}} 
 + 
 +---- 
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
-  - Connect **J4** of the [[http://www.analog.com/EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] (CN0272 Board) to **CON A** of the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] (SDP-B Board)<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware.png?600|}}<html><br><br></html>+  - Connect **J4** of the [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] (CN0272 Board) to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] (SDP-B Board)\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware.png?600|}}\\ \\ 
   - Select the voltage bias of the photodiode.     - Select the voltage bias of the photodiode.  
-    - Select the onboard -5V bias by populating **JP1** with a shorting jumper as depicted below<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware2.png?600|}}<html><br><br></html> +    - Select the onboard -5V bias by populating **JP1** with a shorting jumper as depicted below\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware2.png?600|}}\\ \\  
-    - Select an external voltage bias by populatign **JP1** with a shorting jumper as depicted below.  <WRAP left round important box 60%>**NOTE:** When using an external voltage to bias the photodiode, a SMB connector also must be connected to **J2**.  The other end of this cable must connect to a voltage supply **≤ 15V**.</WRAP><html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware3.png?600|}}<html><br><br></html> +    - Select an external voltage bias by populatign **JP1** with a shorting jumper as depicted below.  <WRAP left round important box 60%>**NOTE:** When using an external voltage to bias the photodiode, a SMB connector also must be connected to **J2**.  The other end of this cable must connect to a voltage supply **≤ 15V**.</WRAP>\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware3.png?600|}}\\ \\  
-  - Connect a 6V supply to the Barrel Jack or the Screw Terminal on the CN0272 Board<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware4.png?600|}}<html><br><br></html> +  - Connect a 6V supply to the Barrel Jack or the Screw Terminal on the CN0272 Board\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware4.png?600|}}\\ \\  
-  - Connect the USB Cable to the SDP-B Board and the PC<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware5.png?600|}}<html><br><br></html>+  - Connect the USB Cable to the SDP-B Board and the PC\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-hardware5.png?600|}}\\ \\  
 + 
 +---- 
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
 ==== Software Control and Indicator Descriptions ==== ==== Software Control and Indicator Descriptions ====
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software.png?|}} {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software.png?|}}
-  -<html><a id="1"><b>SDP Connector Dropdown Menu</b></a></html>+  -**SDP Connector Dropdown Menu**
     * This control will select which connector (on the SDP-B Board) the CN0272 Board is currently connected to.  The options are "connectorA" or "connectorB" The connector to be used must be selected before clicking the **Connect to SDP-B Board Button**     * This control will select which connector (on the SDP-B Board) the CN0272 Board is currently connected to.  The options are "connectorA" or "connectorB" The connector to be used must be selected before clicking the **Connect to SDP-B Board Button**
   -**Connect to SDP-B Board Button**   -**Connect to SDP-B Board Button**
-    * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board.  A connection to the SDP-B Board must be made to use the software. This button is also used in conjuction with the **SDP Connector Dropdown Menu**.   +    * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board.  A connection to the SDP-B Board must be made to use the software. This button is also used in conjunction with the **SDP Connector Dropdown Menu**.   
   -**Take Snapshot(s) Button**   -**Take Snapshot(s) Button**
-    * When this button is pressed, the SDP-B Board will collect a single Snapshot or a collection of Snapshots depending on the **Acquisition Mode** setting.+    * When this button is pressed, the SDP-B Board will collect a single Snapshot or a collection of Snapshots depending on the **Acquisition Mode** setting.\\ \\ <WRAP left round info 60%>**Snapshot** - a collection of analog to digital conversions, sampled at 20MSPS, acquired by the SDP-B Board and displayed in the graph.</WRAP>\\ \\ \\ \\ \\ \\
   -**Save Snapshot(s) Button**   -**Save Snapshot(s) Button**
     * When this button is pressed, the software will save a single Snapshot or a collection of Snapshots to a tab delimited ASCII spreadsheet file.     * When this button is pressed, the software will save a single Snapshot or a collection of Snapshots to a tab delimited ASCII spreadsheet file.
Line 84: Line 91:
     * This indicator displays a message to the user detailing the current state of the software.     * This indicator displays a message to the user detailing the current state of the software.
   -**System Status LED Indicator**   -**System Status LED Indicator**
-    * This indicator displays the current state of the software in the form of an LED.  There are four status LED colors.<html><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-inactive.png?nolink&|}}Inactive<html><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-busy.png?nolink&|}}Busy<html><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-powerdown.png?nolink&|}}ADC in Power-Down<html><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-error.png?nolink&|}}Error+    * This indicator displays the current state of the software in the form of an LED.  There are four status LED colors.\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-inactive.png?nolink&|}}Inactive\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-busy.png?nolink&|}}Busy\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-powerdown.png?nolink&|}}ADC in Power-Down\\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-error.png?nolink&|}}Error 
 + 
 +---- 
 ==== Establishing a USB Connection Link ==== ==== Establishing a USB Connection Link ====
   - Follow the instructions to properly install the software and connect the hardware as described in the previous sections.   - Follow the instructions to properly install the software and connect the hardware as described in the previous sections.
-  - Load the **CN0272.exe** found at the installation location.<html><br><br></html><WRAP left round box 50%>**NOTE:** If the software was installed to the default location it will be found at <html><br></html>**C:\Program Files\Analog Devices\CN0272\CN0272.exe**</WRAP><html><br><br><br><br></html> +  - Open the file named **CN0272.exe** in the installation directory.\\ \\ <WRAP left info round box 60%>**NOTE:** If the software was installed to the default location it will be found at \\ **C:\Program Files\Analog Devices\CN0272\CN0272.exe**</WRAP>\\ \\ \\ \\ \\ \\ 
-  - Select the connector to use from the <html><a href="#1"><b>SDP Connector Dropdown Menu</b></a></html>+  - Select the connector to use from the **SDP Connector Dropdown Menu**
-  - Click the **Connect to SDP-B Board Button**.  A window with a progress bar will load.<html><br><br></html>{{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-wait.png?nolink&|}}<html><br><br></html>+  - Click the **Connect to SDP-B Board Button**.  A window with a progress bar will load.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-wait.png?nolink&|}}\\ \\ 
   - Upon success, the **System Status String Indicator** will display __SDP-B Ready to Take Snapshot(s)__   - Upon success, the **System Status String Indicator** will display __SDP-B Ready to Take Snapshot(s)__
 ==== Capturing a Single Snapshot ==== ==== Capturing a Single Snapshot ====
 +  - **Establish a USB Connection Link**.
 +  - Select __Single Snapshot__ as the **Acquisition Mode**
 +  - Set the number of conversions in the snapshot
 +  - Click the **Take Snapshot(s) Button**
 ==== Capturing Multiple Snapshots ==== ==== Capturing Multiple Snapshots ====
 +  - **Establish a USB Connection Link**.
 +  - Select __Multiple Snapshots__ as the **Acquisition Mode**.
 +  - Set the number of conversions in each snapshot.
 +  - Set the number of snapshots to take.
 +  - Set the snapshot delay.
 +  - Click the **Take Snapshot(s) Button**.
 ==== Displaying a Specific Snapshot ==== ==== Displaying a Specific Snapshot ====
 +  - **Establish a USB Connection Link**.
 +  - Select __Multiple Snapshots__ as the **Acquisition Mode**.
 +  - Set the number of conversions in each snapshot.
 +  - Set the number of snapshots to take.
 +  - Set the snapshot delay.
 +  - Click the **Take Snapshot(s) Button**.
 +  - Type the number of the snapshot of interest into the **Snapshot Displayed Numerical Control**
 ==== Saving a Single Snapshot to a Spreadsheet File ==== ==== Saving a Single Snapshot to a Spreadsheet File ====
-==== Saving Multiple Snapshots to Spreadsheet File ==== +  - **Establish USB Connection Link**. 
-==== Powering the ADC Down ====+  - **Capture a Single Snapshot**. 
 +  - Click the **Save Snapshot(s) Button**. 
 +  - Select either **Microamps (µA)** or **ADC Codes**.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-save_units.png?nolink&|}}\\ \\  
 +  - Click the **OK Button**. 
 +  - Browse to the directory location where the spreadsheet file is to be saved. 
 +  - Name the file. 
 +  - Click the **OK Button**.\\ \\ <WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</WRAP>
  
  
  
- +==== Saving Multiple Snapshots to a Spreadsheet File ==== 
 +  - **Establish a USB Connection Link**. 
 +  - **Capture Multiple Snapshots**. 
 +  - Click the **Save Snapshot(s) Button**. 
 +  - Select either **All Snapshots** or **Range of Snapshot(s)**. 
 +    * If **Range of Snapshot(s)** is selected, input the subset of snapshots to be saved. 
 +  - Select either **Microamps (µA)** or **ADC Codes**.\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0272:cn0272-software-save_full.png?nolink&|}}\\ \\  
 +  - Click the **OK button**. 
 +  - Browse to the directory location where the spreadsheet file is to be saved. 
 +  - Name the file. 
 +  - Click the **OK Button**.\\ \\ <WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</WRAP> 
 +\\ \\ \\ \\ \\ \\ 
 + 
 +=====Registration=====  
 +<WRAP round tip 80% > 
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0272-SDPZ?&v=RevD|Register]] to receive all these great benefits and more! 
 +</WRAP>
resources/eval/user-guides/circuits-from-the-lab/cn0272.1354217296.txt.gz · Last modified: 29 Nov 2012 20:28 by James Fitzgerald