This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0272 [29 Nov 2012 23:57] – [Establishing a USB Connection Link] James Fitzgerald | resources:eval:user-guides:circuits-from-the-lab:cn0272 [29 Jul 2021 06:04] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
===== Overview ===== | ===== Overview ===== | ||
- | [[http:// | + | [[adi>CN0272|CN-0272]] is a high-speed photodiode signal conditioning circuit with dark current compensation. The system converts current from a high-speed silicon PIN photodiode and drives the inputs of a 20 MSPS ADC. This combination of parts offers spectral sensitivity from 400 nm to 1050 nm with 49 nA of photocurrent sensitivity, |
Other suitable applications for this circuit would be as an analog opto-isolator. It can also be adapted to applications that require larger bandwidth and less resolution such as adaptive speed control systems. | Other suitable applications for this circuit would be as an analog opto-isolator. It can also be adapted to applications that require larger bandwidth and less resolution such as adaptive speed control systems. | ||
- | This user guide will discuss how to use the evaluation software to collect data from the [[http:// | + | This user guide will discuss how to use the evaluation software to collect data from the [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Daughter Board |
{{: | {{: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Daughter Board (**CN0272 Board**) |
- | * [[http:// | + | * [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] Power Supply or equivalent +6V power supply |
* [[ftp:// | * [[ftp:// | ||
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) | ||
Line 25: | Line 25: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Board connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] SDP-B Board via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] DC power supply powers the [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] Board via the DC barrel jack |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] SDP-B Board connects to the PC via the USB cable.\\ \\ {{: |
+ | |||
+ | ---- | ||
- | {{: | ||
- | < | ||
===== Installing the Software ===== | ===== Installing the Software ===== | ||
- | - Extract the file **CN0272 SDP Eval Software.zip** and open the file **setup.exe**.< | + | - Extract the file **CN0272 SDP Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> |
- | - Click **Next** to view the installation review page< | + | - Click **Next** to view the installation review page\\ \\ {{: |
- | - Click **Next** to start the installation< | + | - Click **Next** to start the installation\\ \\ {{: |
- | - Upon completion of the installation of the **CN0272 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute.< | + | - Upon completion of the installation of the **CN0272 SDP Eval Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> |
- | - Press **“Next”** to set the installation location for the **SDP Drivers**.< | + | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: |
- | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | + | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. |
- | < | + | |
+ | ---- | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect **J4** of the [[http:// | + | - Connect **J4** of the [[adi>EVAL-CN0272-SDPZ|EVAL-CN0272-SDPZ]] (CN0272 Board) to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] (SDP-B Board)\\ \\ {{: |
- Select the voltage bias of the photodiode. | - Select the voltage bias of the photodiode. | ||
- | - Select the onboard -5V bias by populating **JP1** with a shorting jumper as depicted below< | + | - Select the onboard -5V bias by populating **JP1** with a shorting jumper as depicted below\\ \\ {{: |
- | - Select an external voltage bias by populatign **JP1** with a shorting jumper as depicted below. | + | - Select an external voltage bias by populatign **JP1** with a shorting jumper as depicted below. |
- | - Connect a 6V supply to the Barrel Jack or the Screw Terminal on the CN0272 Board< | + | - Connect a 6V supply to the Barrel Jack or the Screw Terminal on the CN0272 Board\\ \\ {{: |
- | - Connect the USB Cable to the SDP-B Board and the PC< | + | - Connect the USB Cable to the SDP-B Board and the PC\\ \\ {{: |
- | < | + | |
+ | ---- | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
==== Software Control and Indicator Descriptions ==== | ==== Software Control and Indicator Descriptions ==== | ||
{{: | {{: | ||
- | -< | + | -**SDP Connector Dropdown Menu** |
- | * This control will select which connector (on the SDP-B Board) the CN0272 Board is currently connected to. The options are " | + | * This control will select which connector (on the SDP-B Board) the CN0272 Board is currently connected to. The options are " |
- | -< | + | -**Connect to SDP-B Board Button** |
- | * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board. | + | * When this button is pressed, the SDP-B Board makes a USB connection to the CN0272 Board. |
- | -< | + | -**Take Snapshot(s) Button** |
- | * When this button is pressed, the SDP-B Board will collect a single Snapshot or a collection of Snapshots depending on the < | + | * When this button is pressed, the SDP-B Board will collect a single Snapshot or a collection of Snapshots depending on the **Acquisition Mode** setting.\\ \\ <WRAP left round info 60%> |
- | -< | + | -**Save Snapshot(s) Button** |
* When this button is pressed, the software will save a single Snapshot or a collection of Snapshots to a tab delimited ASCII spreadsheet file. | * When this button is pressed, the software will save a single Snapshot or a collection of Snapshots to a tab delimited ASCII spreadsheet file. | ||
- | -< | + | -**Acquisition Mode Radio Buttons** |
* __Single Snapshot__ - When the software is in this mode, the SDP-B Board will collect a single Snapshot of data. | * __Single Snapshot__ - When the software is in this mode, the SDP-B Board will collect a single Snapshot of data. | ||
* __Multiple Snapshots__ - When the software is in this mode, the SDP-B Board will collect multiple Snapshots of data. | * __Multiple Snapshots__ - When the software is in this mode, the SDP-B Board will collect multiple Snapshots of data. | ||
- | -< | + | -**Conversions in Snapshot Numerical Control** |
* This control determines the number of conversions in a single Snapshot of data. | * This control determines the number of conversions in a single Snapshot of data. | ||
* The minimum value is 1 and the maximum value is 65,536. | * The minimum value is 1 and the maximum value is 65,536. | ||
- | -< | + | -**Snapshots to Take Numerical Control** |
* This control determines the number of Snapshots of data the SDP-B Board collects. | * This control determines the number of Snapshots of data the SDP-B Board collects. | ||
* The minimum value is 1 and the maximum is 65,536 | * The minimum value is 1 and the maximum is 65,536 | ||
* This control is only enabled in __Multiple Snapshots Acquisition Mode__. | * This control is only enabled in __Multiple Snapshots Acquisition Mode__. | ||
- | -< | + | -**Snapshot Delay (ms) Numerical Control** |
* This control determines the delay (in milliseconds) between Snapshots. | * This control determines the delay (in milliseconds) between Snapshots. | ||
* The minimum value is 1 and the maximum value is 65,536 | * The minimum value is 1 and the maximum value is 65,536 | ||
* This control is only enabled in __Multiple Snapshots Acquisition Mode__. | * This control is only enabled in __Multiple Snapshots Acquisition Mode__. | ||
- | -< | + | -**Control Tabs** |
* __Photocurrent Results__ - Clicking this tab brings the Photocurrent Results graph to the front | * __Photocurrent Results__ - Clicking this tab brings the Photocurrent Results graph to the front | ||
* __Histogram Results__ - Clicking this tab brings the Histogram Results graph to the front | * __Histogram Results__ - Clicking this tab brings the Histogram Results graph to the front | ||
* __Configure__ - Clicking this tab brings the System Settings to the front | * __Configure__ - Clicking this tab brings the System Settings to the front | ||
- | -< | + | -**Graph Controls** |
* These controls allow the user to zoom-in, zoom-out, and pan through the Snapshot displayed. | * These controls allow the user to zoom-in, zoom-out, and pan through the Snapshot displayed. | ||
- | -< | + | -**Graph Units Radio Buttons** |
* This control determines the Y-Axis units of the " | * This control determines the Y-Axis units of the " | ||
- | -< | + | -**Snapshot Displayed Numerical Control/ |
* This control determines the current Snapshot to display in the graph. | * This control determines the current Snapshot to display in the graph. | ||
* This control also acts as an indicator of the current Snapshot displayed in the graph. | * This control also acts as an indicator of the current Snapshot displayed in the graph. | ||
* This control/ | * This control/ | ||
- | -< | + | -**System Status String Indicator** |
* This indicator displays a message to the user detailing the current state of the software. | * This indicator displays a message to the user detailing the current state of the software. | ||
- | -< | + | -**System Status LED Indicator** |
- | * This indicator displays the current state of the software in the form of an LED. There are four status LED colors.< | + | * This indicator displays the current state of the software in the form of an LED. There are four status LED colors.\\ {{: |
- | < | + | |
+ | ---- | ||
==== Establishing a USB Connection Link ==== | ==== Establishing a USB Connection Link ==== | ||
- Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | - Follow the instructions to properly install the software and connect the hardware as described in the previous sections. | ||
- | - Open the file named **CN0272.exe** in the installation directory.< | + | - Open the file named **CN0272.exe** in the installation directory.\\ \\ <WRAP left info round box 60%> |
- | - Select the connector to use from the < | + | - Select the connector to use from the **SDP Connector Dropdown Menu**. |
- | - Click the < | + | - Click the **Connect to SDP-B Board Button**. A window with a progress bar will load.\\ \\ {{: |
- | - Upon success, the < | + | - Upon success, the **System Status String Indicator** will display __SDP-B Ready to Take Snapshot(s)__ |
==== Capturing a Single Snapshot ==== | ==== Capturing a Single Snapshot ==== | ||
- | - < | + | - **Establish a USB Connection Link**. |
- | - Select __Single Snapshot__ as the < | + | - Select __Single Snapshot__ as the **Acquisition Mode** |
- | - Set the number of < | + | - Set the number of conversions in the snapshot |
- | - Click the < | + | - Click the **Take Snapshot(s) Button** |
==== Capturing Multiple Snapshots ==== | ==== Capturing Multiple Snapshots ==== | ||
- | - < | + | - **Establish a USB Connection Link**. |
- | - Select __Multiple Snapshots__ as the < | + | - Select __Multiple Snapshots__ as the **Acquisition Mode**. |
- | - Set the number of < | + | - Set the number of conversions in each snapshot. |
- | - Set the < | + | - Set the number of snapshots to take. |
- | - Set the < | + | - Set the snapshot delay. |
- | - Click the < | + | - Click the **Take Snapshot(s) Button**. |
==== Displaying a Specific Snapshot ==== | ==== Displaying a Specific Snapshot ==== | ||
- | - < | + | - **Establish a USB Connection Link**. |
- | - Select __Multiple Snapshots__ as the < | + | - Select __Multiple Snapshots__ as the **Acquisition Mode**. |
- | - Set the number of < | + | - Set the number of conversions in each snapshot. |
- | - Set the < | + | - Set the number of snapshots to take. |
- | - Set the < | + | - Set the snapshot delay. |
- | - Click the < | + | - Click the **Take Snapshot(s) Button**. |
- | - Type the number of the snapshot of interest into the < | + | - Type the number of the snapshot of interest into the **Snapshot Displayed Numerical Control** |
==== Saving a Single Snapshot to a Spreadsheet File ==== | ==== Saving a Single Snapshot to a Spreadsheet File ==== | ||
- | - < | + | - **Establish a USB Connection Link**. |
- | - < | + | - **Capture a Single Snapshot**. |
- | - Click the < | + | - Click the **Save Snapshot(s) Button**. |
+ | - Select either **Microamps (µA)** or **ADC Codes**.\\ \\ {{: | ||
+ | - Click the **OK Button**. | ||
- Browse to the directory location where the spreadsheet file is to be saved. | - Browse to the directory location where the spreadsheet file is to be saved. | ||
- Name the file. | - Name the file. | ||
- | - Click the **OK Button**.< | + | - Click the **OK Button**.\\ \\ <WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</ |
==== Saving Multiple Snapshots to a Spreadsheet File ==== | ==== Saving Multiple Snapshots to a Spreadsheet File ==== | ||
- | - < | + | - **Establish a USB Connection Link**. |
- | - < | + | - **Capture Multiple Snapshots**. |
- | - Click the < | + | - Click the **Save Snapshot(s) Button**. |
- Select either **All Snapshots** or **Range of Snapshot(s)**. | - Select either **All Snapshots** or **Range of Snapshot(s)**. | ||
- | * If **Range of Snapshot(s)** is selected, input the subset of snapshots to be saved.< | + | * If **Range of Snapshot(s)** is selected, input the subset of snapshots to be saved. |
+ | - Select either **Microamps (µA)** or **ADC Codes**.\\ \\ {{: | ||
- Click the **OK button**. | - Click the **OK button**. | ||
- Browse to the directory location where the spreadsheet file is to be saved. | - Browse to the directory location where the spreadsheet file is to be saved. | ||
- Name the file. | - Name the file. | ||
- | - Click the **OK Button**.< | + | - Click the **OK Button**.\\ \\ <WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</ |
+ | \\ \\ \\ \\ \\ \\ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |