This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0263 [27 Dec 2017 09:09] – Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0263 [24 Apr 2024 03:30] (current) – [CN0263 User Guide (DEPRECATED)] Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== CN0263 | + | ====== CN0263 |
+ | |||
+ | <WRAP round important 65%> | ||
+ | \\ | ||
+ | This reference design has been **RETIRED** or **DEPRECATED**, | ||
+ | \\ | ||
+ | This page is here for historical/ | ||
+ | \\ | ||
+ | </ | ||
+ | |||
===== Overview ===== | ===== Overview ===== | ||
[[ADI> | [[ADI> | ||
Line 86: | Line 96: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
====Main Tab==== | ====Main Tab==== | ||
- | {{ : | + | {{ : |
+ | \\ | ||
+ | \\ | ||
+ | {{ : | ||
| | ||
\\ | \\ | ||
+ | |||
+ | ==== Running the System ==== | ||
+ | -Open the ADV Register Control | ||
+ | -When the ADV Register Control opens a window called ADV Register Program Configuration opens, make sure that the “USB Connected” indicator is green | ||
+ | -If indicator doesn' | ||
+ | -Select the proper script according to the model type of your ADV7180. In the case of CN0263 board, ADV7180_ADV7180@_ADV7393-VER.1.0LQFP64.txt shall be selected. | ||
+ | -To program the CN0263 evaluation board press Setting -> Scripts | ||
+ | -Select which script you want to run on the drop down menu. The desired script depends on the analog video inputted to the ADV7180, and the desired analog video output from the video encoder on the evaluation board | ||
---- | ---- | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
- | * [[ftp:// | ||
- | * [[ADI> | ||
- | * [[http:// | ||
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
- | ===== Schematic, PCB Layout, Bill of Materials | + | =====Registration===== |
- | + | <WRAP round tip 80% > | |
- | <WRAP round 80% download> | + | Receive software update notifications, |
- | [[http:// | + | |
- | * Schematics | + | |
- | * PCB Layout | + | |
- | * Bill of Materials | + | |
- | * PADS project | + | |
</ | </ | ||
- | |||
//End of Document// | //End of Document// | ||