This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0251 [17 Feb 2021 08:49] – [Required Equipment] Harvey John De Chavez | resources:eval:user-guides:circuits-from-the-lab:cn0251 [30 Jul 2021 07:26] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 42: | Line 42: | ||
* **JP1** and **JP2** configure the analog inputs for single-ended or differential inputs | * **JP1** and **JP2** configure the analog inputs for single-ended or differential inputs | ||
* **JP3** and **JP4** configure the gain of the [[adi> | * **JP3** and **JP4** configure the gain of the [[adi> | ||
- | - Connect the [[http://www.digilentinc.com/Products/Detail.cfm? | + | - Connect the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADALM2000.html#eb-overview|ADALM2000]] to the [[adi> |
* The waveform outputs should be connected to **J1:2 (IN1-)** and **J1:3 (IN2+)** of the **CN-0251 Board**. | * The waveform outputs should be connected to **J1:2 (IN1-)** and **J1:3 (IN2+)** of the **CN-0251 Board**. | ||
- | * The [[http://www.digilentinc.com/Products/Detail.cfm? | + | * The [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADALM2000.html#eb-overview|ADALM2000]] ground should be connected to **AGND** of the **CN-0251 Board**.\\ \\ {{: |
- Connect the +6V Power Supply to the screw terminal at **J3**. | - Connect the +6V Power Supply to the screw terminal at **J3**. | ||
- Connect the ±15V Power Supply to the screw terminal at **J4**. | - Connect the ±15V Power Supply to the screw terminal at **J4**. | ||
Line 52: | Line 52: | ||
---- | ---- | ||
- | ===== Setting up Digilent WaveForms | + | ===== Getting Started with ADALM2000 and Scopy ===== |
- | - Install [[https:// | + | - Use the USB Type-A to USB Micro-B cable to connect the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/ADALM2000.html#eb-overview|ADALM2000]] to the PC. A detailed guide on how to start ADALM2000 and install [[: |
- | - Use the USB Type-A to USB Micro-B cable to connect the [[http://www.digilentinc.com/Products/Detail.cfm? | + | - Upon connecting |
- | - Open the file named [[https://docs.google.com/file/d/ | + | - Click the **Run button**.\\ {{: |
- | - Click the **Run All Button**\\ {{: | + | |
---- | ---- | ||
Line 120: | Line 119: | ||
- Click the **OK Button**. | - Click the **OK Button**. | ||
<WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</ | <WRAP left round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs.</ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |