This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0204 [07 Aug 2017 08:35] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0204 [30 Jul 2021 07:20] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 21: | Line 21: | ||
* ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | ||
* Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | ||
- | * PC (Windows 2000 or Windows XP) with USB interface | + | * PC with USB interface |
+ | * Windows 7 or higher | ||
---- | ---- | ||
Line 36: | Line 37: | ||
* Connect the **-25 V** power supply to the **GND_ISO** terminal | * Connect the **-25 V** power supply to the **GND_ISO** terminal | ||
* Terminal block **CN4** is the voltage output | * Terminal block **CN4** is the voltage output | ||
- | * **Optionally**, | + | * **Optionally** |
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
==== Jumper Settings ==== | ==== Jumper Settings ==== | ||
- | See the table in the image below for the jumper settings. Values in bold are the default settings for the [[ADI> | + | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> |
- | {{ : | + | {{ : |
---- | ---- | ||
Line 110: | Line 111: | ||
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
+ | |||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | //End of Document// |