This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0204 [06 Sep 2017 09:49] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0204 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 21: | Line 21: | ||
* ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | ||
* Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | ||
- | * PC (Windows 7) with USB interface | + | * PC with USB interface |
+ | * Windows 7 or higher | ||
---- | ---- | ||
Line 42: | Line 43: | ||
See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> | ||
- | {{ : | + | {{ : |
---- | ---- | ||
Line 110: | Line 111: | ||
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
+ | |||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[adi> | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | //End of Document// |