This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0204 [07 Aug 2017 08:36] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0204 [06 Sep 2017 09:53] – Angelo Nikko Catapang | ||
---|---|---|---|
Line 21: | Line 21: | ||
* ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | ||
* Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | ||
- | * PC (Windows | + | * PC (Windows |
---- | ---- | ||
Line 36: | Line 36: | ||
* Connect the **-25 V** power supply to the **GND_ISO** terminal | * Connect the **-25 V** power supply to the **GND_ISO** terminal | ||
* Terminal block **CN4** is the voltage output | * Terminal block **CN4** is the voltage output | ||
- | * **Optionally**, | + | * **Optionally** |
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
==== Jumper Settings ==== | ==== Jumper Settings ==== | ||
- | See the table in the image below for the jumper settings. Values in bold are the default settings for the [[ADI> | + | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> |
- | {{ : | + | {{ : |
---- | ---- |