This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0204 [07 Aug 2017 06:09] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0204 [21 Sep 2017 18:51] – adding design files Brandon Bushey | ||
---|---|---|---|
Line 21: | Line 21: | ||
* ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | * ±25 V/1 A Triple Output DC Power Supply (**Agilent E3631A**) | ||
* Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | * Optional Digital Multimeter for Verification (**Agilent 34401A 6.5 Digital Multimeter**) | ||
- | * PC (Windows 2000 or Windows XP) with USB interface | + | * PC with USB interface |
+ | * Windows 7 or higher | ||
---- | ---- | ||
Line 36: | Line 37: | ||
* Connect the **-25 V** power supply to the **GND_ISO** terminal | * Connect the **-25 V** power supply to the **GND_ISO** terminal | ||
* Terminal block **CN4** is the voltage output | * Terminal block **CN4** is the voltage output | ||
- | * **Optionally**, | + | * **Optionally** |
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
==== Jumper Settings ==== | ==== Jumper Settings ==== | ||
- | See the table in the image below for the jumper settings. Values in bold are the default settings for the [[ADI> | + | See the table in the image below for the jumper settings. Values in red are the default settings for the [[ADI> |
- | {{ : | + | {{ : |
---- | ---- | ||
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== | ||
- | - Extract the file **[[ftp:// | + | - Extract the file **[[ftp:// |
- | - Press **Next** to view the installation review page\\ {{ : | + | - Press **Next** to view the installation review page\\ {{: |
- | - Press **Next** to start the installation\\ {{ : | + | - Press **Next** to start the installation\\ {{: |
- | - Upon completion of the installation of the **CN0204 Evaluation Software**, the installer for the ADI SDP Drivers will execute.\\ <WRAP left tip round box 60%> | + | - Upon completion of the installation of the **CN0204 Evaluation Software**, the installer for the ADI SDP Drivers will execute.\\ <WRAP left tip round box 60%> |
- | - Press **Next** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | + | - Press **Next** to set the installation location for the **SDP Drivers**\\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: |
- | - Press **Next** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{ : | + | - Press **Next** to install the **SDP Drivers**. When prompted by Windows Security, just press **Install**\\ {{: |
- | - Press **Finish** to complete the installation\\ {{ : | + | - Press **Finish** to complete the installation\\ {{: |
---- | ---- | ||
Line 59: | Line 60: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
==== Main Window ==== | ==== Main Window ==== | ||
+ | {{ : | ||
+ | * **Title Bar** <fc # | ||
+ | * **Connect Button** | ||
+ | * Starts the connection with the [[ADI> | ||
+ | * **Disconnect Button** | ||
+ | * Ends the connection with the [[ADI> | ||
+ | * **System Configuration** <fc # | ||
+ | * **Connector** | ||
+ | * Selects which 120-pin connection of the **SDP-B Board** to use | ||
+ | * **SCLK (Hz)** | ||
+ | * Sets the SPI clock frequency used by the evaluation board | ||
+ | * **AD5751 Configuration** <fc # | ||
+ | * **JP1 Configuration** | ||
+ | * Sets the SPI address of the AD5750-1 based on the position of JP1 | ||
+ | * **Range Select** | ||
+ | * Sets the voltage/ | ||
+ | * **Toggle CLEAR** | ||
+ | * Sets the outputs to the zero/ | ||
+ | * **AD5751 Error Indicator** <fc # | ||
+ | * **Vout Fault** | ||
+ | * There is a short circuit on the VOUT pin | ||
+ | * **Iout Fault** | ||
+ | * There is an open circuit on the IOUT pin | ||
+ | * **Over Temp** | ||
+ | * The AD5751 core temperature exceeds 150 °C | ||
+ | * **PEC Error** | ||
+ | * CRC-8 error checking detected an interface error | ||
+ | * **Output Setting** <fc # | ||
+ | * **Write AD5662** | ||
+ | * Writes the hexadecimal value in the left field to the AD5662 output voltage | ||
+ | * **Reset AD5751** | ||
+ | * Resets the AD5751 to its power-on state | ||
+ | * **Quit** | ||
+ | * Exits the software application | ||
+ | ==== Running the System ==== | ||
+ | - Open the **CN0204.exe** application from the default installation location. | ||
+ | - Set the correct connector and SCLK settings for the board in the System Configuration section. | ||
+ | - Click the **Connect Button** | ||
+ | - Upon successful connection, select the desired range of output on the Range Select drop-down menu. | ||
+ | - Input a hex value equivalent of the desired output level in the Output Setting section. | ||
+ | - Click **Write AD5662** | ||
+ | - Click **Disconnect Button** if finished. | ||
+ | ---- | ||
+ | |||
+ | ===== More Information and Useful Links ===== | ||
+ | * [[ftp:// | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | |||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | [[http:// | ||
+ | * Schematics | ||
+ | * PCB Layout | ||
+ | * Bill of Materials | ||
+ | * PADS project | ||
+ | </ | ||
+ | |||
+ | //End of Document// |