This version is outdated by a newer approved version.This version (16 Oct 2012 16:56) is a draft.
Approvals: 0/1
This is an old revision of the document!
Tilt Measurement Using a Dual Axis Accelerometer (CN0189)
Overview
The ADXL203 is a polysilicon surface micromachined sensor and signal conditioning circuit. Acceleration in the X or Y axis will produce a corresponding output voltage on the XOUT or YOUT output pins of the device. The X axis and Y axis are perpendicular to one another.The AD8608 quad op amp buffers, attenuates, and level shifts the ADXL203 outputs so they are at the proper levels to drive the inputs of the The AD7887. The AD7887 is configurable for either dual or single channel operation via the on-chip control register. In this application it is configured for dual channel mode, allowing the user to monitor both outputs of the ADXL203, thereby providing a more accurate and complete solution.
General Setup
Minimum PC/System Requirements
How to Install the Evaluation Software
Extract the files within the file
CN0189 SDP Eval Software.zip and open the file
setup.exe. It is recommended that you install the CN0189 SDP Evaluation Software to the default directory path
C:\Program Files\Analog Devices\CN0189\ and all National Instruments products to
C:\Program Files\National Instruments\
Press
“Next”.
Press “Next”.
Upon completion of the installation of the
CN0189 SDP Eval Software, the installer for the
ADI SDP Drivers will execute. Follow the on-screen prompts to install the drivers. It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.
Press “Next”.
It is recommended that you install the drivers to the default directory path C:\Program Files\Analog Devices\SDP\Drivers\
Press “Next” to install the Drivers and complete the installation of all software necessary to evaluate the EVAL-CN0189-SDPZ
Step by Step Instruction for Connecting the Hardware
-
Plug in the DC barrel jack to connector J3 of the
EVAL-CN0189-SDPZ and the mini end of the
USB cable into connector J2 of the
EVAL-SDP-CS1Z. And connect the other end of the
USB cable into the Laptop or PC.
Opening and Enabling the Evaluation Software
Launch the executable found at C:\Program Files\Analog Devices\CN0189 and press the “Connect“ button.
Step by Step Instruction to Using the Evaluation Software
The following is a list of all available software controls, grouped according to their location in the software:
System Controls
Connect – This button configures the
AD7887 by writing to the necessary registers.
-
Connector A - This menu allows the user to select which connector of the SDP board is being utilized.
Conversion Mode Controls -
Continuous Conversion Mode
This control brings the user to the Demonstration Tab and locks out unnecessary tabs.
This control displays/hides the necessary controls in the Data Acquisition Controls Tab.
Data Acquisition Controls
Click to Begin Continuous Sampling - This control starts the demonstration mode which measures the angle the PCB makes with the gravity vector and displays it.
Single Sample
This control brings the user to the Sample Data tab and locks out unnecessary tabs.
This control displays/hides the necessary controls in the Data Acquisition Controls tab.
Data Acquisition Controls
Input Angle - Having set the PCB at a specific angle, this control allows the user to input that angle and to compare the ADC result with the actual angle.
Single Sample - This control instructs the ADC to sample and convert one acceleration reading from each axis.
Clear Data - This control clears the X-Y plot.
Remove Data Point - This control removes the last data point from the X-Y plot.
Save Data - This control prompts and allows the user to save their data to a text file.