This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0188 [02 Nov 2017 08:57] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0188 [03 Jan 2021 21:55] – fix links Robin Getz | ||
---|---|---|---|
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
* [[adi> | * [[adi> | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp:// | * [[ftp:// | ||
* Power Supply | * Power Supply | ||
Line 29: | Line 29: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0188-SDPZ|EVAL-CN0188-SDPZ]] **(CN-0188 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input | ||
* Terminal block **J3** is the test point for 6 V DC output | * Terminal block **J3** is the test point for 6 V DC output | ||
- | * Terminal block **J4** | + | * Terminal block **J4** |
\\ | \\ | ||
Line 39: | Line 39: | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[adi> | + | - Connect the 120-pin connector on the [[adi> |
- Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | - Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above | ||
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | ||
*//If available, a +6 V "wall wart" can be connected to the barrel connector on the board and used in place of the +6 V power supply// | *//If available, a +6 V "wall wart" can be connected to the barrel connector on the board and used in place of the +6 V power supply// | ||
- Connect the USB cable supplied with the SDP board to the USB port on the PC | - Connect the USB cable supplied with the SDP board to the USB port on the PC | ||
- | - Apply power to the +6 V supply (or “wall wart”) connected to [[adi> | + | - Apply power to the +6 V supply (or “wall wart”) connected to [[adi> |
- Launch the evaluation software | - Launch the evaluation software | ||
- Connect the USB cable from the PC to the USB mini connector on the SDP board | - Connect the USB cable from the PC to the USB mini connector on the SDP board | ||
Line 51: | Line 51: | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | Do **not** connect | + | Connect the **system ground** and the **PCB isolated ground** |
</ | </ | ||
Line 66: | Line 66: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
====Test Setup Tab==== | ====Test Setup Tab==== | ||
- | {{ : | + | ==== Main Window ==== |
- | | + | {{ : |
+ | - **Connect** Button - Starts the connection between the [[ADI> | ||
+ | - **Disconnect** Button - Ends the connection between the [[ADI> | ||
+ | - **Select SDP Connector** - Selects which 120-pin connection of the SDP-B Board to use | ||
+ | - **Shunt Voltage Input** - Determines input shunt voltage level in millivolts | ||
+ | - **Temperature** - Temperature level test conditions of input signal | ||
+ | - **Data Acquisition** Controls | ||
+ | * **Sample Data** - Start acquisition of measurement data | ||
+ | * **Remove Data Point** - Remove a data point from samples | ||
+ | * **Save Data** - Save measurement data to file | ||
+ | * **Clear Data** - Clear the current measurement data | ||
+ | | ||
+ | * **ADC Code Plot** Enable - Show or hide the ADC Code plot | ||
+ | * **Error Plot** Enable - Show or hide the Error plot | ||
+ | * **Converted Shunt Voltage** - Shunt voltage value from the ADC | ||
+ | * **Over/ | ||
+ | * **Plot Options** - Edit plot display and options like interpolation and color of output waveform | ||
+ | - **Administration** Tab \\ {{ : | ||
+ | * **Flash LED** - Flashes the LED on the SDP controller board | ||
+ | * **Read Firmware** - Reads the firmware of CN0240 Evaluation Board | ||
+ | - **Quit** Button - Closes the evaluation software\\ | ||
\\ | \\ | ||
+ | ==== Running the System ==== | ||
+ | -Open the CN0188.exe application from the default installation location | ||
+ | -Set the correct connector and click the Connect Button | ||
+ | -Upon successful connection, set the desired input signal parameters such as shunt voltage and temperature | ||
+ | -Start and control data acquisition through the data acquisition control buttons | ||
+ | -Output data will be shown in the graph. Edit graph through plot options and check boxes provided | ||
+ | -Click Disconnect if finished | ||
+ | -Click Quit to exit the program | ||
+ | |||
+ | \\ | ||
---- | ---- | ||
Line 75: | Line 105: | ||
* [[ftp:// | * [[ftp:// | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
Line 85: | Line 115: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout |