This is an old revision of the document!
CN0188 Evaluation Board Guide
Overview
CN0188 is a circuit that monitors current in individual channels of −48 V to better than 1% accuracy. The load current passes through a shunt resistor, which is external to the circuit. The shunt resistor value is chosen so that the shunt voltage is approximately 50 mV at maximum load current. The entire circuit operates on a single +3.3 V supply.
The AD7171 is a very low power, 16-bit, analog-to-digital converter (ADC). It contains a precision, 16-bit, Σ-Δ ADC and an on-chip oscillator. The measurement result from AD7171 is provided as a digital code utilizing a simple 2-wire, SPI-compatible serial interface. Optional galvanic isolation is provided by the ADUM5402 quad channel isolator. In addition to isolating the output data, the digital isolator can also supply isolated +3.3 V for the circuit.
The ADA4051-2 is a CMOS, micropower, zerodrift operational amplifier utilizing an innovative chopping technique. This amplifier feature rail-to-rail input/output swing and extremely low offset voltage while operating from a 1.8 V to 5.5 V power supply.
The ADR381 is precision 2.500 V band gap voltage reference featuring high accuracy, high stability, and low power consumption in a tiny footprint. It is a micropower, low dropout voltage (LDV) device that provides a stable output voltage from supplies as low as 300 mV above the output voltage.
The EVAL-CN0188-SDPZ Board connects to ADI’s System Demonstration Platform (SDP) and is powered by a +6 V supply or +6 V “wall wart”.
Required Equipment
General Setup
Block assignments
Test setup

-
Connect a shunt resistor across the input terminals with a load to ground as indicated in figure above
With power to the supply off, connect a +6
V power supply to the pins marked “+6V” and “GND” on the board
If available, a +6 V “wall wart” can be connected to the barrel connector on the board and used in place of the +6 V power supply
Connect the
USB cable supplied with the SDP board to the
USB port on the PC
-
Launch the evaluation software
Connect the
USB cable from the PC to the
USB mini connector on the SDP board
Connect the system ground and the PCB isolated ground to guarantee correct voltage levels and operation. Test point 31 and test point 32 give access to the GND_ISO required to properly make this connection.
Installing the Evaluation Software
Extract the file
CN0188_Evaluation_Software.zip and open the file
setup.exe.
NOTE: It is recommended that you install the CN0188 Evaluation Software to the default directory path C:\Program Files (x86)\Analog Devices\CN0188\ and all National Instruments products to C:\Program Files\National Instruments\
Click
Next to view the installation review page
Click
Next to start the installation
Upon completion of the installation of the
CN-0188 Evaluation Software, the installer for the
ADI SDP Drivers will execute.
NOTE: It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer.

Press
“Next” to set the installation location for the
SDP Drivers.
It is recommended that you install the drivers to the default directory path
C:\Program Files\Analog Devices\SDP\Drivers

Press
“Install” to install the
SDP Drivers and complete the installation of all software. Click
“Finish” when done.

Using the Evaluation Software
Test Setup Tab
Main Window
-
-
Select SDP Connector - Selects which 120-pin connection of the SDP-B Board to use
Shunt Voltage Input - Determines input shunt voltage level in millivolts
Temperature - Temperature level test conditions of input signal
Data Acquisition Controls

Sample Data - Start acquisition of measurement data
Remove Data Point - Remove a data point from samples
Save Data - Save measurement data to file
Clear Data - Clear the current measurement data
Sample Data Graph Tab - Shows the XY plot of ADC code and output error (%) with respect to the shunt voltage

ADC Code Plot Enable - Show or hide the ADC Code plot
Error Plot Enable - Show or hide the Error plot
Converted Shunt Voltage - Shunt voltage value from the ADC
Over/Under Voltage Indicator - Indicates over or under voltage conditions
Plot Options - Edit plot display and options like interpolation and color of output waveform
Administration Tab

Quit Button - Closes the evaluation software
Running the System
Open the CN0188.exe application from the default installation location
Set the correct connector and click the Connect Button
Upon successful connection, set the desired input signal parameters such as shunt voltage and temperature
Start and control data acquisition through the data acquisition control buttons
Output data will be shown in the graph. Edit graph through plot options and check boxes provided
Click Disconnect if finished
Click Quit to exit the program
Schematic, PCB Layout, Bill of Materials