This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0187 [29 Sep 2017 07:43] – [Calibration Instructions] erbe reyta | resources:eval:user-guides:circuits-from-the-lab:cn0187 [30 Jul 2021 07:14] (current) – Victor Calinao, Jr | ||
---|---|---|---|
Line 9: | Line 9: | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * [[http:// | + | * [[adi>EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] Evaluation Board |
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board |
* [[ftp:// | * [[ftp:// | ||
* (supplied with provided CD in kit) | * (supplied with provided CD in kit) | ||
Line 41: | Line 41: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
{{ : | {{ : | ||
- | - Connect the 120-pin connector on the [[http:// | + | - Connect the 120-pin connector on the [[adi>EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] circuit board to the connector marked “CON A” on the EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors as depicted in the image below. |
- | - Using an appropriate RF cable, connect the RF signal source to the [[http:// | + | - Using an appropriate RF cable, connect the RF signal source to the [[adi>EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] board via the SMA RF input connector. |
- With power to the supply off, connect a +6 V power supply to the pins marked “+6 V” and “GND” on the board. If available, a +6 V "wall wart" can be connected to the barrel jack connector on the board and used in place of the +6 V power supply. | - With power to the supply off, connect a +6 V power supply to the pins marked “+6 V” and “GND” on the board. If available, a +6 V "wall wart" can be connected to the barrel jack connector on the board and used in place of the +6 V power supply. | ||
- | - Connect the USB cable, supplied along with the [[http:// | + | - Connect the USB cable, supplied along with the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation board, from the SDP board to the USB port on the PC. |
---- | ---- | ||
Line 55: | Line 55: | ||
{{ : | {{ : | ||
- | ==== Calibrate | + | ==== Calibration |
+ | |||
+ | {{ : | ||
+ | |||
+ | <note important> | ||
{{ : | {{ : | ||
+ | |||
+ | |||
-Input | -Input | ||
- Input Power (dBm) | - Input Power (dBm) | ||
Line 86: | Line 92: | ||
{{ : | {{ : | ||
+ | |||
+ | <note important> | ||
+ | |||
- List of Input Buttons | - List of Input Buttons | ||
- Acquire Data | - Acquire Data | ||
Line 112: | Line 121: | ||
{{ : | {{ : | ||
+ | |||
+ | <note important> | ||
+ | |||
- Sclk (Hz) | - Sclk (Hz) | ||
* set the SPI clock reference | * set the SPI clock reference | ||
Line 118: | Line 130: | ||
- Sample Size | - Sample Size | ||
* set the sample size | * set the sample size | ||
- | <note important> | + | |
==== Graphical Output ==== | ==== Graphical Output ==== | ||
Line 133: | Line 145: | ||
{{: | {{: | ||
- | {{ : | + | {{ : |
< | < | ||
Crest factor is the peak amplitude of the waveform divided by the RMS value of the waveform | Crest factor is the peak amplitude of the waveform divided by the RMS value of the waveform | ||
</ | </ | ||
- | ===== Calibration Instructions ===== | ||
- | |||
- | {{ : | ||
- | |||
- | <note important> | ||
===== Schematics, PCB Layout, Bill of Materials ===== | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
Line 152: | Line 159: | ||
* {{: | * {{: | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
// End of Document // | // End of Document // |