Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0187 [29 Sep 2017 07:43] – [Graphical Output] erbe reytaresources:eval:user-guides:circuits-from-the-lab:cn0187 [30 Jul 2021 07:14] (current) Victor Calinao, Jr
Line 9: Line 9:
  
 ===== General Setup ===== ===== General Setup =====
-  * [[http://www.analog.com/EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] Evaluation Board +  * [[adi>EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] Evaluation Board 
-  * [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board+  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Evaluation Board
   * [[ftp://ftp.analog.com/pub/cftl/CN0187|CN0187 Evaluation Software]]   * [[ftp://ftp.analog.com/pub/cftl/CN0187|CN0187 Evaluation Software]]
     * (supplied with provided CD in kit)     * (supplied with provided CD in kit)
Line 41: Line 41:
 ===== Connecting the Hardware ===== ===== Connecting the Hardware =====
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:cn0187_block_diagram_v1.png |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:cn0187_block_diagram_v1.png |}}
-  - Connect the 120-pin connector on the [[http://www.analog.com/EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] circuit board to the connector marked “CON A” on the EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors as depicted in the image below. +  - Connect the 120-pin connector on the [[adi>EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] circuit board to the connector marked “CON A” on the EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware should be used to firmly secure the two boards, using the holes provided at the ends of the 120-pin connectors as depicted in the image below. 
-  - Using an appropriate RF cable, connect the RF signal source to the [[http://www.analog.com/EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] board via the SMA RF input connector.+  - Using an appropriate RF cable, connect the RF signal source to the [[adi>EVAL-CN0187-SDPZ|EVAL-CN0187-SDPZ]] board via the SMA RF input connector.
   - With power to the supply off, connect a +6 V power supply to the pins marked “+6 V” and “GND” on the board. If available, a +6 V "wall wart" can be connected to the barrel jack connector on the board and used in place of the +6 V power supply.    - With power to the supply off, connect a +6 V power supply to the pins marked “+6 V” and “GND” on the board. If available, a +6 V "wall wart" can be connected to the barrel jack connector on the board and used in place of the +6 V power supply. 
-  - Connect the USB cable, supplied along with the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation board, from the SDP board to the USB port on the PC.+  - Connect the USB cable, supplied along with the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation board, from the SDP board to the USB port on the PC.
  
 ---- ----
Line 55: Line 55:
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:calibrate.png?direct |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:calibrate.png?direct |}}
  
-==== Calibrate ====+==== Calibration ==== 
 + 
 +{{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:sub_calibration_intructions_v1.png |}} 
 + 
 +<note important>Calibration procedure needs to be done for every change in frequency.</note>
  
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:main_cal.png?direct |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:main_cal.png?direct |}}
 +
 +
     -Input     -Input
       - Input Power (dBm)       - Input Power (dBm)
Line 86: Line 92:
  
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:main_measure.png?direct |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:main_measure.png?direct |}}
 +
 +<note important>The board must be calibrated before Input Power can be measured</note>
 +
     - List of Input Buttons     - List of Input Buttons
       - Acquire Data       - Acquire Data
Line 112: Line 121:
  
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:main_advance.png?direct |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:main_advance.png?direct |}}
 +
 +<note important>Note: Do not modify these  values unless you need to</note>
 +
     - Sclk (Hz)     - Sclk (Hz)
       * set the SPI clock reference       * set the SPI clock reference
Line 118: Line 130:
     - Sample Size     - Sample Size
       * set the sample size       * set the sample size
-<note important>Note: Do not modify these  values unless you need to</note>+
   
 ==== Graphical Output ==== ==== Graphical Output ====
Line 133: Line 145:
  
 {{:resources:eval:user-guides:circuits-from-the-lab:cn0187:sub_crest.png?450|}} {{:resources:eval:user-guides:circuits-from-the-lab:cn0187:sub_crest.png?450|}}
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:crest_factor_sample_output.png?350|}}+{{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:crest_factor_sample_output.png?380|}}
  
 <note> <note>
 Crest factor is the peak amplitude of the waveform divided by the RMS value of the waveform Crest factor is the peak amplitude of the waveform divided by the RMS value of the waveform
 </note> </note>
-===== Calibration Instructions ===== 
  
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0187:sub_calibration_intructions_v1.png |}} 
- 
-<note Note>Calibration procedure needs to be done for every change in frequency.</note> 
 ===== Schematics, PCB Layout, Bill of Materials ===== ===== Schematics, PCB Layout, Bill of Materials =====
  
Line 151: Line 159:
   * {{:resources:eval:user-guides:circuits-from-the-lab:cn0187:eval-cn0187-sdpz-assemblydrawing-revb.pdf|Assembly Drawing}}(PDF)   * {{:resources:eval:user-guides:circuits-from-the-lab:cn0187:eval-cn0187-sdpz-assemblydrawing-revb.pdf|Assembly Drawing}}(PDF)
 </WRAP> </WRAP>
 +
 +=====Registration===== 
 +<WRAP round tip 80% >
 +Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware.  [[reg>EVAL-CN0187-SDPZ?&v=Rev B|Register]] to receive all these great benefits and more!</WRAP>
  
 // End of Document // // End of Document //
resources/eval/user-guides/circuits-from-the-lab/cn0187.txt · Last modified: 30 Jul 2021 07:14 by Victor Calinao, Jr