Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0178 [04 Dec 2017 10:38] – update Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0178 [23 Mar 2022 05:53] (current) – updated sw link Trisha Cabildo |
---|
===== Required Equipment ===== | ===== Required Equipment ===== |
* [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] | * [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] |
* [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
* [[ftp://ftp.analog.com/pub/cftl/CN0178/|CN0178 Evaluation Software]] | * [[http://swdownloads.analog.com/cse/cftl/CN0178/CN0178_SDP_Eval_Software.zip|CN0178 Evaluation Software]] |
* 6 V or 6 V Wall wart | * 6 V or 6 V Wall wart |
* //Agilent E3631A power supply// | * //Agilent E3631A power supply// |
==== Block assignments ==== | ==== Block assignments ==== |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0178:10-25-2017_2-16-34_pm.png?nolink&650 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0178:10-25-2017_2-16-34_pm.png?nolink&650 |}}\\ |
* The [[http://www.analog.com/EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ]] **(CN-0178 Board)** connects to the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector | * The [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ]] **(CN-0178 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
* The [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Terminal block **J1** is the +6 V power supply | * Terminal block **J1** is the +6 V power supply |
* Terminal block **J2** is the +6 V barrel connector for wall wart supply input | * Terminal block **J2** is the +6 V barrel connector for wall wart supply input |
==== Test setup ==== | ==== Test setup ==== |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0178:10-30-2017_3-33-48_pm.png?nolink&600 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0178:10-30-2017_3-33-48_pm.png?nolink&600 |}}\\ |
- Connect the 120-pin connector on the [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board | - Connect the 120-pin connector on the [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] to the connector marked “CON A” on the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] evaluation (SDP) board |
- Connect the RF signal source to the [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] via the SMA RF input connector | - Connect the RF signal source to the [[adi>EVAL-CN0178-SDPZ|EVAL-CN0178-SDPZ Evaluation Board]] via the SMA RF input connector |
- With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board | - With power to the supply off, connect a +6 V power supply to the pins marked “+6V” and “GND” on the board |
---- | ---- |
===== Installing the Evaluation Software ===== | ===== Installing the Evaluation Software ===== |
- Extract the file **CN0178_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[ftp://ftp.analog.com/pub/cftl/CN0178/|CN0178 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0178\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP> {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:1.png?nolink&500|}} | - Extract the file **CN0178_Evaluation_Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%>**NOTE:** It is recommended that you install the [[http://swdownloads.analog.com/cse/cftl/CN0178/CN0178_SDP_Eval_Software.zip|CN0178 Evaluation Software]] to the default directory path **C:\Program Files (x86)\Analog Devices\CN0178\** and all National Instruments products to **C:\Program Files\National Instruments\**</WRAP> {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:1.png?nolink&500|}} |
- Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:2.png?nolink&500|}}\\ \\ | - Click **Next** to view the installation review page\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:2.png?nolink&500|}}\\ \\ |
- Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:3.png?nolink&500|}}\\ \\ | - Click **Next** to start the installation\\ \\ {{:resources:eval:user-guides:circuits-from-the-lab:cn0178:3.png?nolink&500|}}\\ \\ |
| |
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== |
* [[ftp://ftp.analog.com/pub/cftl/CN0178/|CN0178 Evaluation Software]] | * [[http://swdownloads.analog.com/cse/cftl/CN0178/CN0178_SDP_Eval_Software.zip|CN0178 Evaluation Software]] |
* [[ADI>CN0178|CN0178 Circuit Note Page]] | * [[ADI>CN0178|CN0178 Circuit Note Page]] |
* [[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0178-DesignSupport.zip|CN0178 Design Support Package]] | * [[adi>media/en/reference-design-documentation/design-integration-files/CN0178-DesignSupport.zip|CN0178 Design Support Package]] |
| |
* [[ADI>ADL5902|ADL5902 Product Page]] | * [[ADI>ADL5902|ADL5902 Product Page]] |
| |
<WRAP round 80% download> | <WRAP round 80% download> |
[[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0178-DesignSupport.zip|EVAL-CN0178-SDPZ Design & Integration Files]] | [[adi>media/en/reference-design-documentation/design-integration-files/CN0178-DesignSupport.zip|EVAL-CN0178-SDPZ Design & Integration Files]] |
* Schematics | * Schematics |
* PCB Layout | * PCB Layout |
* PADS project | * PADS project |
</WRAP> | </WRAP> |
| |
| =====Registration===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0178-SDPZ?&v=Rev C|Register]] to receive all these great benefits and more!</WRAP> |
| |
//End of Document// | //End of Document// |
| |