Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:user-guides:arduino-uno:reference_designs:demo_cn0391 [23 Jan 2018 16:21] – [General Description/Overview] Mircea Caprioru | resources:eval:user-guides:arduino-uno:reference_designs:demo_cn0391 [03 Jan 2021 22:04] – fix links Robin Getz |
---|
===== General Description/Overview ===== | ===== General Description/Overview ===== |
| |
The **CN0391_example** project uses the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-CN0391-ARDZ.html|EVAL-CN0391-ARDZ shield]] which is a multichannel thermocouple temperature measurement system with cold junction compensation. | The **CN0391_example** project uses the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-CN0391-ARDZ.html|EVAL-CN0391-ARDZ shield]] which is a multichannel thermocouple temperature measurement system with cold junction compensation. |
| |
The EVAL-CN0391-ARDZ shield uses the [[http://www.analog.com/en/products/analog-to-digital-converters/precision-adc-10msps/ad7124-8| AD7124-8 part]] which is a **8-Channel** Low Noise, Low Power, **24-Bit**, Sigma-Delta **ADC** with PGA and Reference. All signal conditioning and excitation is performed by the AD7124-8, no additional components are needed. | The EVAL-CN0391-ARDZ shield uses the [[adi>en/products/analog-to-digital-converters/precision-adc-10msps/ad7124-8| AD7124-8 part]] which is a **8-Channel** Low Noise, Low Power, **24-Bit**, Sigma-Delta **ADC** with PGA and Reference. All signal conditioning and excitation is performed by the AD7124-8, no additional components are needed. |
| |
{{ :resources:eval:user-guides:arduino-uno:reference_designs:img_20180123_170932.jpg?600 |}} | {{ :resources:eval:user-guides:arduino-uno:reference_designs:img_20180123_170932.jpg?600 |}} |
\\ | \\ |
<note> | <note> |
The second approximation formula was implemented for [[http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0382.html|CN0382 circuit]], using data gathered in a smaller temperature range: 0°C to 105°C. | The second approximation formula was implemented for [[adi>en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0382.html|CN0382 circuit]], using data gathered in a smaller temperature range: 0°C to 105°C. |
</note> | </note> |
| |