This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:agilenet6t [09 Nov 2018 11:51] – Mahendravarman rajarao | resources:eval:user-guides:agilenet6t [24 Sep 2019 08:31] (current) – [Additional resources] Aditya S | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AgileNet 6T Wireless Networking Protocol Solutions ====== | + | ====== AgileNet 6T (AN6T) |
- | AgileNet 6T is a long range Sub-GHz wireless networking solution | + | AgileNet 6T is a long range Sub-GHz wireless networking solution |
- | AgileNet 6T is based on 6TiSCH. 6TiSCH is combining the performance of IEEE802.15.4e TSCH with an IPv6-enabled upper stack. TSCH aims at reducing the impact of the wireless medium unpredictability to enable the use of reliable low-power wireless networks. It is very good at saving the nodes' energy because each node shares a schedule, allowing it to know in advance when to turn on or off its radio. The IEEE 802.15.4 standard uses different frequency band, and each frequency band is separated in channels. In TSCH, communications are done using those different channels and at different times. | + | AgileNet 6T is based on 6TiSCH. 6TiSCH is combining the performance of IEEE802.15.4e TSCH with an IPv6-enabled upper stack. The IEEE 802.15.4 standard uses different frequency band, and each frequency band is separated in channels. In TSCH, communications are done using those different channels and at different times. However, IEEE 802.15.4 standard does not define how to build and maintain the communication schedule. AN6T Wireless networking solution defines to organize the communication schedule in a distributed way. |
+ | ===== AN6T Wireless Solution Architecture ===== | ||
+ | |||
+ | {{: | ||
+ | ===== Features and Specifications ===== | ||
+ | * Reliable Mesh Network | ||
+ | * Data rate around 50Kbps | ||
+ | * Payload size 90 bytes | ||
+ | * Range: Indoors & Outdoors - To be Measured | ||
+ | * OTA Support | ||
+ | * Secured Communication | ||
+ | ===== AN6T Stack Architecture ===== | ||
+ | |||
+ | {{: | ||
+ | |||
+ | |||
+ | ===== AgileNet-6T software package ===== | ||
+ | |||
+ | ==== Installing the AgileNet-6T software package ==== | ||
+ | Download the AgileNet-6T software by filling in the request form at https:// | ||
+ | - Fill in the requested information under the Software Recipient Information and Commercial information sections. | ||
+ | - Under the Software requested section, set Target hardware to Ultra Low Power Microcontrollers, | ||
+ | - After the request is approved, a link to download the software is sent to the provided email address. | ||
+ | - Use the link to install the AgileNet-6T software package. | ||
+ | |||
+ | ===== Additional resources ===== | ||
+ | * Evaluation kits | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * Hardware | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | |