This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adum770x [04 Apr 2019 17:04] – [Overview] Applications should be a title Istvan Csomortani | resources:eval:user-guides:adum770x [20 Jan 2022 17:25] (current) – [Downloads] z zg | ||
---|---|---|---|
Line 32: | Line 32: | ||
User can configure the corresponding interface type, by setting the **adc_port_type** Tcl variable in the system_project.tcl file. Note that this variable should be set before generating any bit file. | User can configure the corresponding interface type, by setting the **adc_port_type** Tcl variable in the system_project.tcl file. Note that this variable should be set before generating any bit file. | ||
- | The output of the device is a continuous digital bit stream, to reconstruct the original input signal information, | + | The output of the device is a continuous digital bit stream, to reconstruct the original input signal information, |
< | < | ||
Line 79: | Line 79: | ||
* {{https:// | * {{https:// | ||
</ | </ | ||
+ | bbbbbbbb |