This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adum770x [03 Apr 2019 09:37] – Update the overveiw with the latest informations from the datasheet Istvan Csomortani | resources:eval:user-guides:adum770x [20 Jan 2022 17:25] (current) – [Downloads] z zg | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADuM7701 - No-OS Driver | + | ====== ADuM7701 - Reference Design |
+ | |||
+ | ==== Supported Devices | ||
- | ===== Supported Devices ===== | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | |||
+ | ==== Supported Carrier Board ==== | ||
+ | |||
+ | * [[http:// | ||
===== Overview ===== | ===== Overview ===== | ||
Line 14: | Line 19: | ||
The serial interface is digitally isolated. High speed complementary metal-oxide semiconductor (CMOS) technology, combined with monolithic transformer technology, results in the on-chip isolation providing outstanding performance characteristics, | The serial interface is digitally isolated. High speed complementary metal-oxide semiconductor (CMOS) technology, combined with monolithic transformer technology, results in the on-chip isolation providing outstanding performance characteristics, | ||
- | Applications: | + | ==== Applications |
* Shunt current monitoring | * Shunt current monitoring | ||
* AC motor controls | * AC motor controls | ||
Line 23: | Line 28: | ||
===== HDL Reference Design ===== | ===== HDL Reference Design ===== | ||
- | The provided HDL reference design support' | + | The provided HDL reference design support' |
User can configure the corresponding interface type, by setting the **adc_port_type** Tcl variable in the system_project.tcl file. Note that this variable should be set before generating any bit file. | User can configure the corresponding interface type, by setting the **adc_port_type** Tcl variable in the system_project.tcl file. Note that this variable should be set before generating any bit file. | ||
- | The output of the device is a continuous digital bit stream, to reconstruct the original input signal information, | + | The output of the device is a continuous digital bit stream, to reconstruct the original input signal information, |
< | < | ||
Line 74: | Line 79: | ||
* {{https:// | * {{https:// | ||
</ | </ | ||
+ | bbbbbbbb |