Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:adrv9009-zu11eg:hardware [20 Sep 2021 11:15] – [High level block diagram showing key components and IO routing] Claudia Gogaresources:eval:user-guides:adrv9009-zu11eg:hardware [24 May 2022 19:55] (current) Brian OLoughlin
Line 106: Line 106:
 === Programmable Logic GPIOs === === Programmable Logic GPIOs ===
 == High Performance GPIOs == == High Performance GPIOs ==
-Programmable logic high performance banks 65, 67 and 68 are fully accessible in connector P2. Prior of using these signals the bank supply VCCO must be provided, with a voltage between 0.95V and 1.9V. A reference voltage must be applied as well, if the IO standard requires one. To use the internal VREF voltage a 500 or 1K resistor needs to be connected from VREF pin to ground.+Programmable logic high performance banks 65, 67 and 68 are fully accessible in connector P2. Prior of using these signals the bank supply VCCO must be provided, with a voltage between 0.95V and 1.9V. A reference voltage must be applied as well, if the IO standard requires one. To use the internal VREF voltage a 500 or 1KOhm resistor needs to be connected from VREF pin to ground.
 == High Density GPIOs  == == High Density GPIOs  ==
 Programmable logic High density bank 89 is partially available in connector P2. Connect a voltage between 1.14V and 3.4V to the bank supply voltage VCCO_89. Programmable logic High density bank 89 is partially available in connector P2. Connect a voltage between 1.14V and 3.4V to the bank supply voltage VCCO_89.
Line 169: Line 169:
 <note important>The ADRV9009-ZU11EG RF-SOM requires active cooling. It includes overtemperature protection, which interrupts power to the RF-SOM when board temperature reaches 90degC. Without a fan the RF-SOM will turn off in a few minutes under normal operating conditions (25degC ambient, Linux machine running). </note> <note important>The ADRV9009-ZU11EG RF-SOM requires active cooling. It includes overtemperature protection, which interrupts power to the RF-SOM when board temperature reaches 90degC. Without a fan the RF-SOM will turn off in a few minutes under normal operating conditions (25degC ambient, Linux machine running). </note>
  
-Included in the ADRV9009-ZU11EG RF-SOM package is a custom designed heat spreader plate, that acts as a mounting base for an active cooler. The Panasonic EYG-T7070A10A thermal pad, which is included in the package should be used as contact area between Xilinx Ultrascale+ package and heat spreader plate.+The ADRV9009-ZU11EG RF-SOM comes equipped with a custom designed heat spreader plate, that acts as a mounting base for an active cooler. Panasonic EYG-T7070A10A thermal pad is used between RF-SOM and plate.
  
  
Line 175: Line 175:
  
  
-The [[adi>ADRV2CRR-FMC]] kit includes a heatsink with active cooler for the ADRV9009-ZU11EG RF-SOM, and Würth Elektronik 39410 EMI gasket sheet, that acts both as thermal transfer material between heat plate and heatsink and RF Shield/Absorber. +The [[adi>ADRV2CRR-FMC]] kit includes a heatsink with fan for the ADRV9009-ZU11EG RF-SOM, and Würth Elektronik 39410 EMI gasket sheet, that acts both as thermal transfer material between plate and heatsinkand RF Shield/Absorber. 
  
 ---- ----
 +==== Supplementary Testing ====
 +
 +<WRAP round download>
 +EMC testing has been carried out on the SOM. This may be useful as a reference for validation or qualification of custom designs. The report can be found here:
 +  * {{:resources:eval:user-guides:adrv9009_zu11eg:ADRV9009-ZU11EG EMC Conformance.pdf|EMC Test report}}
 +
 +</WRAP>
 +
 +----
 +
 ==== Mechanical Reference Material ==== ==== Mechanical Reference Material ====
 <WRAP round download> <WRAP round download>
Line 199: Line 209:
 ---- ----
 ==== ADRV9009-ZU11EG Schematics, BOM & Errata ==== ==== ADRV9009-ZU11EG Schematics, BOM & Errata ====
-Rev C is the latest and is in mass production.+Rev C is the latest available version.
 <WRAP round download> <WRAP round download>
     * {{:resources:eval:user-guides:adrv9009_zu11eg:02-048949-01-c.pdf|Rev C Schematics}}     * {{:resources:eval:user-guides:adrv9009_zu11eg:02-048949-01-c.pdf|Rev C Schematics}}
     * {{:resources:eval:user-guides:adrv9009_zu11eg:05-048949-01-c.zip|Rev C BOM}}     * {{:resources:eval:user-guides:adrv9009_zu11eg:05-048949-01-c.zip|Rev C BOM}}
     * {{:resources:eval:user-guides:adrv9009_zu11eg:revb_to_revc_errata.xlsx|Rev B to Rev C Errata}}     * {{:resources:eval:user-guides:adrv9009_zu11eg:revb_to_revc_errata.xlsx|Rev B to Rev C Errata}}
 +    * {{ :resources:eval:user-guides:adrv9009-zu11eg:letter_of_volatility_adrv9009-zu11eg.pdf|Rev C Letter of Volatility}}
 </WRAP> </WRAP>
  
resources/eval/user-guides/adrv9009-zu11eg/hardware.txt · Last modified: 24 May 2022 19:55 by Brian OLoughlin