This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:adin1300-and-adin1200:phy_faq [06 Oct 2022 16:22] – [Do the Exposed Pad and Bus Bars have to be soldered down?] Mark Bolger | resources:eval:user-guides:adin1300-and-adin1200:phy_faq [16 Jan 2023 10:37] (current) – Added section for MDI pins in Unpowered device Mark Bolger | ||
---|---|---|---|
Line 191: | Line 191: | ||
When comparing PHY devices, ensure to check whether the output stage is voltage mode or current mode and also review whether the power consumption figures for current mode include the current dissipated in the transformer as a result of termination resistors. | When comparing PHY devices, ensure to check whether the output stage is voltage mode or current mode and also review whether the power consumption figures for current mode include the current dissipated in the transformer as a result of termination resistors. | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Connecting a Cable to an Unpowered Device ===== | ||
+ | |||
+ | The ADIN1300 and ADIN1200 have internal protection circuitry on the MDI pins that will protect them from damage when standard ethernet traffic is sent into an unpowered device from a remote active device. | ||
---- | ---- |