This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:adin1300-and-adin1200:adin1300-ieee-compliance-test-mode-access [09 Feb 2022 12:50] – template added Mark Bolger | resources:eval:user-guides:adin1300-and-adin1200:adin1300-ieee-compliance-test-mode-access [18 Feb 2022 13:18] (current) – Remove Prelim at top Mark Bolger | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
+ | ===== Overview ===== | ||
- | <WRAP group> | + | The purpose of this application note is to describe the configuration of the ADIN1300 for the various Ethernet PHY compliance test modes as set out by IEEE802.3. |
- | <WRAP half column> | + | |
- | ====== Overview ====== | + | |
- | This PHY exchange guide captures pertinent information to support migration from the TI DP83867IR/ | + | The ADIN1300 |
- | The ADIN1300 has compelling reasons | + | |
- | {{: | + | ==== Testing Equipment |
- | The ADIN1300 | + | When performing this testing, user will need Ethernet |
- | The following sections detail the modifications at the schematic level required to migrate from a DP83867 device to the ADIN1300 device. Including a description of differences corresponding to each functional group of pins and differences | + | |
- | The ADIN1300 datasheet provides a detailed description | + | |
+ | Once equipment is in place and hardware powered and connected to the test fixture, configure the PHY through the MDIO interface to set the required test mode and use the compliance software to record and report the results. | ||
- | ===== Hardware Changes By Function ===== | + | ==== Reset Between Tests ==== |
- | ==== Power Supplies Overview ==== | + | To ensure the device is in a known state, either start from a power cycle or alternatively, |
- | Both devices require a minimum of 2 power supply rails, where the VDDIO is connected to the same power supply voltage as the MAC or as the PHY analog supply AVDD_3P3 | + | * GE_SFT_RST_CFG_EN.Write(0b1) - Register 0xFF0D |
+ | * GE_SFT_RST. Write(0b1) - Register 0xFF0C subsystem reset | ||
- | {{: | + | ==== Extended Register Addressing ==== |
- | The ADIN1300 | + | The ADIN1300 |
- | Decoupling requirements for each device differ as described in Table 2 | + | If using Clause 22 access, write the 16-bit register address into the EXT_REG_PTR register and then read or write the EXT_REG_DATA register. |
- | {{: | + | ---- |
+ | ===== 1000BASE-T Testing ===== | ||
+ | ==== IEEE Test Modes ==== | ||
+ | The ADIN1300 supports the IEEE test modes, Test Mode 1, Test Mode 2, Test Mode 3 and Test Mode 4 used for 1000BASE-T IEEE compliance testing. An IEEE test mode can be selected by writing to register address 9, bits 15:13. The TST_MODE bit field can be used to select the transmit test waveforms required for Gigabit IEEE compliance testing. | ||
+ | * Test Mode 1 is used for testing of the 1000BASE-T transmitter waveform. | ||
+ | * Test Mode 2 and 3 are used for testing of the 1000BASE-T transmitter jitter. | ||
+ | * Test Mode 4 is used testing of the 1000BASE-T transmitter distortion. | ||
- | ==== RESET Operation | + | ==== 1000BASE-T Test Modes (Master Slave Control Register) |
- | Both devices have a RESET_N pin which initializes | + | Address: 0x09: Reset, 0x0200, Name: MSTR_SLV_CONTROL |
- | The ADIN1300 includes power monitoring circuitry to monitor all of the supplies. At power-up, the ADIN1300 is held in hardware reset until each of the supplies has crossed its minimum rising threshold value. | + | This address corresponds to the MASTER-SLAVE Control register specified in clause 40.5.1.1 of IEEE Std 802.3. Only Test mode bits are show in table below, refer to datasheet register map for further detail. |
- | The hardware strapping pins are read and updated at the de-assertion of reset for both devices. For the ADIN1300, the RESET_N pin resides in the AVDD_3P3 voltage domain. | + | {{ : |
- | In applications where the MAC interface is powered from VDDIO of 1.8V, level shifting of the RESET_N signal applied to the ADIN1300 may be required to ensure the voltage level on the RESET_N pin is in excess of the minimum input high threshold level. | + | |
- | The DP83867 requires external control over the RESET_N pin during power up and a much longer time to when the management registers are accessible. If the RESET_N pin is connected to a host controller, then the PHY must be held in reset for a minimum of 200 ms after the last supply powers up. If the host controller cannot be connected to RESET_N, then a 100-Ω resistor | + | |
- | ==== Clocking ==== | ||
- | A 25 MHz crystal or external clock source is used to provide the reference clock for both devices. A crystal can be connected to pins XTAL_I/ | ||
- | In RMII mode, the ADIN1300 expects an external 50 MHz REF_CLK provided to the XTAL_I/ | ||
+ | ==== TEST MODE 1: TRANSMIT WAVEFORM TEST ==== | ||
+ | This test mode is used for a number of tests as follows: | ||
+ | - To verify the PHY transmit waveforms fit the IEEE defined templates. | ||
+ | - To verify the PHY transmitter output voltage levels are in range | ||
+ | - To verify the PHY transmitter output voltage droop is in range | ||
+ | To configure the device in Test Mode 1, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(1) - Register 0x0009, bit 15:13: Enable Test Mode 1 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000, bit 11: Bring PHY out of Software | ||
- | ==== Bias Resistor | + | ==== TEST MODE 2 & 3 ==== |
- | An external resistor | + | This test mode is used to ensure the TX_TCLK jitter with respect to an un-jittered |
+ | Note the ADIN1300 | ||
+ | To configure the device in Test Mode 2, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(2) - Register 0x0009, bits 15:13: Enable Test Mode 2 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000, bit 11: Bring PHY out of Software Power Down | ||
+ | To configure the device in Test Mode 3, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(3) - Register 0x0009, bits 15:13: Enable Test Mode 3 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000, bit 11: Bring PHY out of Software Power Down | ||
- | {{: | ||
- | ==== Media Dependent Interface (MDI) ==== | + | ==== TEST MODE 4 ==== |
- | The ADIN1300 has voltage | + | This test mode is used |
- | The recommended external circuit for the interface to the magnetics and RJ-45 is shown in Figure 2. | + | |
+ | | ||
+ | - To verify | ||
+ | To configure the device in Test Mode 4, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(4) - Register 0x0009, bits 15:13. Enable Test Mode 4 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11: Bring PHY out of Software Power Down | ||
- | </ | + | ---- |
- | <WRAP half column> | ||
- | {{: | + | ===== 100BASE-TX ===== |
- | ==== MDIO/ | + | For 100BASE-TX operation there are a variety of tests. There are two main test modes main register involved here is the B_100_TX_TST_MODE register at address 0xB413 |
- | + | ||
- | Both devices support the IEEE management interface using the MDIO/MDC pins and require | + | |
- | Both devices provide an interrupt pin, INT_N (¯INT). This pin requires a 1.5 kΩ pull-up resistor to VDDIO. The DP83867 recommends 2.2kΩ pull-up resistors for their interrupt pin. | + | |
- | ==== LED Function | + | ==== 100BASE-TX Transmit Test Mode Register |
- | The ADIN1300 support two LED pins on LED_0 and LINK_ST. The LED_0 has programmability of LED functions, with different blinking operation possible through MDIO configuration, the default mode is ON when Link is Up, blink if activity. The LINK_ST provides static information about Link up or down status. | + | Address: 0xB413, Reset: 0x0000, Name: B_100_TX_TST_MODE |
- | The DP83867 supports 3 LEDs pins 45, 46, 47 (QFN) or pins 61, 62, 63 (QFP) in addition | + | This register provides |
- | Both devices use these pins for strapping purposes. | + | |
+ | {{ : | ||
- | + | To configure | |
- | === LED Circuit === | + | * MII_CONTROL.Write(0x2900) - Register 0x0000 to place the device into Software PD, configure 100BASE-TX full duplex, autoneg disabled |
- | + | * PHY_CTRL_1.AUTO_MDI_EN.Write(0b) - Register 0x0012, bit 10: Disable Auto MDI/MDIX | |
- | The ADIN1300 LED_0 operates from the AVDD_3P3 voltage domain, therefore can support driving LEDs even when the MAC interface is running at the lower voltage of 1.8V. | + | * PHY_CTRL_1.MAN_MDIX.Write(0b0) |
- | The default LED operation is on if the Link is up and blinks when there is activity, this operation can be reprogrammed through MDIO write. | + | * B_100_TX_TST_MODE.Write(1/ |
- | For the LED_0 of the ADIN1300, it can be configured with 4-level strapping. The strapping configuration will have an impact on how the LED function operates and needs to be considered if the LED pins are used to directly drive an LED. If the strap pin is pulled high by the strapping resistors, | + | * PHY_CTRL_3. LINK_EN.Write(0b1) - Register 0x0017, bit 13: Enable linking |
- | + | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 | |
- | {{: | + | |
- | + | ||
- | === Link Status, LINK_ST === | + | |
- | + | ||
- | + | ||
- | The ADIN1300 has a dedicated LINK_ST pin to provide information to the MAC on the status of the Link. By default, the LINK_ST pin goes high indicating the link is up and low to indicate the link is down. The LINK_ST polarity is programmable by setting the bit high GE_LNK_STAT_INV_EN. | + | |
- | The LINK_ST could be used to drive an LED, however it resides in the VDDIO voltage domain, therefore, when driving an LED in an integrated RJ45 jack where the PHY VDDIO is 1.8V, level shifting will be required. This can be done using a FET. | + | |
- | + | ||
- | + | ||
- | </ | + | |
- | </ | + | |
- | + | ||
---- | ---- | ||
- | <WRAP group> | ||
- | <WRAP half column> | ||
- | ==== MAC Interface ==== | ||
- | The ADIN1300 supports RGMII, MII and RMII MAC interface modes. The following sections describe the RGMII, MII and RMII interfaces for both devices. | + | ===== 10BASE-TE/ |
- | === RGMII Interface | + | |
- | The RGMII interface is the communication path between | + | When operating in 10 Mbps speeds, |
- | Both devices support the internal delay on the clocks. By default, the ADIN1300 | + | The 10BASE-Te/T compliance tests are: |
+ | * Link Pulse Testing | ||
+ | * Medium Attachment Unit (MAU) | ||
+ | * TP_IDL | ||
+ | * Jitter | ||
+ | * Differential Voltage | ||
+ | * Harmonics | ||
+ | * Transmitter Return Loss | ||
+ | * Receiver Return Loss | ||
+ | * Common-Mode Voltage | ||
+ | The B_10_TX_TST_MODE register | ||
- | {{: | ||
- | === MII Interface | + | ==== 10BASE-T Transmit Test Mode Register ==== |
- | The MII interface is the communication path between the PHY and MAC devices. The MII interface has a high pin count, with a total of 15 pins for data transmission, | ||
- | When using the ADIN1300 in MII mode, the multifunction pin “LED_0/ | ||
- | </ | + | Address: 0xB412, Reset: 0x0000, Name: B_10_TX_TST_MODE |
+ | This register provides the ability to transmit a 10BASE-T test signal. | ||
- | <WRAP half column> | + | {{ : |
- | The ADIN1300 sub-system registers provide | + | |
- | Note, the DP83867IR only support MII mode with the 64-QFP 12x12 mm package. | + | |
- | {{: | + | To configure the device for 10BASE-T transmit test mode, consisting of 5MHz square wave on desired dimension, issue the following writes over MDIO |
+ | * GE_SFT_RST_CFG_EN.Write(0b1) - Register 0xFF0D to ensure the hardware configuration is refreshed. | ||
+ | * GE_SFT_RST. Write(0b1) - Register 0xFF0C subsystem reset | ||
+ | * MII_CONTROL.SFT_RST. Write(0b1) - Register 0x0000 Issue a software reset, this bit is self clearing | ||
+ | * MII_CONTROL.Write(0x0900) | ||
+ | * B_10_TX_TST_MODE.Write(0b100) | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 Bring PHY out of Software | ||
- | === RMII Interface === | + | An alternative configuration, |
+ | * GE_SFT_RST_CFG_EN.Write(0b1) - Register 0xFF0D to ensure the hardware configuration is refreshed. | ||
+ | * GE_SFT_RST. Write(0b1) - Register 0xFF0C subsystem reset | ||
+ | * MII_CONTROL.SFT_RST. Write(0b1) - Register 0x0000 bit 15, Issue a software reset, this bit is self clearing | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11, Bring PHY out of Software | ||
+ | * PHY_CTRL_1.DIAG_CLK_EN.Write(0b1) - Register 0x0012 bit 2, Enable the Diagnostic Clock | ||
+ | * MII_CONTROL.LOOPBACK.Write(0b1) - Register 0x0000 bit 14, Enable Loopback | ||
+ | * PHY_CTRL_1.MAN_MDIX.Write(0b0) - Register 0x0012 bit 9, Operate in MDI configuration | ||
+ | * PHY_CTRL_STATUS_1.LB_TX_SUP.Write(0b0) - Register 0x0013 bit 6, Stop suppressing the transmit signal at the MDI pins in all digital loopback | ||
+ | * PHY_CTRL_STATUS_1.LB_ALL_DIG_SEL.Write(0b1) - Register 0x0013 bit12 Enable all digital loopback | ||
+ | * PHY_CTRL_3. LINK_EN.Write(0b1) - Register 0x0017 bit 13, Enable linking | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11, Bring PHY out of Software | ||
+ | * Wait for Link up | ||
+ | * FG_CONT_MODE_EN.Write(0b1) - Register 0x9417 Enable the frame generator into continuous mode | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(1) - Register 0x9416, bits 2:0: Enable random number in the MAC client data frame field, options of decrementing, | ||
+ | * FG_EN.FG_EN.Write(1) - Enable Frame Generator | ||
+ | Setup for 10BASE-T forced mode in loopback with Tx suppression disabled, with transmission of frames with random payloads using the frame generator, | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b011) - 0xFF repeating payloads | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b010) - 0x00 repeating payloads | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b100) - alternative 0x55 payloads | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b101) - data field decrementing from 255 to 0(decimal) | ||
- | The DP83867 does not support | + | 10BASE-T is configured by writing |
- | {{: | + | * B_10_E_EN.Write(0x0) |
- | In RMII mode, the ADIN1300 requires an external 50MHz clock applied | + | |
- | |||
- | </ | ||
- | </ | ||
---- | ---- | ||
+ | ===== Testing Using ADI Evaluation GUI ===== | ||
- | <WRAP group> | + | The ADI evaluation board uses small MDIO dongle board for USB to MDIO communications and the accompanying GUI provides access to the various Test modes from the “Test Mode” tab. Select the relevant test mode to configure and “Execute Test”. In the “Activity log” the register writes can be observed. |
- | <WRAP half column> | + | |
- | ==== Output Clocks ==== | + | {{ : |
- | The ADIN1300 provides a 25 MHz output reference clock on the REF_CLK pin. This can be used a 25 MHz input reference clock for another PHY device. | ||
- | The ADIN1300 can optionally provide a number of clock signals on the GP_CLK pin. This is configured via MDIO writes and the clocks available are a 125 MHz free running clock, 25 MHz clock and 25 MHz/125 MHz recovered clock. | ||
- | |||
- | ===== Hardware Configuration ===== | ||
- | |||
- | Both devices have a number of strapping options to enable managed or unmanaged configurations of the PHY function such as PHY address, mode of operation, Auto-Negotiation and MAC Interface. | ||
- | After power on, the strapping pin voltages get sensed and latched upon existing from a reset and the sensed voltages are used to set the personality of the PHY. | ||
- | When configuring any strapping configurations, | ||
- | The DP83867 uses 4-level strapping options throughout, while the ADIN1300 uses a mix of 2-level and 4-level. In general, strapping pins are multi-functional and have different operation after the device is brought out of reset. The ADIN1300 has internal pull downs on many of its strapping pins (not all), therefore it would be possible to minimize external strapping resistors. | ||
- | |||
- | {{: | ||
- | |||
- | {{: | ||
- | |||
- | Strapping configurations are very specific to the device, consult the respective datasheets to determine the exact configuration for required use case. | ||
- | The DP83867 has internal 9 kΩ pulldown resistors on all pins used for strapping functions. | ||
- | |||
- | {{: | ||
- | |||
- | ==== Hardware Configuration of Speed ==== | ||
- | |||
- | For the ADIN1300, speed configuration is done using two pins, PHY_CFG0 and PHY_CFG1. These pins do not have any internal pull resistors, therefore external strapping is required. Both pins support 4-level strapping, providing much flexibility in terms of the possible combinations, | ||
- | |||
- | </ | ||
- | |||
- | <WRAP half column> | ||
- | |||
- | {{: | ||
- | {{: | ||
- | |||
- | ==== Hardware Configuration of Auto-MDIX ==== | ||
- | |||
- | Selection of Auto-MDIX for the ADIN1300 is done using one pin, (MDIX_MODE) with 4-level strapping. | ||
- | |||
- | {{: | ||
- | |||
- | ==== MAC Interface Selection ==== | ||
- | |||
- | The ADIN1300 uses two hardware pins, MACIF_SEL0 and MACIF_SEL1 to provide user ability to select different MAC interfaces. These two pins have internal weak pull downs, therefore the default operation would be RGMII with delays as shown in Table 12. To configure any other MAC interface mode, use 10kΩ pull up or pull down resistors to select accordingly. | ||
- | {{: | ||
- | |||
- | ==== Hardware Configuration of PHY Address ==== | ||
- | |||
- | Both devices have a default strapping providing a PHY address of 0x0000. | ||
- | The ADIN1300 uses two-level strapping for the four PHY address pins, either pull high or low to configure the PHY address, with an option of 16 unique addresses possible. Two level strapping provides a very robust PHY addressing scheme. | ||
- | The DP83867 provides four level strapping for the PHY address pins, capable of 16 unique address when using the QFN device or 32 when using the QFP. | ||
- | When configuring any strapping configurations, | ||
- | |||
- | |||
- | |||
- | |||
- | </ | ||
- | </ | ||
- | |||
- | <WRAP center round important 60%> | ||
- | Strapping configurations are very specific to the device, consult the respective datasheets to determine the exact configuration for required use case. | ||
- | </ | ||
---- | ---- | ||
- | |||
- | <WRAP group> | ||
- | <WRAP half column> | ||
- | ===== Package ===== | ||
- | |||
- | The ADIN1300 is available in a 40 lead LFCSP (6 mm x 6 mm footprint). The DP83867 is available in two package options, 48 lead QFN (7 mm x 7 mm) and 64 pin QFP (12 mm x 12 mm). Due to the smaller package footprint and differing pinout, the ADIN1300 is not a drop-in replacement for the DP83867 product. It will require a re-spin of schematic and board layout to achieve this exchange. | ||
- | |||
- | {{: | ||
- | |||
- | The DP83867 requires the 64-QFP (12 mm x 12 mm) option to support MII or RMII interface. | ||
- | |||
- | {{: | ||
- | |||
- | The underside of the LFCSP package for the ADIN1300 includes an exposed paddle which should be soldered directly to the board with an array of vias for thermal purposes. There are also two exposed stripes adjacent to the exposed paddle. These do not need to be soldered to the board, they should be treated as a keep out area as they are connected to supply rails in the device, therefore should not be tied to ground and there should be no routing or traces on the PCB layer directly underneath them. | ||
- | ===== Other Pinout Considerations ===== | ||
- | |||
- | ==== Integrated MDI Termination ==== | ||
- | |||
- | Both devices include integrated termination resistors on the MDI paths. These are voltage mode PHYs, no external resistors are required for biasing and no supply voltage is required at the center tap of the transformer. | ||
- | |||
- | </ | ||
- | |||
- | <WRAP half column> | ||
- | |||
- | ==== RGMII Drive/ | ||
- | |||
- | The ADIN1300 provides user with ability to adjust the RGMII drive current through the GE_RGMII_IO_CNTRL register. | ||
- | |||
- | ==== MII ==== | ||
- | The ADIN1300 also supports MII MAC interface mode in the standard 40-QFN (6 mm x 6mm) package for 10/100M operation. The DP83867 must use the 64-QFP (12 mm x 12 mm) package. | ||
- | ==== RMII ==== | ||
- | The ADIN1300 also supports RMII MAC interface mode for 10/100M operation. The DP83867 does not support the RMII interface. | ||
- | ==== SGMII ==== | ||
- | The DP83867 supports SGMII interface in the CS/E/IS variants. The ADIN1300 does not support SGMII interface. | ||
- | ==== GMII ==== | ||
- | The DP83867 supports GMII interface in the 64-lead QFP (12 mm x 12 mm) package option. The ADIN1300 does not support GMII interface. | ||
- | |||
- | ===== Software Considerations ===== | ||
- | |||
- | Both devices can be hardware strapped to be used in an unmanaged configuration. Alternatively, | ||
- | Registers 0x0 to 0xF are common across all PHYs. | ||
- | |||
- | ==== Linux Driver ==== | ||
- | |||
- | The ADIN1300 has a Linux Driver available in the Linux mainline kernel. The ADIN1300 linux driver detail is captured here: | ||
- | https:// | ||
- | |||
- | |||
- | |||
- | </ | ||
- | </ | ||
- | <note tip>The ADIN1300 has a Linux Driver available in the Linux mainline kernel.</ | ||
- | |||
- | ===== Side by Side Package/ | ||
- | |||
- | |||
- | The following is a side-by-side comparison of the package and pinouts, showing the position of the corresponding functional pins on each device | ||
- | {{: | ||
- | ---- | ||
- | ===== Feature Comparison Table ===== | ||
- | {{: | ||
- | ===== Example Configuration for RGMII ===== | ||
- | |||
- | The following example captures how to configure the ADIN1300 for an unmanaged configuration with RGMII Interface, operating in Auto Negotiation mode advertising all speeds. The PHY will power up in this state, ready to establish a link with a link partner. | ||
- | The MAC interface configuration pins (MACIF_SEL0/ | ||
- | |||
- | The following list summarizes an RGMII auto negotiate, 10 Mbps, 100 Mbps, or 1000 Mbps with full duplex or half duplex, with the software power-down enabled after reset: | ||
- | * MAC Interface = RGMII with 2ns delay on RXC/TXC | ||
- | * MACIF_SEL0 = MODE_1 = 10 kΩ pull-down resistor | ||
- | * MACIF_SEL1 = MODE_1 = 10 kΩ pull-down resistor | ||
- | * MDIX_MODE = automatic MDIX, preferred MDI | ||
- | * MDIX_MODE = MODE_4 | ||
- | * PHY address = 0b0001 | ||
- | * Speed selection = 10 Mbps, 100 Mbps, or 1000 Mbps with full duplex or half duplex, automatic negotiate enabled | ||
- | * PHY_CFG0 = MODE_4 = 10 kΩ pull-up resistor | ||
- | *PHY_CFG1 = MODE_1 = 10 kΩ pull-down resistor | ||
- | |||
- | {{: |