This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:adin1300-and-adin1200:adin1300-ieee-compliance-test-mode-access [09 Feb 2022 12:49] – created Mark Bolger | resources:eval:user-guides:adin1300-and-adin1200:adin1300-ieee-compliance-test-mode-access [18 Feb 2022 13:18] (current) – Remove Prelim at top Mark Bolger | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | Placeholder | + | |
+ | ====== Configuring the ADIN1300 for Ethernet PHY Compliance Test Modes ====== | ||
+ | |||
+ | ===== Overview ===== | ||
+ | |||
+ | The purpose of this application note is to describe the configuration of the ADIN1300 for the various Ethernet PHY compliance test modes as set out by IEEE802.3. | ||
+ | |||
+ | The ADIN1300 supports the IEEE test modes, Test Mode 1, Test Mode 2, Test Mode 3 and Test Mode 4 used for 1000BASE-T IEEE compliance testing. The ADIN1300 has some additional test modes that are useful for 10BASE-T and 100BASE-TX compliance testing. Details of the registers, sequences of writes are captured in this document. Use this application note in conjunction with the product datasheet. | ||
+ | |||
+ | ==== Testing Equipment and Setup ==== | ||
+ | |||
+ | When performing this testing, user will need Ethernet compliance test fixture and associated Ethernet physical layer compliance software. There are a number of vendors provide Ethernet Compliance test equipment. For ADI in-house validation, we used Tektronix TDSET3 compliance software in addition to having UNH (University of New Hampshire perform compliance testing). | ||
+ | |||
+ | Once equipment is in place and hardware powered and connected to the test fixture, configure the PHY through the MDIO interface to set the required test mode and use the compliance software to record and report the results. | ||
+ | |||
+ | ==== Reset Between Tests ==== | ||
+ | |||
+ | To ensure the device is in a known state, either start from a power cycle or alternatively, | ||
+ | |||
+ | * GE_SFT_RST_CFG_EN.Write(0b1) - Register 0xFF0D to ensure the hardware configuration is refreshed. | ||
+ | * GE_SFT_RST. Write(0b1) - Register 0xFF0C subsystem reset | ||
+ | |||
+ | ==== Extended Register Addressing ==== | ||
+ | |||
+ | The ADIN1300 supports a range of extended management interface registers which can be accessed using Clause 45 access or alternatively using Clause 22 access through the EXT_REG_PTR (address 0x0010) and EXT_REG_DATA (address 0x0011), these registers provide user ability to read/write to the extended register space (any register greater than 0x001F) indirectly. | ||
+ | If using Clause 22 access, write the 16-bit register address into the EXT_REG_PTR register and then read or write the EXT_REG_DATA register. | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== 1000BASE-T Testing ===== | ||
+ | |||
+ | ==== IEEE Test Modes ==== | ||
+ | |||
+ | The ADIN1300 supports the IEEE test modes, Test Mode 1, Test Mode 2, Test Mode 3 and Test Mode 4 used for 1000BASE-T IEEE compliance testing. An IEEE test mode can be selected by writing to register address 9, bits 15:13. The TST_MODE bit field can be used to select the transmit test waveforms required for Gigabit IEEE compliance testing. | ||
+ | * Test Mode 1 is used for testing of the 1000BASE-T transmitter waveform. | ||
+ | * Test Mode 2 and 3 are used for testing of the 1000BASE-T transmitter jitter. | ||
+ | * Test Mode 4 is used testing of the 1000BASE-T transmitter distortion. | ||
+ | |||
+ | ==== 1000BASE-T Test Modes (Master Slave Control Register) ==== | ||
+ | |||
+ | Address: 0x09: Reset, 0x0200, Name: MSTR_SLV_CONTROL | ||
+ | This address corresponds to the MASTER-SLAVE Control register specified in clause 40.5.1.1 of IEEE Std 802.3. Only Test mode bits are show in table below, refer to datasheet register map for further detail. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | ==== TEST MODE 1: TRANSMIT WAVEFORM TEST ==== | ||
+ | |||
+ | This test mode is used for a number of tests as follows: | ||
+ | - To verify the PHY transmit waveforms fit the IEEE defined templates. | ||
+ | - To verify the PHY transmitter output voltage levels are in range | ||
+ | - To verify the PHY transmitter output voltage droop is in range | ||
+ | To configure the device in Test Mode 1, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(1) - Register 0x0009, bit 15:13: Enable Test Mode 1 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000, bit 11: Bring PHY out of Software | ||
+ | |||
+ | ==== TEST MODE 2 & 3 ==== | ||
+ | |||
+ | This test mode is used to ensure the TX_TCLK jitter with respect to an un-jittered reference is within range. | ||
+ | Note the ADIN1300 does not expose TX_TCLK directly. | ||
+ | To configure the device in Test Mode 2, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(2) - Register 0x0009, bits 15:13: Enable Test Mode 2 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000, bit 11: Bring PHY out of Software Power Down | ||
+ | To configure the device in Test Mode 3, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(3) - Register 0x0009, bits 15:13: Enable Test Mode 3 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000, bit 11: Bring PHY out of Software Power Down | ||
+ | |||
+ | |||
+ | ==== TEST MODE 4 ==== | ||
+ | |||
+ | This test mode is used | ||
+ | - To ensure the peak distortion is within the specified range. | ||
+ | - To verify the return loss is above the specified attenuation. | ||
+ | - To verify the PHYs common-mode rejection ratio is in range | ||
+ | To configure the device in Test Mode 4, issue the following writes over MDIO | ||
+ | * MII_CONTROL.SFT_PD. Write(0b1) - Register 0x0000, bit 11: Place the device into Software Power Down | ||
+ | * MSTR_SLV_CONTROL.TST_MODE.Write(4) - Register 0x0009, bits 15:13. Enable Test Mode 4 | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11: Bring PHY out of Software Power Down | ||
+ | |||
+ | ---- | ||
+ | |||
+ | |||
+ | ===== 100BASE-TX ===== | ||
+ | |||
+ | For 100BASE-TX operation there are a variety of tests. There are two main test modes main register involved here is the B_100_TX_TST_MODE register at address 0xB413 (available via Clause 45 access) | ||
+ | |||
+ | |||
+ | ==== 100BASE-TX Transmit Test Mode Register ==== | ||
+ | |||
+ | Address: 0xB413, Reset: 0x0000, Name: B_100_TX_TST_MODE | ||
+ | This register provides the ability to transmit a 100BASE-TX test signal. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | To configure the device for 100BASE-TX VOD measurements, | ||
+ | * MII_CONTROL.Write(0x2900) - Register 0x0000 to place the device into Software PD, configure 100BASE-TX full duplex, autoneg disabled | ||
+ | * PHY_CTRL_1.AUTO_MDI_EN.Write(0b) - Register 0x0012, bit 10: Disable Auto MDI/MDIX | ||
+ | * PHY_CTRL_1.MAN_MDIX.Write(0b0) - Register 0x0012, bit 9: Operate in MDI configuration | ||
+ | * B_100_TX_TST_MODE.Write(1/ | ||
+ | * PHY_CTRL_3. LINK_EN.Write(0b1) - Register 0x0017, bit 13: Enable linking | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11: Bring PHY out of Software Power Down | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== 10BASE-TE/ | ||
+ | |||
+ | When operating in 10 Mbps speeds, the PHY is configured for 10BASE-Te transmit levels by default. 10BASE-T provides larger transmit levels and can be configured by clearing the B_10_E_EN register. | ||
+ | The 10BASE-Te/T compliance tests are: | ||
+ | * Link Pulse Testing | ||
+ | * Medium Attachment Unit (MAU) | ||
+ | * TP_IDL | ||
+ | * Jitter | ||
+ | * Differential Voltage | ||
+ | * Harmonics | ||
+ | * Transmitter Return Loss | ||
+ | * Receiver Return Loss | ||
+ | * Common-Mode Voltage | ||
+ | The B_10_TX_TST_MODE register is used to select transmit test signals useful for 10BASE-T compliance testing. | ||
+ | |||
+ | |||
+ | ==== 10BASE-T Transmit Test Mode Register ==== | ||
+ | |||
+ | |||
+ | Address: 0xB412, Reset: 0x0000, Name: B_10_TX_TST_MODE | ||
+ | This register provides the ability to transmit a 10BASE-T test signal. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | To configure the device for 10BASE-T transmit test mode, consisting of 5MHz square wave on desired dimension, issue the following writes over MDIO | ||
+ | * GE_SFT_RST_CFG_EN.Write(0b1) - Register 0xFF0D to ensure the hardware configuration is refreshed. | ||
+ | * GE_SFT_RST. Write(0b1) - Register 0xFF0C subsystem reset | ||
+ | * MII_CONTROL.SFT_RST. Write(0b1) - Register 0x0000 Issue a software reset, this bit is self clearing | ||
+ | * MII_CONTROL.Write(0x0900) - Register 0x0000 Enter Software Power Down and configure 10M FD, disable AutoNegotiation | ||
+ | * B_10_TX_TST_MODE.Write(0b100) - Register 0xB412 Choice of 100: Enable Transmit 5MHz square wave on Dim 1; 011: 5MHz on Dim0; 010 10MHz on Dim1; 001: 10MHz on Dim0. | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 Bring PHY out of Software | ||
+ | |||
+ | An alternative configuration, | ||
+ | * GE_SFT_RST_CFG_EN.Write(0b1) - Register 0xFF0D to ensure the hardware configuration is refreshed. | ||
+ | * GE_SFT_RST. Write(0b1) - Register 0xFF0C subsystem reset | ||
+ | * MII_CONTROL.SFT_RST. Write(0b1) - Register 0x0000 bit 15, Issue a software reset, this bit is self clearing | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11, Bring PHY out of Software | ||
+ | * PHY_CTRL_1.DIAG_CLK_EN.Write(0b1) - Register 0x0012 bit 2, Enable the Diagnostic Clock | ||
+ | * MII_CONTROL.LOOPBACK.Write(0b1) - Register 0x0000 bit 14, Enable Loopback | ||
+ | * PHY_CTRL_1.MAN_MDIX.Write(0b0) - Register 0x0012 bit 9, Operate in MDI configuration | ||
+ | * PHY_CTRL_STATUS_1.LB_TX_SUP.Write(0b0) - Register 0x0013 bit 6, Stop suppressing the transmit signal at the MDI pins in all digital loopback | ||
+ | * PHY_CTRL_STATUS_1.LB_ALL_DIG_SEL.Write(0b1) - Register 0x0013 bit12 Enable all digital loopback | ||
+ | * PHY_CTRL_3. LINK_EN.Write(0b1) - Register 0x0017 bit 13, Enable linking | ||
+ | * MII_CONTROL.SFT_PD.Write(0b0) - Register 0x0000 bit 11, Bring PHY out of Software | ||
+ | * Wait for Link up | ||
+ | * FG_CONT_MODE_EN.Write(0b1) - Register 0x9417 Enable the frame generator into continuous mode | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(1) - Register 0x9416, bits 2:0: Enable random number in the MAC client data frame field, options of decrementing, | ||
+ | * FG_EN.FG_EN.Write(1) - Enable Frame Generator | ||
+ | Setup for 10BASE-T forced mode in loopback with Tx suppression disabled, with transmission of frames with random payloads using the frame generator, | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b011) - 0xFF repeating payloads | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b010) - 0x00 repeating payloads | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b100) - alternative 0x55 payloads | ||
+ | * FG_CNTRL_RSTRT.FG_CNTRL.Write(0b101) - data field decrementing from 255 to 0(decimal) | ||
+ | |||
+ | 10BASE-T is configured by writing the following register – include it in the sequence above if 10BASE-T operation is required. | ||
+ | * B_10_E_EN.Write(0x0) - 10BASE-Te is enabled by default, write 0 to configure 10BASE-T. | ||
+ | |||
+ | |||
+ | ---- | ||
+ | |||
+ | |||
+ | ===== Testing Using ADI Evaluation GUI ===== | ||
+ | |||
+ | The ADI evaluation board uses small MDIO dongle board for USB to MDIO communications and the accompanying GUI provides access to the various Test modes from the “Test Mode” tab. Select the relevant test mode to configure and “Execute Test”. In the “Activity log” the register writes can be observed. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ---- |