| Previous revisionNext revision |
— | resources:eval:user-guides:ad7403 [08 Oct 2014 12:55] – [User Notes] Aidan Frost |
---|
| ====== MathWorks Simulink Model of AD7403 ====== |
| |
| A model of the [[http://www.analog.com/AD7403?doc=AD7403.pdf|AD7403]] is provided here for functional demonstration. It can accept various sources (for example: ramp, constant, sinusoid etc) and there is the option to apply a sinc filter to the output. The sinc filter is necessary to reconstruct the original information, by digitally filtering and decimating the modulator output. |
| |
| The [[http://www.analog.com/AD7403?doc=AD7403.pdf|AD7403]] is a high performance, second-order, Σ-Δ modulator that converts an analog input signal into a high speed, single-bit data stream, with on-chip digital isolation based on Analog Devices, Inc., iCoupler® technology. The [[http://www.analog.com/AD7403?doc=AD7403.pdf|AD7403]] operates from a 5 V (VDD1) power supply and accepts a differential input signal of ±250 mV (±320 mV full-scale). The differential input is ideally suited to shunt voltage monitoring in high voltage applications where galvanic isolation is required. |
| |
| The analog input is continuously sampled by a high performanceanalog modulator, and converted to a ones density digital output stream with a data rate of up to 20 MHz. The original information can be reconstructed with an appropriate digital filter to achieve 88 dB signal to noise ratio (SNR) at 78.1 kSPS.The serial input/output can use a 5 V or a 3 V supply (VDD2).The serial interface is digitally isolated. High speed complementarymetal oxide semiconductor (CMOS) technology, combined with monolithic transformer technology, means the on-chip isolation provides outstanding performance characteristics, superior to alternatives such as optocoupler devices. The [[http://www.analog.com/AD7403?doc=AD7403.pdf|AD7403]] device is offered in a 16-lead, wide-body SOIC package and has an operating temperature range of −40°C to +125°C. |
| |
| [[http://www.analog.com/AD7403?doc=AD7403.pdf|{{:resources:eval:user-guides:ad7403_fbs_1_.png?direct|}}]] |
| |
| <WRAP round info 65%> |
| In order to run the AD7403 model, your [[mw>products/matlab/|MATLAB]] license needs to include the following components: |
| * MATLAB (R2014a and beyond) |
| * Simulink |
| </WRAP> |
| |
| ====== Downloads ====== |
| |
| <WRAP download> |
| * http://www.analog.com/static/imported-files/design_tools/AD7403_Matlab_Model.zip |
| * This link provides a download of the .zip file. Simply extract the .zip and launch AD7403.slx. This will launch [[mw>products/matlab/|MATLAB]] and Simulink. |
| </WRAP> |
| ====== User Notes ====== |
| |
| To use the AD7403 model, ensure all the above packages are installed and download the zip file [[http://www.analog.com/static/imported-files/design_tools/AD7403_Matlab_Model.zip|here]]. Extract the files, and double click on <file>AD7403.slx</file>. |
| |
| On opening Simulink, the following block diagram will appear. |
| |
| {{:resources:eval:user-guides:simulink_bd.png?direct&300|}} |
| |
| If it is the first time running MATLAB, then it will need to be configured to use a compiler. To do this type the command <code matlab>mex -setup</code> This brings up the following window where a compiler can be selected. |
| |
| {{:resources:eval:user-guides:mex.png?direct&300|}} |
| |
| Various sources can be used as inputs to the model. Here, a Sine Wave source is used. A ramp or constant input can also be employed. |
| |
| The parameters of the sinc filter can be edited by double clicking on the relevant block. This launches the following window. |
| |
| {{:resources:eval:user-guides:sinc_variables.png?direct&300|}} |
| |
| The order of the filter and the decimation rate can be adjusted here. |
| |
| Running the model using the default conditions will result in the following output from the modulator and sinc filter. |
| |
| {{:resources:eval:user-guides:scope.png?direct&300|}} |
| |
| It is possible to change the FCLKIN frequency of the model. It is a global variable within the model as both the AD7403 and the SINC filter utilise it. To edit the variable, select Model Properties -> Callbacks -> InitFcn* |
| See below images. |
| |
| {{:resources:eval:user-guides:model_properties.png?direct&300|}} |
| |
| {{:resources:eval:user-guides:model_properties_2.png?direct&300|}} |