This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad713x:hdl [21 Jul 2023 11:32] – Update block diagram Laurentiu Popa | resources:eval:user-guides:ad713x:hdl [31 Jul 2023 08:32] (current) – Laurentiu Popa | ||
---|---|---|---|
Line 36: | Line 36: | ||
The design only supports the slave mode for both devices with both DCLK and ODR generated by the FPGA. Each device sends data on 4 of the 8 DIN bits. | The design only supports the slave mode for both devices with both DCLK and ODR generated by the FPGA. Each device sends data on 4 of the 8 DIN bits. | ||
- | {{: | + | {{: |
In order to build the HDL design the user has to go through the following steps: | In order to build the HDL design the user has to go through the following steps: |