This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad4170:hardwareguide [18 Mar 2024 07:29] – Addition on information for resistor jumper modification with input type selection Samruth Krishna Kumar | resources:eval:user-guides:ad4170:hardwareguide [14 May 2024 08:48] (current) – [Selecting the reference source:] Samruth Krishna Kumar | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== Set-up Procedures ====== | ====== Set-up Procedures ====== | ||
After following the instructions in the [[resources: | After following the instructions in the [[resources: | ||
- | * **Warning: | + | * **Warning: |
- | - Connect the EV-AD4170-ASD1Z-U1 | + | - Connect the EVAL-AD4170-4ARDZ to the controller board |
- | - **Option A:** Connect the EV-AD4170-ASD1Z-U1 to the EVAL-SDP-CK1Z | + | - Using the Arduino Connectors {{ : |
- | - Using the 120 pin connector | + | |
- | * Screw the two boards together using the plastic screw-washer set included in the evaluation board kit to ensure that the boards are connected firmly together. | + | |
- | | + | |
- | - **Option B:** Connect the EV-AD4170-ASD1Z-U1 to the EVAL-SDP-CB1Z | + | |
- | * Using the 120 pin connector | + | |
- | * Screw the two boards together using the plastic screw-washer set included in the evaluation board kit to ensure that the boards are connected firmly together. {{ : | + | |
Line 38: | Line 33: | ||
| LK18 |N/A |DNI|SCP connect AC amplifier external AVDD and Ground| Left of J5| | | LK18 |N/A |DNI|SCP connect AC amplifier external AVDD and Ground| Left of J5| | ||
| LK19 |Black| Uninserted|XTAL2 to Digital connector| Above PMOD (P6)| | | LK19 |Black| Uninserted|XTAL2 to Digital connector| Above PMOD (P6)| | ||
+ | |LK20 |Black| A |External VREF LTC6655 | Right to J1 | | ||
| LK21 |Black| Inserted| Inserted: External crystal Uninserted External clock| Above SMB1 (Right)| | | LK21 |Black| Inserted| Inserted: External crystal Uninserted External clock| Above SMB1 (Right)| | ||
| LK22 | Blue | A| GPIO 0: Pos A: To Connector J4 Pos B: Mosfet| Below J4| | | LK22 | Blue | A| GPIO 0: Pos A: To Connector J4 Pos B: Mosfet| Below J4| | ||
Line 67: | Line 63: | ||
|AC input|R41, R110|R27, R40| | |AC input|R41, R110|R27, R40| | ||
|DC input|R42, R111|R26, | |DC input|R42, R111|R26, | ||
+ | {{ : | ||
+ | *For configuring AIN3-AIN4 as AC inputs resistors R41, R110 must be populated and R42, R111 must not be populated. Similarly for configuring AIN3-AIN4 as AC inputs resistors R42, R111 must be populated and R41, R110 must not be populated. | ||
+ | *For configuring AIN7-AIN8 as AC inputs resistors R27, R40 must be populated and R26, R39 must not be populated. Similarly for configuring AIN7-AIN8 as AC inputs resistors R26, R39 must be populated and R27, R40 must not be populated. | ||
====== On Board Connections ====== | ====== On Board Connections ====== | ||
Line 209: | Line 207: | ||
There are four primary signals: CS, SCLK, SDI, and SDO/RDY (all are inputs, except for SDO/RDY, which is an output). | There are four primary signals: CS, SCLK, SDI, and SDO/RDY (all are inputs, except for SDO/RDY, which is an output). | ||
===Serial communication options=== | ===Serial communication options=== | ||
- | - SDP-B board and the respective 120 pin SDP connector. | ||
- | *When using the SDP-B connection (120 pin) The evaluation board connects via the serial peripheral interface (SPI) to the Blackfin® [[adi> | ||
- Arduino connection SDP-K1 | - Arduino connection SDP-K1 | ||
- PMOD connector | - PMOD connector | ||
- Standalone mode | - Standalone mode | ||
- | * Removing the links LK12,27,28,29and using the pins from these links can then be used to fly-wire the signals to an alternative digital capture setup | + | * Removing the jumper resistors R92,R86,R88,R90 and mounting them on R93, |
For an introduction to the Serial Peripheral Interface (SPI), click [[adi> | For an introduction to the Serial Peripheral Interface (SPI), click [[adi> | ||
Line 223: | Line 219: | ||
====== Reference Options ====== | ====== Reference Options ====== | ||
- AD4170 Internal Reference | - AD4170 Internal Reference | ||
- | - **DEFAULT** [[adi> | + | - **DEFAULT: |
- External Reference Connector J1 | - External Reference Connector J1 | ||
* Option to use PT1000 precision resistor (R3) insert LK3 | * Option to use PT1000 precision resistor (R3) insert LK3 | ||
Line 240: | Line 236: | ||
- **Internal Reference** REFIN_REFOUT (Hex Value 2). | - **Internal Reference** REFIN_REFOUT (Hex Value 2). | ||
===Hardware=== | ===Hardware=== | ||
- | If REFIN1+/- is selected the options below are available using links LKREF+ and LKREF- shown in the diagram below | + | If REFIN1+/- is selected the options below are available using links LKREF+ and LKREF- shown in the diagram below |
- | - [[adi> | + | - External Voltage reference (LTC6655 - Default) |
+ | [[adi> | ||
+ | [[adi> | ||
- External Reference Connector J1 | - External Reference Connector J1 | ||
- External Reference Connector J2 | - External Reference Connector J2 | ||
+ | |||
Line 288: | Line 287: | ||
====== Schematics ====== | ====== Schematics ====== | ||
- | {{ : | + | {{ : |
====== Bill of Materials ====== | ====== Bill of Materials ====== | ||
- | {{ : | + | {{ : |
[[resources: | [[resources: | ||
Line 305: | Line 304: | ||
{{: | {{: | ||
+ | *Mount Resistors R111,R42 and depopulate R42, R110 to make AIN3-AIN4 compatible for DC measurements. | ||
{{: | {{: | ||
+ | *Mount Resistors R26,R39 and depopulate R27,R40 to make AIN7-AIN8 compatible for DC measurements. | ||
===== 3 wire RTD ===== | ===== 3 wire RTD ===== | ||
Line 312: | Line 313: | ||
{{: | {{: | ||
+ | *Mount Resistors R111,R42 and depopulate R42, R110 to make AIN3-AIN4 compatible for DC measurements. | ||
+ | *Mount Resistors R26,R39 and depopulate R27,R40 to make AIN7-AIN8 compatible for DC measurements. | ||
===== 4 wire RTD ===== | ===== 4 wire RTD ===== | ||
Line 319: | Line 322: | ||
{{: | {{: | ||
+ | *Mount Resistors R26,R39 and depopulate R27,R40 to make AIN7-AIN8 compatible for DC measurements. | ||
===== Thermocouple ===== | ===== Thermocouple ===== | ||
{{: | {{: | ||
Line 327: | Line 331: | ||
{{: | {{: | ||
+ | *Mount Resistors R111,R42 and depopulate R42, R110 to make AIN3-AIN4 compatible for DC measurements. | ||
{{: | {{: | ||
{{: | {{: | ||
+ | *Mount Resistors R26,R39 and depopulate R27,R40 to make AIN7-AIN8 compatible for DC measurements. | ||
===== Loadcell with DC excitation ===== | ===== Loadcell with DC excitation ===== | ||
Line 336: | Line 342: | ||
{{: | {{: | ||
+ | *Mount Resistors R111,R42 and depopulate R42, R110 to make AIN3-AIN4 compatible for DC measurements. | ||
{{: | {{: | ||
{{: | {{: | ||
+ | *Mount Resistors R26,R39 and depopulate R27,R40 to make AIN7-AIN8 compatible for DC measurements. | ||
===== Loadcell with AC excitation ===== | ===== Loadcell with AC excitation ===== | ||
Line 345: | Line 353: | ||
{{: | {{: | ||
+ | *Mount Resistors R111,R42 and depopulate R42, R110 to make AIN3-AIN4 compatible for DC measurements. | ||
{{: | {{: | ||
{{: | {{: | ||
+ | *Mount Resistors R26,R39 and depopulate R27,R40 to make AIN7-AIN8 compatible for DC measurements. | ||
===== Accelerometer ===== | ===== Accelerometer ===== | ||
{{: | {{: | ||
+ | *Mount Resistors R24 and depopulate R25 to make AIN2 compatible for Accelerometer measurements. | ||