After following the instructions in the Software Procedures section, set up the evaluation and SDP boards as detailed in this section.
Link Numbers | Colour | Default Position | Descirption | Rough Board Location |
---|---|---|---|---|
LK1 | Blue | Inserted | Noise Test. Channels AIN5 + AIN6 | Right of J1 |
LK2 | Red | Inserted | Thermocouple - Cold Junction Resistor Bypass | Right of J1 |
LK3 | Red | Inserted | Precision Reference Resistor Bypass | Right of J1 |
LK4 | Red | A | Pos A: GPIO 1 (IOUT1) to J1 Pos B: REFOUT | Right of J1 |
LK5 | Blue | B | Wire Bridge EXC+ select: Pos A: MOSFET+ Pos B: AVDD | Right of J2 (EXC+) |
LK6 | Blue | Uninserted | Short EXC+/REFIN+: Pos Inserted = 4 Wire Bridge | Right of J2 (4/6 wire) |
LK7 | Blue | B | Wire Bridge EXC- select: Pos A: MOSFET- Pos B: Power Switch (GPIO1) | Right of J2 (EXC-) |
LK8 | Blue | Uninserted | Short EXC-/AVSS: Pos Inserted = 4 Wire Bridge | Right of J2 (EXC-) |
LK9 | Blue | Uninserted | Short EXC-/REFIN-: Pos Inserted = 4 Wire Bridge | Right of J2 (4/6 wire) |
LK10 | Black | A | AD4595 AIN3+ AIN4. AVDD select. Pos A: Internal AVDD Pos B: External AVDD | Below of J5 (AMP34) |
LK11 | Black | A | AD4595 AIN3+ AIN4. AVSS select. Pos A: Internal AVSS Pos B: External AVSS | Below of J5 (AMP34) |
LK12 | Black | A | AD4595 AIN7+ AIN8. AVDD select. Pos A: Internal AVDD Pos B: External AVDD | Below of J5 (AMP78) |
LK13 | Black | A | AD4595 AIN7+ AIN8. AVSS select. Pos A: Internal AVSS Pos B: External AVSS | Below of J5 (AMP78) |
LK14 | N/A | DNI | SCP connect AC amplifier external AVSS and Ground | Left of J5 |
LK15 | N/A | DNI | SCP connect external AVSS and Ground | Right of J5 |
LK16 | N/A | DNI | SCP connect external AVDD and Ground | Right of J5 |
LK17 | N/A | DNI | SCP connect external IOVDD and Ground | Right of J5 |
LK18 | N/A | DNI | SCP connect AC amplifier external AVDD and Ground | Left of J5 |
LK19 | Black | Uninserted | XTAL2 to Digital connector | Above PMOD (P6) |
LK21 | Black | Inserted | Inserted: External crystal Uninserted External clock | Above SMB1 (Right) |
LK22 | Blue | A | GPIO 0: Pos A: To Connector J4 Pos B: Mosfet | Below J4 |
LK23 | Blue | A | GPIO 1: Pos A: To Connector J4/J2 (LK31) Pos B: Mosfet | Below J4 |
LK24 | Red | A | GPIO 2: Pos A: To Connector J1 Pos B: Mosfet | Right of J2 |
LK25 | Red | A | GPIO 3: Pos A: To Connector J1 Pos B: Mosfet | Right of J2 |
LK26 | Black | A | ADXL1002 Test Pos A: Test Pos B:Standard | Below IOVDD LED (midle right) |
LK31 | Blue | A | GPIO1 Connector select. Pos A: J2 (Power Switch) Pos B: J3 | Below J4 |
LK32 | Black | A | IOVDD select. Pos A: 3.3V Pos B: EXT | Below J5 (near IOVDD LED) |
LK33 | Black | A | LT1962-5 power down Pos A: On | Below J5 |
LK34 | Black | A | LTC3129 power down Pos A: On | Below J5 |
LK35 | Black | A | LT1962-2.5 power down Pos A: On | Below J5 |
LK36 | Black | A | LTC1983 power down Pos A: On | Below J5 |
LK37 | Black | A | ADP7182 power down Pos A: On | Below J5 |
LK38 | Black | A | ADP150 power down Pos A: On | Below J5 |
LK39 | Grey | Inserted | AVSS GND short | Top Left |
LK40 | Grey | Inserted | AVSS GND short | Above Thermocouple Connection |
LK41 | Grey | Inserted | AVSS GND short | Below J4 |
LK42 | Grey | Inserted | AVSS GND short | Below J5 |
LK43 | Grey | Inserted | AVSS GND short | Right of J1 |
LK44 | Grey | Inserted | AVSS GND short | Below J5 (near AVDD LED) |
LK45 | Grey | Inserted | AVSS GND short | Left of PMOD (P6) |
LK46 | Grey | Inserted | AVSS GND short | Right of Thermocouple Connection |
LKVOCM34 | Black | 4525 | VOCM ADA4945 Pos A: DACOUT Pos B: VBIAS Pos C: AD4525 Pos D: REFOUT | Right of Thermocouple Connection |
LKVOCM78 | Black | 4525 | VOCM ADA4945 Pos A: DACOUT Pos B: VBIAS Pos C: AD4525 Pos D: REFOUT | Middle of board |
Functionality:
Connection | Function |
---|---|
1 | 1) IOUT1/GPIO2 Excitation current for 3 wire RTD. LK4 (posA) 2) REFOUT lk4 (posB) |
2 | IOUT0 GPIO3 Excitation current for RTDs |
3 | AIN 8 with DC filtering |
4 | AIN 7 with DC filtering |
5 | AIN 4 with DC filtering (TC- connection) |
6 | AIN 3 with DC filtering (TC+ connection) |
7 | AIN 1 with DC filtering (RTD- connection) (Cold Junction- connection) |
8 | AIN 0 with DC filtering (RTD+ connection) (Cold Junction+ connection) |
9 | External Reference + |
10 | External Reference - |
Functionality:
Connection | Function |
---|---|
1 | Ground/shield connection |
2 | Excitation - (MOSFET) /Power Switch Function (GPIO1) for Wire Bridge |
3 | External Reference- / Sense- |
4 | AIN 6 (AINN) with DC filtering(DNI) and noise test channel |
5 | AIN 5 (AINP) with DC filtering(DNI) and noise test channel |
6 | External Reference+ / Sense+ |
7 | Excitation+ (MOSFET) /AVDD supply for Wire Bridge |
8 | Ground/shield connection |
Functionality:
Connection | Function |
---|---|
1 | AIN 8 with AC filtering |
2 | AIN 7 with AC filtering |
3 | AIN 4 with AC filtering |
4 | AIN 3 with AC filtering |
5 | AIN 2 with DC filtering |
6 | DACOUT with 2kΩ Load |
Connection | Function |
---|---|
1 | GPIO1 |
2 | GPIO0 |
3 | DIGAUX1 |
4 | DIGAUX2 |
Connection | Function |
---|---|
1 | External AVDD connection |
2 | External AVSS connection |
3 | External IOVDD connection |
4 | External GND connection |
5 | External AVDD connection for Amplifier |
6 | External AVSS connection for Amplifier |
7 | External GND connection for Amplifier |
Connection | Function | Connection | Function |
---|---|---|---|
1 | XTAL2 | 7 | SDO |
2 | CS_N | 8 | SCLK |
3 | DIGAUX1 | 9 | GND |
4 | SDI | 10 | GND |
5 | DIGAUX2 | 11 | IOVDD |
6 | SDO | 12 | IOVDD |
There are 9 SMB connections on the board. To allow clock signals and analog inputs into the board.
The evaluation board receives power through the controller board when connected to the PC via USB. Linear regulators generate the required power supply levels from the applied USB voltage.
Supply | Regulator | Shut down Link (ORANGE) |
---|---|---|
5V regulator | LTC3129-1EUD | LK34 |
2.5V regulator | LT1962 | LK35 |
-3.3V regulator | LTC1983 | LK36 |
-2.5V regulator | ADP7182 | LK37 |
Supply | Regulator | Shut down Link (ORANGE) |
---|---|---|
3.3V regulator | ADP7182 | LK34 |
There are four primary signals: CS, SCLK, SDI, and SDO/RDY (all are inputs, except for SDO/RDY, which is an output).
For an introduction to the Serial Peripheral Interface (SPI), click here
Example shows setting reference for Channel 0, for channel n, go to register AFE[n]
If REFIN1+/- is selected the options below are available using links LKREF+ and LKREF- shown in the diagram below
The General purpose input/output pins are powered by AVDD/AVSS. They can be used to provide AC-Excitation signals for AC-Excited sensors, using 2 or 4 outputs. Can be used to automatically control an external multiplexer by outputting the current sequencer channel. Other optional functions include Current Source outputs , 2nd Reference input, Power-down switch.
GPIO | Functionality |
---|---|
GPIO0 | PSW |
IOUT | |
REFIN2+ | |
GPIO1 | REFIN2- |
PSW | |
IOUT | |
GPIO2 | IOUT |
GPIO3 | IOUT |
The evaluation board highlights the functionality of the GPIOs
Below is the circuit for the AC excitation circuit.
This Circuit outputs to EXC+ and EXC- on J2. This is enabled when LK22,LK23,LK24,LK25 are in posB
This section summarizes the sensor connection and jumper configuration used depending the selected demo mode. For every demo mode, the sensor can be connected to several input channels, therefore the EVAL must be correctly configured to ensure the proper operation.
These configurations are the ones used by default with the provided mbed firmware. If any other configuration is desired, the software must be modified by the user.