This shows you the differences between two versions of the page.
— | resources:eval:user-guides:ad2s1210_sdz [19 Jul 2023 16:14] (current) – created Andrei Grozav | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== EVAL-AD2S1210SDZ Evaluation Board on ZedBoard User Guide ====== | ||
+ | **Evaluation Board for the AD2S1210 Variable Resolution, 10-Bit to 16-Bit R/D Converter with Reference Oscillator** | ||
+ | |||
+ | ADD PIC | ||
+ | |||
+ | ===== Features ===== | ||
+ | * Complete monolithic resolver-to-digital converter | ||
+ | * Is supported on [[https:// | ||
+ | |||
+ | ===== Hardware Required ===== | ||
+ | * 16GB (or larger) Class 10 (or faster) micro-SD card | ||
+ | * [[https:// | ||
+ | * [[: | ||
+ | * 12Vdc, 3A power supply | ||
+ | * Micro-USB cable | ||
+ | * Ethernet cable | ||
+ | * User interface setup (choose one): | ||
+ | * HDMI monitor, keyboard, and mouse plugged directly into the Zedboard | ||
+ | * Host Windows/ | ||
+ | |||
+ | ===== Software Required ===== | ||
+ | * You need a Host PC (Windows or Linux) | ||
+ | * A UART terminal (Putty/Tera Term/ | ||
+ | * IIO Scope Download | ||
+ | * [[: | ||
+ | |||
+ | ===== General Description ===== | ||
+ | The EVAL-AD2S1210SDZ is a full featured evaluation board designed to allow the user to easily evaluate all the features of the AD2S1210 resolver-to-digital converter (RDC). | ||
+ | |||
+ | ===== Quick Start Guide ===== | ||
+ | |||
+ | ==== Loading Image on SD Card ==== | ||
+ | To boot the Zedboard and control the [[ADI> | ||
+ | |||
+ | ==== Configuring the SD Card ==== | ||
+ | |||
+ | Follow the configuration procedure under **Configuring the SD Card for FPGA Projects** on the [[: | ||
+ | |||
+ | |||
+ | * **uImage** file for Zynq | ||
+ | * **BOOT.BIN** specific to your [[ADI> | ||
+ | * **devicetree.dtb** for Zynq specific to your [[ADI> | ||
+ | |||
+ | |||
+ | |||
+ | ==== Setting up the Hardware ==== | ||
+ | |||
+ | |||
+ | You will need to: | ||
+ | |||
+ | * Get the [[https:// | ||
+ | * Insert the SD-CARD into the SD Card Interface Connector (J12). \\ | ||
+ | * Connect the [[ADI> | ||
+ | * Connect USB UART J14 (Micro USB) to your host PC. \\ | ||
+ | * Plug your ethernet cable into the RJ45 ethernet connector(J11). \\ | ||
+ | * Plug the Power Supply into the 12V Power input connector (J20) (DO NOT turn the device on). \\ | ||
+ | * Set the jumpers as seen in the below picture: {{ resources: | ||
+ | <note tip> | ||
+ | * Connect the oscilloscope probes to the SMB connectors. \\ | ||
+ | * Turn it on. \\ | ||
+ | * Wait ~30 seconds for the “DONE” LED to turn blue. This is near the DISP1. \\ | ||
+ | |||
+ | {{page> | ||
+ | |||
+ | ===== Application Software (both locally and remotely on the FPGA) ===== | ||
+ | |||
+ | ==== Hardware Connection ==== | ||
+ | ^ FPGA ^^ SDP ADAPTER | ||
+ | |Connected to | FMC NAME | FMC PIN | SCH SIG NAME | SDP(J2) PIN | SCH NAME | | ||
+ | |PS SPI 0 SDI | FMC_LPC_LA01_CC_P | ||
+ | |PS SPI 0 SDO | FMC_LPC_CLK0_M2C_P | H04 | CON_PAR_DATA[14] | | ||
+ | |PS SPI 0 CLK | FMC_LPC_CLK0_M2C_N | H05 | CON_PAR_DATA[13] | | ||
+ | |Logic low | FMC_LPC_LA04_N | ||
+ | |PS SPI 0 CSn 0 | FMC_LPC_LA09_N | ||
+ | |PS EMIO 32 (Linux 86)| FMC_LPC_LA13_N | ||
+ | |PS EMIO 33 (Linux 87)| FMC_LPC_LA07_P | ||
+ | |PS EMIO 34 (Linux 88)| FMC_LPC_LA21_P | ||
+ | |PS EMIO 35 (Linux 89)| FMC_LPC_LA26_P | ||
+ | |PS EMIO 36 (Linux 90)| FMC_LPC_LA27_P | ||
+ | |||
+ | SPI connections | ||
+ | |||
+ | ^ SPI manager instance | ||
+ | | psu spi 0 | spi_fpga | ||
+ | |||
+ | === GPIO signals(schematic) === | ||
+ | |||
+ | Ps8 EMIO offset = 54 | ||
+ | |||
+ | ^ GPIO Signal | ||
+ | | TMR_A (SAMPLE) | 90 | 36 | | ||
+ | | SDP_RES_1 | ||
+ | | SDP_RES_0 | ||
+ | | A1 | 87 | 33 | | ||
+ | | A0 | 86 | 32 | | ||
+ | |||
+ | ==== IIO Oscilloscope ==== | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | * Once done with the installation or an update of the latest IIO-Oscilloscope, | ||
+ | * Press refresh to display available IIO Devices and press connect. | ||